Setup ADRV9364-Z7020 with ADRV1CRR-FMC using MATLAB

Matlab has the whole instructions on how to setup the radio using Communication Toolbox for Zynq , I followed the procedure. But I have a doubt on switch configuration. I am trying to boot using SD card.I have tried with S1,S3,S4 On(position away from dot on switch). For some reason the LED DS3 which should've blinked suggesting successful boot, isn't happening. I even did a carrier rest according to the procedure and waited at least 5mins but it didn't work.

D3,D4 LED are ON continuously. 

I just took a random SD card and Matlab downloaded some files onto it, Is there anything I am missing? I am a rookie in the field, any help would be great. 

And is there any jumper setting? Currently all are open



V1
[edited by: Sumanth_Raikar at 6:30 AM (GMT -4) on 26 Jul 2021]
Parents Reply Children
  • Does that mean I can't use HDL coder or Embedded Coder from MATLAB?

    I saw many example designs based on MATLAB which used adrv9361, but is it valid to 9364?

    If I can't use MATLAB packages then what are the options I have?

  • 1. I would reach out to MathWorks to see if they have some support for this configuration.

    2. You can try the Transceiver Toolbox: https://wiki.analog.com/resources/tools-software/transceiver-toolbox It does have support for ADRV9364. We do not test ADRV9364+FMC but the BOB should work on the data path. I would first verify your board boots with the boot files provided on the SD card first. That will tell you if the combination functions.

    -Travis

  • I copied boot.bin and .dtb from bob-cmos folder to boot partition main directory, Switches s1,s3,s4 on ADRV9364 are ON(pointing away from the dot on switches), which I think does SD Card boot from the FMC Card slot. But I am only seeing D3,D4 LED's on SOM glowing continuously.

    On the FMC DS8,DS2  glows red.  I opened serial console using teraterm  but the terminal is blank. Please help me identify the problem with booting.

  • Someone with an ADRV9364+FMC will try out this configuration and get back to you.

    -Travis

  • Tested on my side using the 2021-02-23-ADI-Kuiper.img from here:

    https://wiki.analog.com/resources/tools-software/linux-software/zynq_images

    Copied files from the zynq-adrv9364-z7020-bob-cmos and zynq-common folder.

    My switches are set same as yours.

    Initially all LEDs are like yours, but after a second D4 on the SoM turns off and DS7 on the carrier turns on. These LEDs indicate CFG Done. 

    So in case this doesn't happen. The FPGA didn't boot. 

    Typical root cause is SD card selector in the wrong position, or BOOTMODE set incorrectly.

    Can you try to:

    1) Use our latest boot files from the link above.

    2) Also try to use the SD Card socket on the SoM itself.

    3) Move the switches ON/OFF and make sure they are really in their end position.

     

    U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21)
    
    Board:  Xilinx Zynq
    I2C:   ready
    DRAM:  ECC disabled 512 MiB
    MMC:   zynq_sdhci: 0
    SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
    In:    serial
    Out:   serial
    Err:   serial
    Net:   Gem.e000b000
    Hit any key to stop autoboot:  0 
    Device: zynq_sdhci
    Manufacturer ID: 3
    OEM: 5344
    Name: SC64G 
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 59.5 GiB
    Bus Width: 4-bit
    reading uEnv.txt
    407 bytes read in 26 ms (14.6 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from SD ...
    Running uenvcmd ...
    Copying Linux from SD to RAM...
    reading uImage
    6484280 bytes read in 575 ms (10.8 MiB/s)
    reading devicetree.dtb
    17559 bytes read in 38 ms (451.2 KiB/s)
    reading uramdisk.image.gz
    ** Unable to read file uramdisk.image.gz **
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-4.19.0-ga6ef26d
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    6484216 Bytes = 6.2 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 02a00000
       Booting using the fdt blob at 0x2a00000
       Loading Kernel Image ... OK
       Loading Device Tree to 1ed1c000, end 1ed23496 ... OK
    
    Starting kernel ...
    
    Booting Linux on physical CPU 0x0
    Linux version 4.19.0-ga6ef26d (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1104 SMP PREEMPT Fri Feb 19 15:59:18 GMT 2021
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt: Machine model: Analog Devices ADRV9364-Z7020 (Z7020/AD9364)
    OF: fdt: earlycon: stdout-path /amba@0/uart@E0001000 not found
    Memory policy: Data cache writealloc
    cma: Reserved 128 MiB at 0x38000000
    random: get_random_bytes called from start_kernel+0xa0/0x404 with crng_init=0
    percpu: Embedded 16 pages/cpu @(ptrval) s33548 r8192 d23796 u65536
    Built 1 zonelists, mobility grouping on.  Total pages: 260608
    Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1�
    Booting kernel: `1ṹ' invalid for parameter `cpuidle.off'
    Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    Memory: 888452K/1048576K available (9216K kernel code, 760K rwdata, 7012K rodata, 1024K init, 163K bss, 29052K reserved, 131072K cma-reserved, 131072K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
        lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0x(ptrval) - 0x(ptrval)   (10208 kB)
          .init : 0x(ptrval) - 0x(ptrval)   (1024 kB)
          .data : 0x(ptrval) - 0x(ptrval)   ( 761 kB)
           .bss : 0x(ptrval) - 0x(ptrval)   ( 164 kB)
    rcu: Preemptible hierarchical RCU implementation.
    rcu:    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
            Tasks RCU enabled.
    rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    efuse mapped to (ptrval)
    slcr mapped to (ptrval)
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at (ptrval)
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at (ptrval), irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: Spectre v2: using BPIALL workaround
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100060
    rcu: Hierarchical SRCU implementation.
    smp: Bringing up secondary CPUs ...
    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    CPU1: Spectre v2: using BPIALL workaround
    smp: Brought up 1 node, 2 CPUs
    SMP: Total of 2 processors activated (1333.33 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    futex hash table entries: 512 (order: 3, 32768 bytes)
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 6249999) is a xuartps
    console [ttyPS0] enabled
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    media: Linux media interface: v0.10
    videodev: Linux video capture interface: v2.00
    jesd204: found 0 devices and 0 topologies
    FPGA manager framework
    Advanced Linux Sound Architecture Driver Initialized.
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
    TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    UDP hash table entries: 512 (order: 2, 16384 bytes)
    UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    NET: Registered protocol family 1
    hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    workingset: timestamp_bits=30 max_order=18 bucket_order=0
    bounce: pool size: 64 pages
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    io scheduler mq-deadline registered
    io scheduler kyber registered
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    brd: module loaded
    loop: module loaded
    Registered mathworks_ip class
    mwipcore 43c00000.mwipcore: Dev memory resource found at (ptrval) 0000FFFF. 
    mwipcore 43c00000.mwipcore: 'mwipcore' device not found, creating
    mwipcore 43c00000.mwipcore: Char dev region registered: major num:247
    mwipcore 43c00000.mwipcore: 'mwipcore' device created
    m25p80 spi1.0: SPI-NOR-UniqueID 100000235523732500290028090216db49
    m25p80 spi1.0: n25q256a (32768 Kbytes)
    6 fixed-partitions partitions found on MTD device spi1.0
    Creating 6 MTD partitions on "spi1.0":
    0x000000000000-0x0000000e0000 : "qspi-fsbl-uboot"
    0x0000000e0000-0x000000100000 : "qspi-uboot-env"
    0x000000100000-0x000000600000 : "qspi-linux"
    0x000000600000-0x000000620000 : "qspi-device-tree"
    0x000000620000-0x000001300000 : "qspi-rootfs"
    0x000001300000-0x000002000000 : "qspi-bitstream"
    MACsec IEEE 802.1AE
    libphy: Fixed MDIO Bus: probed
    tun: Universal TUN/TAP device driver, 1.6
    libphy: MACB_mii_bus: probed
    Marvell 88E1510 e000b000.ethernet-ffffffff:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.ethernet-ffffffff:00, irq=POLL)
    macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:0a:35:00:01:22)
    usbcore: registered new interface driver asix
    usbcore: registered new interface driver ax88179_178a
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver net1080
    usbcore: registered new interface driver cdc_subset
    usbcore: registered new interface driver zaurus
    usbcore: registered new interface driver cdc_ncm
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    usbcore: registered new interface driver uas
    usbcore: registered new interface driver usb-storage
    usbcore: registered new interface driver usbserial_generic
    usbserial: USB Serial support registered for generic
    usbcore: registered new interface driver ftdi_sio
    usbserial: USB Serial support registered for FTDI USB Serial Device
    usbcore: registered new interface driver upd78f0730
    usbserial: USB Serial support registered for upd78f0730
    chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
    chipidea-usb2 e0002000.usb: Linked as a consumer to regulator.0
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    ci_hdrc ci_hdrc.0: EHCI Host Controller
    ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: EHCI Host Controller
    usb usb1: Manufacturer: Linux 4.19.0-ga6ef26d ehci_hcd
    usb usb1: SerialNumber: ci_hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    i2c /dev entries driver
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (1.1.1)
    gspca_main: v2.14.0 registered
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
    Xilinx Zynq CpuIdle Driver started
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
    ledtrig-cpu: registered to indicate activity on CPUs
    hidraw: raw HID events driver (C) Jiri Kosina
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    ad7291: probe of 0-002c failed with error -5
    ad9361 spi0.0: ad9361_probe : enter (ad9364)
    ad9361 spi0.0: No GPIOs defined for ext band ctrl
    random: fast init done
    mmc0: new high speed SDXC card at address aaaa
    mmcblk0: mmc0:aaaa SC64G 59.5 GiB 
     mmcblk0: p1 p2 p3
    ad9361 spi0.0: ad9361_probe : AD936x Rev 2 successfully initialized
    cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x79024000 mapped to 0x(ptrval), probed DDS AD9364
    axi_sysid 45000000.axi-sysid-0: [adrv9364z7020_ccbob] on [cmos] git <061d024d596ef84c6a819854bf2472e6b43a2d5d> clean [2021-02-19 15:52:30] UTC
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
    Registering SWP/SWPB emulation handler
    cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x79020000 mapped to 0x(ptrval), probed ADC AD9364 as MASTER
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    hctosys: unable to open rtc device (rtc0)
    clk: Not disabling unused clocks
    ALSA device list:
      No soundcards found.
    EXT4-fs (mmcblk0p2): recovery complete
    EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing unused kernel memory: 1024K
    Run /sbin/init as init process
    systemd[1]: System time before build time, advancing clock.
    systemd[1]: Failed to lookup module alias 'autofs4': Function not implemented
    systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
    systemd[1]: Detected architecture arm.
    
    Welcome to Kuiper GNU/Linux 10 (buster)!
    
    systemd[1]: Set hostname to <analog>.
    systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    systemd[1]: /etc/systemd/system/tof-server.service:1: Assignment outside of section. Ignoring.
    systemd[1]: /etc/systemd/system/tof-server.service:2: Assignment outside of section. Ignoring.
    random: systemd: uninitialized urandom read (16 bytes read)
    random: systemd: uninitialized urandom read (16 bytes read)
    systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    random: systemd: uninitialized urandom read (16 bytes read)
    systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [  OK  ] Reached target Slices.
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
    [  OK  ] Created slice system-getty.slice.
    [  OK  ] Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [  OK  ] Reached target Swap.
    [  OK  ] Listening on Journal Socket.
             Starting Journal Service...
             Starting Restore / save the current clock...
             Mounting Kernel Debug File System...
             Starting Set the console keyboard layout...
    [  OK  ] Listening on fsck to fsckd communication Socket.
             Mounting RPC Pipe File System...
    [  OK  ] Started Forward Password R�…uests to Wall Directory Watch.
    [  OK  ] Listening on udev Kernel Socket.
             Starting udev Coldplug all Devices...
             Starting Load Kernel Modules...
    [  OK  ] Started Journal Service.
    [  OK  ] Started Restore / save the current clock.
    [  OK  ] Mounted Kernel Debug File System.
    [FAILED] Failed to mount RPC Pipe File System.
    See 'systemctl status run-rpc_pipefs.mount' for details.
    [DEPEND] Dependency failed for RPC �…curity service for NFS server.
    [DEPEND] Dependency failed for RPC �…ice for NFS client and server.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Set the console keyboard layout.
             Mounting Kernel Configuration File System...
             Starting Apply Kernel Variables...
    [  OK  ] Reached target NFS client services.
    [  OK  ] Reached target Remote File Systems (Pre).
    [  OK  ] Reached target Remote File Systems.
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Started Apply Kernel Variables.
             Starting Helper to synchronize boot up for ifupdown...
    [  OK  ] Started Helper to synchronize boot up for ifupdown.
    [  OK  ] Started Remount Root and Kernel File Systems.
             Starting Load/Save Random Seed...
             Starting Create System Users...
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Create System Users.
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Starting udev Kernel Device Manager...
    [  OK  ] Started udev Kernel Device Manager.
             Starting Show Plymouth Boot Screen...
    [  OK  ] Started Show Plymouth Boot Screen.
    [  OK  ] Started Forward Password R�…s to Plymouth Directory Watch.
    [  OK  ] Reached target Local Encrypted Volumes.
    [  OK  ] Found device /dev/ttyPS0.
    [  OK  ] Found device /dev/disk/by-partuuid/18f1f9d5-01.
             Starting File System Check�…isk/by-partuuid/18f1f9d5-01...
    [  OK  ] Started File System Check Daemon to report status.
    [  OK  ] Started File System Check �…/disk/by-partuuid/18f1f9d5-01.
             Mounting /boot...
    [  OK  ] Mounted /boot.
    [  OK  ] Reached target Local File Systems.
             Starting Raise network interfaces...
             Starting Set console font and keymap...
             Starting Create Volatile Files and Directories...
             Starting Preprocess NFS configuration...
             Starting Tell Plymouth To Write Out Runtime Data...
    [  OK  ] Started Set console font and keymap.
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Preprocess NFS configuration.
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting Load Kernel Modules...
    [  OK  ] Started Raise network interfaces.
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Synchronized.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on triggerhappy.socket.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Started Daily man-db regeneration.
    [  OK  ] Started Daily apt download activities.
    [  OK  ] Started Daily apt upgrade and clean activities.
    [  OK  ] Listening on GPS (Global P�…ioning System) Daemon Sockets.
    [  OK  ] Listening on CUPS Scheduler.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Started CUPS Scheduler.
    [  OK  ] Reached target Paths.
    [  OK  ] Reached target Basic System.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting dphys-swapfile - �…unt, and delete a swap file...
             Starting Modem Manager...
             Starting System Logging Service...
             Starting Disk Manager...
             Starting Login Service...
             Starting dhcpcd on all interfaces...
             Starting LSB: Switch to on�…nless shift key is pressed)...
    [  OK  ] Started tof-server.service.
    [  OK  ] Started D-Bus System Message Bus.
             Starting WPA supplicant...
             Starting triggerhappy global hotkey daemon...
    [  OK  ] Started CUPS Scheduler.
             Starting Check for Raspberry Pi EEPROM updates...
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Reached target Timers.
             Starting rng-tools.service...
    [  OK  ] Started Regular background program processing daemon.
    [  OK  ] Started System Logging Service.
    [  OK  ] Started triggerhappy global hotkey daemon.
    [FAILED] Failed to start rng-tools.service.
    See 'systemctl status rng-tools.service' for details.
    [  OK  ] Started Check for Raspberry Pi EEPROM updates.
    [  OK  ] Started dhcpcd on all interfaces.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started Login Service.
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started dphys-swapfile - s�…mount, and delete a swap file.
             Starting Authorization Manager...
    [  OK  ] Reached target Network.
    [  OK  ] Started IIO Daemon.
             Starting HTTP based time synchronization tool...
             Starting /etc/rc.local Compatibility...
             Starting OpenBSD Secure Shell server...
             Starting Permit User Sessions...
    [  OK  ] Started Make remote CUPS printers available locally.
    [  OK  ] Started /etc/rc.local Compatibility.
             Starting Manage, Install and Generate Color Profiles...
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started HTTP based time synchronization tool.
             Starting Light Display Manager...
             Starting Hold until boot process finishes up...
    [  OK  ] Started OpenBSD Secure Shell server.
    [  OK  ] Started Manage, Install and Generate Color Profiles.
    [  OK  ] Started Authorization Manager.
    [  OK  ] Started LSB: Switch to ond�…(unless shift key is pressed).
    [  OK  ] Started Modem Manager.
    
    Raspbian GNU/Linux 10 analog ttyPS0
    
    analog login: root (automatic login)
    
    Last login: Wed Feb 24 01:17:53 GMT 2021 on ttyPS0
    Linux analog 4.19.0-ga6ef26d #1104 SMP PREEMPT Fri Feb 19 15:59:18 GMT 2021 armv7l
    
    The programs included with the Debian GNU/Linux system are free software;
    the exact distribution terms for each program are described in the
    individual files in /usr/share/doc/*/copyright.
    
    Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
    permitted by applicable law.
    root@analog:~# 
    

    -Michael