Setup ADRV9364-Z7020 with ADRV1CRR-FMC using MATLAB

Matlab has the whole instructions on how to setup the radio using Communication Toolbox for Zynq , I followed the procedure. But I have a doubt on switch configuration. I am trying to boot using SD card.I have tried with S1,S3,S4 On(position away from dot on switch). For some reason the LED DS3 which should've blinked suggesting successful boot, isn't happening. I even did a carrier rest according to the procedure and waited at least 5mins but it didn't work.

D3,D4 LED are ON continuously. 

I just took a random SD card and Matlab downloaded some files onto it, Is there anything I am missing? I am a rookie in the field, any help would be great. 

And is there any jumper setting? Currently all are open



V1
[edited by: Sumanth_Raikar at 6:30 AM (GMT -4) on 26 Jul 2021]

Top Replies