ZCU102 + adrv9002, TES Connection Failure

Hello,

I am trying to setup Linux environment.

[Hardware]

    ZCU102 Revision 1.1

    ADRV9002BBCZ NP/W1=0.03-3GHz

[Software]

23 February 2021 release candidate (2019_R2)
        image was copied from E:\zynqmp-common\image

        system.dtb was copied  E:\zynqmp-zcu102-rev10-adrv9002\zynqmp-zcu102-rev10-adrv9002\system.dtb

        BOOT.BIN was copyed  E:\zynqmp-zcu102-rev10-adrv9002\boot_bin_LVDS\BOOT.bin

[Windows PC]

Windows 10

TES : Arg Navis -0.16.0

[Question]

IP address of Windows 10: 192.168.11.3 (Static IP address)

IP address of ZCU102 : 192.168.11.2(static IP address)

When I clicked [connect] on TES, I got the Connection Failure error. 

It is very helpful if you can give me advice to solve this issue. 

When I ran IIO Osilloscope on Windows 10, I confirm that IIO Osilloscope can connect with ZCU102 correctly.

Best regards,

H.Kashima