adrv9002 + zcu102

I trying start adrv9002 on zcu102. Everything according to the guide https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp , but i have errors

[   12.939028] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/                                                                                                                             adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_Cmd_Write, in line  767, variable name devi                                                                                                                             ce.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
[   12.939028]
[   12.966487] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/                                                                                                                             adrv9001/public/src/adi_adrv9001_gpio.c, in function adi_adrv9001_gpio_ControlInit_Configure, in line  393, variable name NULL.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
[   12.966487]
[   12.994981] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/                                                                                                                             adrv9001/public/src/adi_adrv9001_utilities.c, in function adi_adrv9001_Utilities_InitRadio_Load, in line  1512, variable name NULL.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
[   12.994981]
[   13.023816] adrv9002 spi1.0: adrv9002_setup, 1906: failed with "ARM Mailbox Busy. Command not executed in Arm                                                                                                                             CmdWrite()" (3)
[   13.035048] adrv9002: probe of spi1.0 failed with error -14



1
[edited by: Burning_man at 8:43 AM (GMT -4) on 18 May 2021]
  • 0
    •  Analog Employees 
    on May 18, 2021 8:52 AM

    Hello, 

    please can you check what version of the board you have based on this: https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart#identify_your_hardware

    Thank you, 

    Laszlo

  • 0
    •  Analog Employees 
    on May 18, 2021 10:23 AM in reply to Burning_man

    please could you share also a complete  dmesg output. 

    Thank you

    Laszlo

  • Xilinx Zynq MP First Stage Boot Loader
    Release 2019.1   Jun 12 2020  -  15:24:33
    NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
    NOTICE:  BL31: Secure code at 0x0
    NOTICE:  BL31: Non secure code at 0x8000000
    NOTICE:  BL31: v2.0(release):xilinx-v2019.2
    NOTICE:  BL31: Built : 10:19:24, Jan 13 2020
    PMUFW:  v1.1


    U-Boot 2018.01-21436-gbba91bc203 (Jan 13 2020 - 10:50:58 +0200) Xilinx ZynqMP ZCU102 rev1.0, Build: jenkins-development-build_uboot-1

    I2C:   ready
    DRAM:  4 GiB
    EL Level:       EL2
    Chip ID:        zu9eg
    MMC:   sdhci@ff170000: 0 (SD)
    *** Warning - bad CRC, using default environment

    In:    serial@ff000000
    Out:   serial@ff000000
    Err:   serial@ff000000
    Bootmode: LVL_SHFT_SD_MODE1
    Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

    Warning: ethernet@ff0e0000 using MAC address from ROM
    eth0: ethernet@ff0e0000
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc0 is current device
    Device: sdhci@ff170000
    Manufacturer ID: 41
    OEM: 3432
    Name: SD16G
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 14.5 GiB
    Bus Width: 4-bit
    Erase Group Size: 512 Bytes
    reading uEnv.txt
    392 bytes read in 12 ms (31.3 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from SD ...
    Running uenvcmd ...
    Copying Linux from SD to RAM...
    ** No boot file defined **
    reading system.dtb
    42007 bytes read in 20 ms (2 MiB/s)
    reading Image
    32354816 bytes read in 2133 ms (14.5 MiB/s)
    ## Flattened Device Tree blob at 04000000
       Booting using the fdt blob at 0x4000000
       Loading Device Tree to 000000000fff2000, end 000000000ffff416 ... OK

    Starting kernel ...

    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 4.19.0-29506-g6374347742fc (nunojsa@nunojsa-N551JK) (gcc version 8.4.0 (Ubuntu/Linaro 8.4.0-3ubuntu1)) #84 SMP Fri Jun 19 14:16:29 CEST 2020
    [    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] psci: SMC Calling Convention v1.1
    [    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
    [    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Speculative Store Bypass Disable mitigation not required
    [    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
    [    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
    [    0.000000] Memory: 3769828K/4194304K available (14844K kernel code, 1452K rwdata, 14436K rodata, 832K init, 329K bss, 162332K reserved, 262144K cma-reserved)
    [    0.000000] rcu: Hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
    [    0.000004] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
    [    0.008243] Console: colour dummy device 80x25
    [    0.012392] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
    [    0.022757] pid_max: default: 32768 minimum: 301
    [    0.027449] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.034012] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.041796] ASID allocator initialised with 32768 entries
    [    0.046510] rcu: Hierarchical SRCU implementation.
    [    0.051535] EFI services will not be available.
    [    0.055829] smp: Bringing up secondary CPUs ...
    [    0.060488] Detected VIPT I-cache on CPU1
    [    0.060517] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.060822] Detected VIPT I-cache on CPU2
    [    0.060841] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.061128] Detected VIPT I-cache on CPU3
    [    0.061147] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.061191] smp: Brought up 1 node, 4 CPUs
    [    0.095682] SMP: Total of 4 processors activated.
    [    0.100355] CPU features: detected: 32-bit EL0 Support
    [    0.106878] CPU: All CPU(s) started at EL2
    [    0.109535] alternatives: patching kernel code
    [    0.114851] devtmpfs: initialized
    [    0.122368] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.126921] futex hash table entries: 1024 (order: 4, 65536 bytes)
    [    0.138635] xor: measuring software checksum speed
    [    0.177130]    8regs     :  2374.000 MB/sec
    [    0.217158]    8regs_prefetch:  2051.000 MB/sec
    [    0.257190]    32regs    :  2724.000 MB/sec
    [    0.297220]    32regs_prefetch:  2308.000 MB/sec
    [    0.297261] xor: using function: 32regs (2724.000 MB/sec)
    [    0.301571] pinctrl core: initialized pinctrl subsystem
    [    0.307377] NET: Registered protocol family 16
    [    0.311532] audit: initializing netlink subsys (disabled)
    [    0.316600] audit: type=2000 audit(0.268:1): state=initialized audit_enabled=0 res=1
    [    0.324230] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
    [    0.324235] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.338986] DMA: preallocated 256 KiB pool for atomic allocations
    [    0.357475] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.426922] raid6: int64x1  gen()   444 MB/s
    [    0.494950] raid6: int64x1  xor()   451 MB/s
    [    0.562998] raid6: int64x2  gen()   680 MB/s
    [    0.631045] raid6: int64x2  xor()   599 MB/s
    [    0.699104] raid6: int64x4  gen()   981 MB/s
    [    0.767153] raid6: int64x4  xor()   737 MB/s
    [    0.835194] raid6: int64x8  gen()  1162 MB/s
    [    0.903228] raid6: int64x8  xor()   759 MB/s
    [    0.971307] raid6: neonx1   gen()   735 MB/s
    [    1.039324] raid6: neonx1   xor()   880 MB/s
    [    1.107390] raid6: neonx2   gen()  1128 MB/s
    [    1.175407] raid6: neonx2   xor()  1173 MB/s
    [    1.243485] raid6: neonx4   gen()  1479 MB/s
    [    1.311509] raid6: neonx4   xor()  1418 MB/s
    [    1.379574] raid6: neonx8   gen()  1554 MB/s
    [    1.447606] raid6: neonx8   xor()  1459 MB/s
    [    1.447644] raid6: using algorithm neonx8 gen() 1554 MB/s
    [    1.451601] raid6: .... xor() 1459 MB/s, rmw enabled
    [    1.456532] raid6: using neon recovery algorithm
    [    1.461766] SCSI subsystem initialized
    [    1.465011] usbcore: registered new interface driver usbfs
    [    1.470317] usbcore: registered new interface driver hub
    [    1.475595] usbcore: registered new device driver usb
    [    1.480641] media: Linux media interface: v0.10
    [    1.485102] videodev: Linux video capture interface: v2.00
    [    1.490579] pps_core: LinuxPPS API ver. 1 registered
    [    1.495462] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    1.504556] PTP clock support registered
    [    1.508454] EDAC MC: Ver: 3.0.0
    [    1.511949] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
    [    1.519226] jesd204: found 0 devices and 0 topologies
    [    1.523871] FPGA manager framework
    [    1.527381] Advanced Linux Sound Architecture Driver Initialized.
    [    1.533539] Bluetooth: Core ver 2.22
    [    1.536830] NET: Registered protocol family 31
    [    1.541225] Bluetooth: HCI device and connection manager initialized
    [    1.547542] Bluetooth: HCI socket layer initialized
    [    1.552385] Bluetooth: L2CAP socket layer initialized
    [    1.557413] Bluetooth: SCO socket layer initialized
    [    1.562721] clocksource: Switched to clocksource arch_sys_counter
    [    1.568385] VFS: Disk quotas dquot_6.6.0
    [    1.572234] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    1.583323] NET: Registered protocol family 2
    [    1.583708] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
    [    1.591192] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
    [    1.598520] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
    [    1.605297] TCP: Hash tables configured (established 32768 bind 32768)
    [    1.611445] UDP hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.617426] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.623908] NET: Registered protocol family 1
    [    1.628289] RPC: Registered named UNIX socket transport module.
    [    1.633967] RPC: Registered udp transport module.
    [    1.638634] RPC: Registered tcp transport module.
    [    1.643306] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    1.650441] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    1.656946] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [    1.665331] Initialise system trusted keyrings
    [    1.668976] workingset: timestamp_bits=62 max_order=20 bucket_order=0
    [    1.675988] NFS: Registering the id_resolver key type
    [    1.680343] Key type id_resolver registered
    [    1.684483] Key type id_legacy registered
    [    1.688468] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    1.695135] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    [    2.782169] NET: Registered protocol family 38
    [    2.842276] Key type asymmetric registered
    [    2.842314] Asymmetric key parser 'x509' registered
    [    2.845610] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
    [    2.852933] io scheduler noop registered
    [    2.856823] io scheduler deadline registered
    [    2.861081] io scheduler cfq registered (default)
    [    2.865734] io scheduler mq-deadline registered
    [    2.870232] io scheduler kyber registered
    [    2.902142] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [    2.906049] cacheinfo: Unable to detect cache hierarchy for CPU 0
    [    2.913439] brd: module loaded
    [    2.917330] loop: module loaded
    [    2.917546] Registered mathworks_ip class
    [    2.919817] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    2.926896] libphy: Fixed MDIO Bus: probed
    [    2.930750] tun: Universal TUN/TAP device driver, 1.6
    [    2.934627] CAN device driver interface
    [    2.939206] usbcore: registered new interface driver asix
    [    2.943726] usbcore: registered new interface driver ax88179_178a
    [    2.949765] usbcore: registered new interface driver cdc_ether
    [    2.955560] usbcore: registered new interface driver net1080
    [    2.961186] usbcore: registered new interface driver cdc_subset
    [    2.967066] usbcore: registered new interface driver zaurus
    [    2.972611] usbcore: registered new interface driver cdc_ncm
    [    2.978892] usbcore: registered new interface driver uas
    [    2.983514] usbcore: registered new interface driver usb-storage
    [    2.989509] usbcore: registered new interface driver upd78f0730
    [    2.995350] usbserial: USB Serial support registered for upd78f0730
    [    3.002261] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
    [    3.008795] i2c /dev entries driver
    [    3.014077] usbcore: registered new interface driver uvcvideo
    [    3.017912] USB Video Class driver (1.1.1)
    [    3.023308] Bluetooth: HCI UART driver ver 2.3
    [    3.026385] Bluetooth: HCI UART protocol H4 registered
    [    3.031498] Bluetooth: HCI UART protocol BCSP registered
    [    3.036795] Bluetooth: HCI UART protocol LL registered
    [    3.041874] Bluetooth: HCI UART protocol ATH3K registered
    [    3.047254] Bluetooth: HCI UART protocol Three-wire (H5) registered
    [    3.053506] Bluetooth: HCI UART protocol Intel registered
    [    3.058846] Bluetooth: HCI UART protocol QCA registered
    [    3.064055] usbcore: registered new interface driver bcm203x
    [    3.069669] usbcore: registered new interface driver bpa10x
    [    3.075206] usbcore: registered new interface driver bfusb
    [    3.080658] usbcore: registered new interface driver btusb
    [    3.086080] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
    [    3.091746] usbcore: registered new interface driver ath3k
    [    3.097273] EDAC MC: ECC not enabled
    [    3.100949] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [    3.113131] CPUidle arm: Failed to register cpuidle driver
    [    3.118422] sdhci: Secure Digital Host Controller Interface driver
    [    3.124403] sdhci: Copyright(c) Pierre Ossman
    [    3.128727] sdhci-pltfm: SDHCI platform and OF driver helper
    [    3.134732] ledtrig-cpu: registered to indicate activity on CPUs
    [    3.140363] zynqmp_firmware_probe Platform Management API v1.1
    [    3.146119] zynqmp_firmware_probe Trustzone version v1.0
    [    3.154208] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
    [    3.181445] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
    [    3.184148] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
    [    3.189264] zynqmp_aes zynqmp_aes: AES Successfully Registered
    [    3.189264]
    [    3.196778] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
    [    3.202913] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    3.208499] usbcore: registered new interface driver usbhid
    [    3.213819] usbhid: USB HID core driver
    [    3.224079] axi_sysid 85000000.axi-sysid-0: [adrv9001] on [zcu102] git <4af529a57af7acda0a2971601e189df3f01628a5> clean [2020-06-12 14:04:04] UTC
    [    3.231796] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [    3.238351] usbcore: registered new interface driver snd-usb-audio
    [    3.245683] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [    3.251922] Initializing XFRM netlink socket
    [    3.255834] NET: Registered protocol family 10
    [    3.260556] Segment Routing with IPv6
    [    3.263890] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    3.270035] NET: Registered protocol family 17
    [    3.274108] NET: Registered protocol family 15
    [    3.278520] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [    3.291437] can: controller area network core (rev 20170425 abi 9)
    [    3.297569] NET: Registered protocol family 29
    [    3.301955] can: raw protocol (rev 20170425)
    [    3.306192] can: broadcast manager protocol (rev 20170425 t)
    [    3.311817] can: netlink gateway (rev 20170425) max_hops=1
    [    3.317325] Bluetooth: RFCOMM TTY layer initialized
    [    3.322116] Bluetooth: RFCOMM socket layer initialized
    [    3.327236] Bluetooth: RFCOMM ver 1.11
    [    3.330938] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    3.336210] Bluetooth: BNEP filters: protocol multicast
    [    3.341402] Bluetooth: BNEP socket layer initialized
    [    3.346332] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    3.352215] Bluetooth: HIDP socket layer initialized
    [    3.357283] 9pnet: Installing 9P2000 support
    [    3.361393] NET: Registered protocol family 36
    [    3.365808] Key type dns_resolver registered
    [    3.370535] registered taskstats version 1
    [    3.374133] Loading compiled-in X.509 certificates
    [    3.379182] Btrfs loaded, crc32c=crc32c-generic
    ▒▒r▒▒º▒▒console [ttyPS0] enabledttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
    [    3.398732] console [ttyPS0] enabled
    [    3.402324] bootconsole [cdns0] disabled
    [    3.402324] bootconsole [cdns0] disabled
    [    3.410442] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps
    [    3.423552] GPIO line 130 (output_enable) hogged as output/high
    [    3.429721] of-fpga-region fpga-full: FPGA Region probed
    [    3.435565] nwl-pcie fd0e0000.pcie: Link is DOWN
    [    3.440215] nwl-pcie fd0e0000.pcie: host bridge /amba/pcie@fd0e0000 ranges:
    [    3.447190] nwl-pcie fd0e0000.pcie:   MEM 0xe0000000..0xefffffff -> 0xe0000000
    [    3.454411] nwl-pcie fd0e0000.pcie:   MEM 0x600000000..0x7ffffffff -> 0x600000000
    [    3.461994] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
    [    3.468169] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    3.473655] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
    [    3.480527] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
    [    3.492143] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
    [    3.498309] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
    [    3.504887] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
    [    3.511993] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
    [    3.519098] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
    [    3.526204] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
    [    3.533306] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
    [    3.540404] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
    [    3.547507] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
    [    3.554606] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
    [    3.561843] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
    [    3.573087] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
    [    3.581761] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
    [    3.592512] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
    [    3.600579] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
    [    3.608998] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.621440] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.634111] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
    [    3.644295] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
    [    3.651311] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    3.657919] [drm] No driver support for vblank timestamp query.
    [    3.663906] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008fc2930)
    [    4.750730] [drm] Cannot find any crtc or sizes
    [    4.755486] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
    [    4.763586] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
    [    4.772544] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
    [    4.790486] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
    [    4.799442] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
    [    4.809821] scsi host0: ahci-ceva
    [    4.813384] scsi host1: ahci-ceva
    [    4.816839] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
    [    4.824752] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
    [    4.833901] API_LOG:adi_adrv9001_HwReset(...)
    [    4.839275] API_LOG:adi_adrv9001_spi_Configure(...)
    [    4.844252] API_LOG:adi_adrv9001_spi_Verify(...)
    [    4.869450] random: fast init done
    [    5.145003] ata2: SATA link down (SStatus 0 SControl 330)
    [    5.150417] ata1: SATA link down (SStatus 0 SControl 330)
    [    5.834734] [drm] Cannot find any crtc or sizes
    [   12.983178] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_Cmd_Write, in line  767, variable name device.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
    [   12.983178]
    [   13.010634] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_gpio.c, in function adi_adrv9001_gpio_ControlInit_Configure, in line  393, variable name NULL.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
    [   13.010634]
    [   13.039121] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_utilities.c, in function adi_adrv9001_Utilities_InitRadio_Load, in line  1512, variable name NULL.Error message ARM Mailbox Busy. Command not executed in ArmCmdWrite().
    [   13.039121]
    [   13.067961] adrv9002 spi1.0: adrv9002_setup, 1906: failed with "ARM Mailbox Busy. Command not executed in ArmCmdWrite()" (3)
    [   13.079191] adrv9002: probe of spi1.0 failed with error -14
    [   13.085537] m25p80 spi0.0: found n25q512a, expected m25p80
    [   13.091298] m25p80 spi0.0: n25q512a (131072 Kbytes)
    [   13.096189] 4 fixed-partitions partitions found on MTD device spi0.0
    [   13.102537] Creating 4 MTD partitions on "spi0.0":
    [   13.107323] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    [   13.113562] 0x000000100000-0x000000600000 : "qspi-linux"
    [   13.119271] 0x000000600000-0x000000620000 : "qspi-device-tree"
    [   13.125502] 0x000000620000-0x000000c00000 : "qspi-rootfs"
    [   13.133387] macb ff0e0000.ethernet: Not enabling partial store and forward
    [   13.140756] libphy: MACB_mii_bus: probed
    [   13.144752] mdio_bus ff0e0000.ethernet-ffffffff: MDIO device at address 21 is missing.
    [   13.154804] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
    [   13.167841] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 22 (00:0a:35:05:2f:96)
    [   13.177965] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
    [   13.184499] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
    [   13.190996] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
    [   13.197484] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
    [   13.205305] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
    [   13.211153] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
    [   13.219388] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [   13.224883] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [   13.232865] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000202010810
    [   13.242271] xhci-hcd xhci-hcd.0.auto: irq 48, io mem 0xfe200000
    [   13.248390] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [   13.256654] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   13.263872] usb usb1: Product: xHCI Host Controller
    [   13.268741] usb usb1: Manufacturer: Linux 4.19.0-29506-g6374347742fc xhci-hcd
    [   13.275868] usb usb1: SerialNumber: xhci-hcd.0.auto
    [   13.281086] hub 1-0:1.0: USB hub found
    [   13.284848] hub 1-0:1.0: 1 port detected
    [   13.288953] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [   13.294437] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
    [   13.302095] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0  SuperSpeed
    [   13.308829] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [   13.317090] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   13.324309] usb usb2: Product: xHCI Host Controller
    [   13.329177] usb usb2: Manufacturer: Linux 4.19.0-29506-g6374347742fc xhci-hcd
    [   13.336304] usb usb2: SerialNumber: xhci-hcd.0.auto
    [   13.341419] hub 2-0:1.0: USB hub found
    [   13.345178] hub 2-0:1.0: 1 port detected
    [   13.350323] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
    [   13.357576] pca953x 0-0020: Linked as a consumer to regulator.0
    [   13.364301] GPIO line 496 (sel0) hogged as output/low
    [   13.369683] GPIO line 497 (sel1) hogged as output/high
    [   13.375150] GPIO line 498 (sel2) hogged as output/high
    [   13.380621] GPIO line 499 (sel3) hogged as output/high
    [   13.385958] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
    [   13.393201] pca953x 0-0021: Linked as a consumer to regulator.0
    [   13.400629] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.407441] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.414252] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.421059] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.427869] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.434678] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.441483] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.448293] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.455119] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.461933] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.468345] i2c i2c-0: Added multiplexed i2c bus 3
    [   13.473828] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
    [   13.480636] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.487442] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.494255] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.501065] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.507879] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.514687] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.521502] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [   13.527905] i2c i2c-0: Added multiplexed i2c bus 4
    [   13.567404] i2c i2c-0: Added multiplexed i2c bus 5
    [   13.572374] i2c i2c-0: Added multiplexed i2c bus 6
    [   13.577162] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
    [   13.584512] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 24
    [   13.592288] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
    [   13.599039] i2c i2c-1: Added multiplexed i2c bus 7
    [   13.604163] i2c i2c-1: Added multiplexed i2c bus 8
    [   13.611074] si570 9-005d: registered, current frequency 300000000 Hz
    [   13.617469] i2c i2c-1: Added multiplexed i2c bus 9
    [   13.636286] si570 10-005d: registered, current frequency 148500000 Hz
    [   13.642774] i2c i2c-1: Added multiplexed i2c bus 10
    [   13.647875] si5324 11-0069: si5328 probed
    [   13.710785] si5324 11-0069: si5328 probe successful
    [   13.715713] i2c i2c-1: Added multiplexed i2c bus 11
    [   13.720757] i2c i2c-1: Added multiplexed i2c bus 12
    [   13.725793] i2c i2c-1: Added multiplexed i2c bus 13
    [   13.730848] i2c i2c-1: Added multiplexed i2c bus 14
    [   13.735725] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
    [   13.743691] i2c i2c-1: Added multiplexed i2c bus 15
    [   13.775425] i2c i2c-1: Added multiplexed i2c bus 16
    [   13.780478] i2c i2c-1: Added multiplexed i2c bus 17
    [   13.785529] i2c i2c-1: Added multiplexed i2c bus 18
    [   13.790574] i2c i2c-1: Added multiplexed i2c bus 19
    [   13.795624] i2c i2c-1: Added multiplexed i2c bus 20
    [   13.800678] i2c i2c-1: Added multiplexed i2c bus 21
    [   13.805733] i2c i2c-1: Added multiplexed i2c bus 22
    [   13.810605] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
    [   13.818217] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 25
    [   13.824562] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
    [   13.864503] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
    [   13.881379] input: gpio-keys as /devices/platform/gpio-keys/input/input0
    [   13.888327] rtc_zynqmp ffa60000.rtc: setting system clock to 2021-05-18 08:33:52 UTC (1621326832)
    [   13.897206] of_cfs_init
    [   13.899716] of_cfs_init: OK
    [   13.902640] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [   13.997000] mmc0: new ultra high speed SDR104 SDHC card at address 0007
    [   14.004110] mmcblk0: mmc0:0007 SD16G 14.5 GiB
    [   14.009771]  mmcblk0: p1 p2 p3
    [   14.042105] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [   14.048720] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13
    [   14.056492] ALSA device list:
    [   14.059456]   #0: DisplayPort monitor
    [   14.063472] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [   14.072083] cfg80211: failed to load regulatory.db
    [   14.130553] random: crng init done
    [   26.261308] EXT4-fs (mmcblk0p2): recovery complete
    [   26.270750] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [   26.278860] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [   26.290142] devtmpfs: mounted
    [   26.293281] Freeing unused kernel memory: 832K
    [   26.297766] Run /sbin/init as init process
    Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory
     * Setting up X socket directories...                                    [ OK ]
     * STARTDISTCC is set to false in /etc/default/distcc
     * /usr/bin/distccd not starting
     * Starting IIO Daemon iiod                                              [ OK ]

    Last login: Tue May 18 07:47:27 UTC 2021 on tty1
    Welcome to Linaro 14.04 (GNU/Linux 4.19.0-29506-g6374347742fc aarch64)

     * Documentation:  https://wiki.analog.com/ https://ez.analog.com/

    root@analog:~#

  • +1
    •  Analog Employees 
    on May 18, 2021 10:57 AM in reply to Burning_man

    Please can you try the latest 2019_r2  image ? https://swdownloads.analog.com/cse/kuiper/2021-02-23-ADI-Kuiper.img.xz

    It looks you are using an older version. 

    Laszlo