ADRV9008-1 supported by which families of Xilinx FPGA

Looking for clarification about which FPGA families will support the JESD204B interface with an ADRV9008-1 receiver.

Obviously, the  XCZU9EG-2FFVB1156 MPSoC works since it is with the ZCU102 board when paired with the ADRV9008 development board.

This document: https://www.analog.com/en/analog-dialogue/articles/quickly-implement-jesd204b.html  implies that the preference is to use FPGAs that have GTH or GTX high speed serial transceiver built in.

Would it work with the GTP transceiver available on the Artix-7 series (assuming the desired ADC data throughput is less than the max supported by GTP)? 

If so, is the penalty just bandwidth and performance (jitter)?

Thanks

Parents Reply Children
  • 0
    •  Analog Employees 
    on May 18, 2021 9:44 AM in reply to boz336

    The GTP transceiver have a maximum rate up to 6.6Gsps and  Artix devices in general have a low number of transceiver banks/pins. Depending on the part, 6.6 GSPS and 2/4 lanes may not be enough to transfer data at the maximum bandwidth supported. If the datarate and available number of lanes are enough for a specific application, I don't see why it wouldn't work. 

    The AC701 development board has only two GTP transceivers populated in the FMC connector.

    Xilinx JESD204B IP supports Artix devices, it's just we don't have a reference design for it and it's not part of the ADI JESD204 Interface Framework (https://wiki.analog.com/resources/fpga/peripherals/jesd204)

    Regards,

    Adrian