Custom board with 2 AD9361 and problem with IODELAY GROUP

Hello, 

My team and I plan to connect our own RF board containing two AD9361 used only for their RX pins to a ZC706 platform. However compared to the FMCOMMS3 board in which each of the AD9361 is connected to a different FMC Connector, we use only one FMC connector. I used the design provided by AD for ZC706, but when I changed the pinouts to match my board (see enf of the post), I have the following error : 

I saw one of the topics that mentionned the patch : ad9361_iodelay_ctrl.patch and I did the modification described in it. But I ended up with this error : 

Can you please help me find a solution ?

Thanks in advance ! 

PS : Here is the pinout I used : 


# constraints
# ad9361

set_property -dict {PACKAGE_PIN AG17 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports h125_p] ; ## H4 FMC_LPC_CLK0_M2C_P
set_property -dict {PACKAGE_PIN AG16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports h125_n] ; ## H5 FMC_LPC_CLK0_M2C_N

set_property -dict {PACKAGE_PIN AE13 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_clk_in_0_p] ; ## G6 FMC_LPC_LA00_CC_P
set_property -dict {PACKAGE_PIN AF13 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_clk_in_0_n] ; ## G7 FMC_LPC_LA00_CC_N
set_property -dict {PACKAGE_PIN AF15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_frame_in_0_p] ; ## D8 FMC_LPC_LA01_CC_P
set_property -dict {PACKAGE_PIN AG15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_frame_in_0_n] ; ## D9 FMC_LPC_LA01_CC_N
set_property -dict {PACKAGE_PIN AE12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[0]] ; ## H7 FMC_LPC_LA02_P
set_property -dict {PACKAGE_PIN AF12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[0]] ; ## H8 FMC_LPC_LA02_N
set_property -dict {PACKAGE_PIN AG12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[1]] ; ## G9 FMC_LPC_LA03_P
set_property -dict {PACKAGE_PIN AH12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[1]] ; ## G10 FMC_LPC_LA03_N
set_property -dict {PACKAGE_PIN AJ15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[2]] ; ## H10 FMC_LPC_LA04_P
set_property -dict {PACKAGE_PIN AK15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[2]] ; ## H11 FMC_LPC_LA04_N
set_property -dict {PACKAGE_PIN AE16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[3]] ; ## D11 FMC_LPC_LA05_P
set_property -dict {PACKAGE_PIN AE15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[3]] ; ## D12 FMC_LPC_LA05_N
set_property -dict {PACKAGE_PIN AB12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[4]] ; ## C10 FMC_LPC_LA06_P
set_property -dict {PACKAGE_PIN AC12 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[4]] ; ## C11 FMC_LPC_LA06_N
set_property -dict {PACKAGE_PIN AA15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_p[5]] ; ## H13 FMC_LPC_LA07_P
set_property -dict {PACKAGE_PIN AA14 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_0_n[5]] ; ## H14 FMC_LPC_LA07_N

set_property -dict {PACKAGE_PIN AD14 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_clk_in_1_p] ; ## G12 FMC_LPC_LA08_P
set_property -dict {PACKAGE_PIN AD13 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_clk_in_1_n] ; ## G13 FMC_LPC_LA08_N
set_property -dict {PACKAGE_PIN AH14 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_frame_in_1_p] ; ## D14 FMC_LPC_LA09_P
set_property -dict {PACKAGE_PIN AH13 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_frame_in_1_n] ; ## D15 FMC_LPC_LA09_N
set_property -dict {PACKAGE_PIN AJ16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[0]] ; ## H16 FMC_LPC_LA11_P
set_property -dict {PACKAGE_PIN AK16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[0]] ; ## H17 FMC_LPC_LA11_N
set_property -dict {PACKAGE_PIN AD16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[1]] ; ## G15 FMC_LPC_LA12_P
set_property -dict {PACKAGE_PIN AD15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[1]] ; ## G16 FMC_LPC_LA12_N
set_property -dict {PACKAGE_PIN AH17 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[2]] ; ## D17 FMC_LPC_LA13_P
set_property -dict {PACKAGE_PIN AH16 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[2]] ; ## D18 FMC_LPC_LA13_N
set_property -dict {PACKAGE_PIN AC14 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[4]] ; ## C14 FMC_LPC_LA10_P
set_property -dict {PACKAGE_PIN AC13 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[4]] ; ## C15 FMC_LPC_LA10_N
set_property -dict {PACKAGE_PIN AF18 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[3]] ; ## C18 FMC_LPC_LA14_P
set_property -dict {PACKAGE_PIN AF17 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[3]] ; ## C19 FMC_LPC_LA14_N
set_property -dict {PACKAGE_PIN AB15 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_p[5]] ; ## H19 FMC_LPC_LA15_P
set_property -dict {PACKAGE_PIN AB14 IOSTANDARD LVDS_25 DIFF_TERM TRUE} [get_ports rx_data_in_1_n[5]] ; ## H20 FMC_LPC_LA15_N
set_property -dict {PACKAGE_PIN AE18 IOSTANDARD LVCMOS25} [get_ports enable_0] ; ## G18 FMC_LPC_LA16_P
set_property -dict {PACKAGE_PIN AF27 IOSTANDARD LVCMOS25} [get_ports enable_1] ; ## C23 FMC_LPC_LA18_CC_N
set_property -dict {PACKAGE_PIN AE17 IOSTANDARD LVCMOS25} [get_ports txnrx_0] ; ## G19 FMC_LPC_LA16_N
set_property -dict {PACKAGE_PIN AF29 IOSTANDARD LVCMOS25} [get_ports txnrx_1] ; ## G27 FMC_LPC_LA25_P

set_property -dict {PACKAGE_PIN AG26 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_0[0]] ; ## G21 FMC_LPC_LA20_P
set_property -dict {PACKAGE_PIN AG27 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_0[1]] ; ## G22 FMC_LPC_LA20_N
set_property -dict {PACKAGE_PIN AH28 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_0[2]] ; ## H25 FMC_LPC_LA21_P
set_property -dict {PACKAGE_PIN AH29 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_0[3]] ; ## H26 FMC_LPC_LA21_N
set_property -dict {PACKAGE_PIN AK27 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_1[0]] ; ## G24 FMC_LPC_LA22_P
set_property -dict {PACKAGE_PIN AK28 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_1[1]] ; ## G25 FMC_LPC_LA22_N
set_property -dict {PACKAGE_PIN AJ26 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_1[2]] ; ## D23 FMC_LPC_LA23_P
set_property -dict {PACKAGE_PIN AK26 IOSTANDARD LVCMOS25} [get_ports gpio_ctl_1[3]] ; ## D24 FMC_LPC_LA23_N

set_property -dict {PACKAGE_PIN AH27 IOSTANDARD LVCMOS25} [get_ports gpio_sync] ; ## H23 FMC_LPC_LA19_N
set_property -dict {PACKAGE_PIN AD25 IOSTANDARD LVCMOS25} [get_ports gpio_resetb_0] ; ## H31 FMC_LPC_LA28_P

set_property -dict {PACKAGE_PIN AJ30 IOSTANDARD LVCMOS25 PULLTYPE PULLUP} [get_ports spi_ad9361_0] ; ## D26 FMC_LPC_LA26_P
set_property -dict {PACKAGE_PIN AE27 IOSTANDARD LVCMOS25 PULLTYPE PULLUP} [get_ports spi_ad9361_1] ; ## C22 FMC_LPC_LA18_CC_N
set_property -dict {PACKAGE_PIN AK30 IOSTANDARD LVCMOS25} [get_ports spi_clk] ; ## D27 FMC_LPC_LA26_N
set_property -dict {PACKAGE_PIN AJ28 IOSTANDARD LVCMOS25} [get_ports spi_mosi] ; ## C26 FMC_LPC_LA27_P
set_property -dict {PACKAGE_PIN AJ29 IOSTANDARD LVCMOS25} [get_ports spi_miso] ; ## C27 FMC_LPC_LA27_N


# clocks


create_clock -name rx_0_clk -period 4.00 [get_ports rx_clk_in_0_p]
create_clock -name rx_1_clk -period 4.00 [get_ports rx_clk_in_1_p]
create_clock -name ad9361_clk -period 4.00 [get_pins i_system_wrapper/system_i/axi_ad9361_0/clk]

Parents Reply Children
No Data