Post Go back to editing

ADRV9009-ZU11EG Multi-SOM usage: "Device or resource busy"

I have successfully been running multiple ADRV9009-ZU11EG SOMs following the guide here:

https://wiki.analog.com/resources/eval/user-guides/adrv9009-zu11eg/syncronization

Recently I saw that new boot files had been posted to that page, so I sought to update my system.  I installed the 4 files to each of my SOMs, and have not been able to get them to run.

When I try to connect to my SOMs, this is the error that results:

--Connecting to devices
Traceback (most recent call last):
  File "./BeamsGui.py", line 78, in <module>
    multi.primary.trx_lo = freq_lo
  File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/adrv9009.py", line 225, in trx_lo
    self._set_iio_attr("altvoltage0", "frequency", True, value)
  File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/attribute.py", line 86, in _set_iio_attr
    raise ex
  File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/attribute.py", line 84, in _set_iio_attr
    channel.attrs[attr_name].value = str(value)
  File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 707, in <lambda>
    lambda self, x: self._write(x),
  File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 739, in _write
    _c_write_attr(self._channel, self._name_ascii, value.encode("ascii"))
  File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 70, in _check_negative
    raise OSError(-result, _strerror(-result))
OSError: [Errno 16] Device or resource busy

I have tried loading a fresh SD card, with a new Ubuntu installation running pyadi-iio, and receive the same error.

Any suggestions?

Parents Reply Children
  • freq_lo is set to 2400000000

    I tried adrv9009_som_sync.py (changing the ip address) with the same results.

    Should I still be using the "multi-som-adrv9009" branch of pyadi-iio, or has that been rolled into master?

    I've tried both.

  • Use master.

    Does this work:

    import adi

    sdr = adi.adrv9009(<uri>)

    sdr.trx_lo = 2400000000

    -Travis

  • It doesn't:

    ubuntu@ubuntu:~$ python3
    Python 3.8.5 (default, Jul 28 2020, 12:59:40)
    [GCC 9.3.0] on linux
    Type "help", "copyright", "credits" or "license" for more information.
    >>> import adi
    >>> sdr=adi.adrv9009("ip:192.168.1.131")
    >>> sdr.trx_lo=2400000000
    Traceback (most recent call last):
      File "<stdin>", line 1, in <module>
      File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/adrv9009.py", line 225, in trx_lo
        self._set_iio_attr("altvoltage0", "frequency", True, value)
      File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/attribute.py", line 86, in _set_iio_attr
        raise ex
      File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/attribute.py", line 84, in _set_iio_attr
        channel.attrs[attr_name].value = str(value)
      File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 707, in <lambda>
        lambda self, x: self._write(x),
      File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 739, in _write
        _c_write_attr(self._channel, self._name_ascii, value.encode("ascii"))
      File "/home/ubuntu/.local/lib/python3.8/site-packages/iio.py", line 70, in _check_negative
        raise OSError(-result, _strerror(-result))
    OSError: [Errno 16] Device or resource busy
    >>>

  • Ok that means that the chip has not booted correctly. It's not a python issue. Can you provide the output of dmesg?

    -Travis

  • I just tried using the BOOT.BIN, Image, system.dtb, and uEnv.txt files from here:

    wiki.analog.com/.../quick-start-guide

    and your commands work without issue.

    However, I'm trying to run a multi-som configuration, following the guide here:

    https://wiki.analog.com/resources/eval/user-guides/adrv9009-zu11eg/syncronization

    and when i use the BOOT.BIN, Image, system.dtb, and uEnv.txt files from there is when my error occurs.

    But here's the output of dmesg when I run with the "bad" files installed (from the syncronization page):

    root@analog:~# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 4.19.0-76513-g94ad18a0619b-dirty (michael@mhenneri-D06) (gcc version 8.2.0 (GCC)) #1501 SMP Wed Nov 4 11:11:36 CET 2020
    [    0.000000] Machine model: Analog Devices ADRV9009-ZU11EG Rev.B
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
    [    0.000000] On node 0 totalpages: 1048576
    [    0.000000]   DMA32 zone: 7168 pages used for memmap
    [    0.000000]   DMA32 zone: 0 pages reserved
    [    0.000000]   DMA32 zone: 524288 pages, LIFO batch:63
    [    0.000000]   Normal zone: 7168 pages used for memmap
    [    0.000000]   Normal zone: 524288 pages, LIFO batch:63
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] psci: SMC Calling Convention v1.1
    [    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
    [    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
    [    0.000000] pcpu-alloc: s52504 r8192 d29416 u90112 alloc=22*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Speculative Store Bypass Disable mitigation not required
    [    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
    [    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
    [    0.000000] Memory: 3772784K/4194304K available (12604K kernel code, 1524K rwdata, 13324K rodata, 832K init, 326K bss, 159376K reserved, 262144K cma-reserved)
    [    0.000000] rcu: Hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b0074340, max_idle_ns: 440795202884 ns
    [    0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255543ns
    [    0.008241] Console: colour dummy device 80x25
    [    0.012389] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133332)
    [    0.022667] pid_max: default: 32768 minimum: 301
    [    0.027350] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.033921] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.041629] ASID allocator initialised with 32768 entries
    [    0.046414] rcu: Hierarchical SRCU implementation.
    [    0.051426] EFI services will not be available.
    [    0.055726] smp: Bringing up secondary CPUs ...
    [    0.060368] Detected VIPT I-cache on CPU1
    [    0.060395] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.060668] Detected VIPT I-cache on CPU2
    [    0.060686] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.060943] Detected VIPT I-cache on CPU3
    [    0.060961] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.061000] smp: Brought up 1 node, 4 CPUs
    [    0.095586] SMP: Total of 4 processors activated.
    [    0.100259] CPU features: detected: 32-bit EL0 Support
    [    0.106679] CPU: All CPU(s) started at EL2
    [    0.109436] alternatives: patching kernel code
    [    0.114676] devtmpfs: initialized
    [    0.125266] Registered cp15_barrier emulation handler
    [    0.125316] Registered setend emulation handler
    [    0.129285] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.138872] futex hash table entries: 1024 (order: 4, 65536 bytes)
    [    0.150001] xor: measuring software checksum speed
    [    0.189069]    8regs     :  2639.000 MB/sec
    [    0.229094]    8regs_prefetch:  2280.000 MB/sec
    [    0.269120]    32regs    :  3027.000 MB/sec
    [    0.309146]    32regs_prefetch:  2565.000 MB/sec
    [    0.309186] xor: using function: 32regs (3027.000 MB/sec)
    [    0.313487] pinctrl core: initialized pinctrl subsystem
    [    0.319215] NET: Registered protocol family 16
    [    0.323418] audit: initializing netlink subsys (disabled)
    [    0.328506] audit: type=2000 audit(0.272:1): state=initialized audit_enabled=0 res=1
    [    0.336146] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
    [    0.336151] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.350845] DMA: preallocated 256 KiB pool for atomic allocations
    [    0.367905] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.434902] raid6: int64x1  gen()   493 MB/s
    [    0.502859] raid6: int64x1  xor()   501 MB/s
    [    0.570921] raid6: int64x2  gen()   754 MB/s
    [    0.638930] raid6: int64x2  xor()   666 MB/s
    [    0.706961] raid6: int64x4  gen()  1089 MB/s
    [    0.774986] raid6: int64x4  xor()   819 MB/s
    [    0.843029] raid6: int64x8  gen()  1291 MB/s
    [    0.911089] raid6: int64x8  xor()   842 MB/s
    [    0.979143] raid6: neonx1   gen()   817 MB/s
    [    1.047182] raid6: neonx1   xor()   979 MB/s
    [    1.115228] raid6: neonx2   gen()  1255 MB/s
    [    1.183244] raid6: neonx2   xor()  1304 MB/s
    [    1.251283] raid6: neonx4   gen()  1643 MB/s
    [    1.319333] raid6: neonx4   xor()  1577 MB/s
    [    1.387363] raid6: neonx8   gen()  1728 MB/s
    [    1.455419] raid6: neonx8   xor()  1622 MB/s
    [    1.455456] raid6: using algorithm neonx8 gen() 1728 MB/s
    [    1.459411] raid6: .... xor() 1622 MB/s, rmw enabled
    [    1.464341] raid6: using neon recovery algorithm
    [    1.469787] SCSI subsystem initialized
    [    1.472675] libata version 3.00 loaded.
    [    1.472801] usbcore: registered new interface driver usbfs
    [    1.478179] usbcore: registered new interface driver hub
    [    1.483411] usbcore: registered new device driver usb
    [    1.488443] media: Linux media interface: v0.10
    [    1.492908] videodev: Linux video capture interface: v2.00
    [    1.498380] pps_core: LinuxPPS API ver. 1 registered
    [    1.503267] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    1.512358] PTP clock support registered
    [    1.516257] EDAC MC: Ver: 3.0.0
    [    1.519708] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
    [    1.526965] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'clk_sync_stage1'
    [    1.534410] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'clk_sync_stage2'
    [    1.542193] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'clk_sync_stage3'
    [    1.549977] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'link_setup'
    [    1.557330] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'opt_setup_stage1'
    [    1.565201] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'opt_setup_stage2'
    [    1.573073] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'opt_setup_stage3'
    [    1.580944] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'opt_setup_stage4'
    [    1.588816] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'opt_setup_stage5'
    [    1.596688] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'clocks_enable'
    [    1.604299] jesd204: /amba/spi@ff040000/adrv9009-phy@0: stop state: 'link_enable'
    [    1.611988] jesd204: created con: id=0, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@84a30000 <-> /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000
    [    1.623942] jesd204: created con: id=1, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@84a20000 <-> /fpga-axi@0/axi-jesd204-tx@84a30000
    [    1.635620] jesd204: created con: id=2, topo=0, link=0, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-tx@84a20000
    [    1.646691] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcvr-rx-os@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84a70000
    [    1.658629] jesd204: created con: id=4, topo=0, link=2, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-rx-os@84a60000
    [    1.669960] jesd204: created con: id=5, topo=0, link=1, /fpga-axi@0/axi-adxcvr-rx@84a40000 <-> /fpga-axi@0/axi-jesd204-rx@84a50000
    [    1.681638] jesd204: created con: id=6, topo=0, link=1, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-rx@84a40000
    [    1.692713] jesd204: created con: id=7, topo=0, link=1, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff050000/hmc7044-fmc@2
    [    1.703954] jesd204: created con: id=8, topo=0, link=2, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff050000/hmc7044-fmc@2
    [    1.715200] jesd204: created con: id=9, topo=0, link=0, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff050000/hmc7044-fmc@2
    [    1.726459] jesd204: created con: id=10, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@84a50000 <-> /amba/spi@ff050000/adrv9009-phy-d@1
    [    1.738303] jesd204: created con: id=11, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx@84a70000 <-> /amba/spi@ff050000/adrv9009-phy-d@1
    [    1.750153] jesd204: created con: id=12, topo=0, link=0, /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000 <-> /amba/spi@ff050000/adrv9009-phy-d@1
    [    1.762472] jesd204: created con: id=13, topo=0, link=1, /amba/spi@ff050000/adrv9009-phy-d@1 <-> /amba/spi@ff050000/adrv9009-phy-c@0
    [    1.774302] jesd204: created con: id=14, topo=0, link=2, /amba/spi@ff050000/adrv9009-phy-d@1 <-> /amba/spi@ff050000/adrv9009-phy-c@0
    [    1.786158] jesd204: created con: id=15, topo=0, link=0, /amba/spi@ff050000/adrv9009-phy-d@1 <-> /amba/spi@ff050000/adrv9009-phy-c@0
    [    1.797986] jesd204: created con: id=16, topo=0, link=1, /amba/spi@ff050000/hmc7044-fmc@2 <-> /amba/spi@ff040000/hmc7044@0
    [    1.808967] jesd204: created con: id=17, topo=0, link=2, /amba/spi@ff050000/hmc7044-fmc@2 <-> /amba/spi@ff040000/hmc7044@0
    [    1.819953] jesd204: created con: id=18, topo=0, link=0, /amba/spi@ff050000/hmc7044-fmc@2 <-> /amba/spi@ff040000/hmc7044@0
    [    1.830979] jesd204: created con: id=19, topo=0, link=1, /amba/spi@ff050000/adrv9009-phy-c@0 <-> /amba/spi@ff040000/adrv9009-phy-b@0
    [    1.842808] jesd204: created con: id=20, topo=0, link=2, /amba/spi@ff050000/adrv9009-phy-c@0 <-> /amba/spi@ff040000/adrv9009-phy-b@0
    [    1.854667] jesd204: created con: id=21, topo=0, link=0, /amba/spi@ff050000/adrv9009-phy-c@0 <-> /amba/spi@ff040000/adrv9009-phy-b@0
    [    1.866533] jesd204: created con: id=22, topo=0, link=1, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
    [    1.878188] jesd204: created con: id=23, topo=0, link=2, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
    [    1.889872] jesd204: created con: id=24, topo=0, link=0, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
    [    1.901579] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[0] transition uninitialized -> initialized
    [    1.911120] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[1] transition uninitialized -> initialized
    [    1.920721] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[2] transition uninitialized -> initialized
    [    1.930321] jesd204: found 14 devices and 1 topologies
    [    1.935458] FPGA manager framework
    [    1.938989] Advanced Linux Sound Architecture Driver Initialized.
    [    1.945104] Bluetooth: Core ver 2.22
    [    1.948412] NET: Registered protocol family 31
    [    1.952813] Bluetooth: HCI device and connection manager initialized
    [    1.959129] Bluetooth: HCI socket layer initialized
    [    1.963972] Bluetooth: L2CAP socket layer initialized
    [    1.968999] Bluetooth: SCO socket layer initialized
    [    1.974257] clocksource: Switched to clocksource arch_sys_counter
    [    1.979963] VFS: Disk quotas dquot_6.6.0
    [    1.983814] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    1.994724] NET: Registered protocol family 2
    [    1.995239] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
    [    2.002764] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
    [    2.010082] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
    [    2.016838] TCP: Hash tables configured (established 32768 bind 32768)
    [    2.023020] UDP hash table entries: 2048 (order: 4, 65536 bytes)
    [    2.029000] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
    [    2.035473] NET: Registered protocol family 1
    [    2.039854] RPC: Registered named UNIX socket transport module.
    [    2.045546] RPC: Registered udp transport module.
    [    2.050213] RPC: Registered tcp transport module.
    [    2.054885] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    2.061498] PCI: CLS 0 bytes, default 64
    [    2.061943] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    2.068514] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [    2.076846] Initialise system trusted keyrings
    [    2.080543] workingset: timestamp_bits=62 max_order=20 bucket_order=0
    [    2.087501] NFS: Registering the id_resolver key type
    [    2.091917] Key type id_resolver registered
    [    2.096058] Key type id_legacy registered
    [    2.100042] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    2.106708] jffs2: version 2.2. (NAND) (SUMMARY)  \xffffffc2\xffffffa9\xffffffa9 2001-2006 Red Hat, Inc.
    [    3.087129] NET: Registered protocol family 38
    [    3.140993] Key type asymmetric registered
    [    3.141030] Asymmetric key parser 'x509' registered
    [    3.144321] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
    [    3.151648] io scheduler noop registered
    [    3.155538] io scheduler deadline registered
    [    3.159793] io scheduler cfq registered (default)
    [    3.164448] io scheduler mq-deadline registered
    [    3.168945] io scheduler kyber registered
    [    3.197838] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [    3.201686] cacheinfo: Unable to detect cache hierarchy for CPU 0
    [    3.208509] brd: module loaded
    [    3.212076] loop: module loaded
    [    3.212265] Registered mathworks_ip class
    [    3.215457] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    3.222388] libphy: Fixed MDIO Bus: probed
    [    3.226228] tun: Universal TUN/TAP device driver, 1.6
    [    3.230319] CAN device driver interface
    [    3.234899] usbcore: registered new interface driver asix
    [    3.239413] usbcore: registered new interface driver ax88179_178a
    [    3.245453] usbcore: registered new interface driver cdc_ether
    [    3.251246] usbcore: registered new interface driver net1080
    [    3.256869] usbcore: registered new interface driver cdc_subset
    [    3.262750] usbcore: registered new interface driver zaurus
    [    3.268294] usbcore: registered new interface driver cdc_ncm
    [    3.274550] usbcore: registered new interface driver uas
    [    3.279195] usbcore: registered new interface driver usb-storage
    [    3.285186] usbcore: registered new interface driver upd78f0730
    [    3.291033] usbserial: USB Serial support registered for upd78f0730
    [    3.297693] i2c /dev entries driver
    [    3.302450] usbcore: registered new interface driver uvcvideo
    [    3.306413] USB Video Class driver (1.1.1)
    [    3.310937] axi_fan_control_driver 80000000.axi-fan-control: clk_get failed with -517
    [    3.319026] Bluetooth: HCI UART driver ver 2.3
    [    3.322683] Bluetooth: HCI UART protocol H4 registered
    [    3.327783] Bluetooth: HCI UART protocol BCSP registered
    [    3.333075] Bluetooth: HCI UART protocol LL registered
    [    3.338159] Bluetooth: HCI UART protocol ATH3K registered
    [    3.343539] Bluetooth: HCI UART protocol Three-wire (H5) registered
    [    3.349787] Bluetooth: HCI UART protocol Intel registered
    [    3.355128] Bluetooth: HCI UART protocol QCA registered
    [    3.360335] usbcore: registered new interface driver bcm203x
    [    3.365950] usbcore: registered new interface driver bpa10x
    [    3.371488] usbcore: registered new interface driver bfusb
    [    3.376936] usbcore: registered new interface driver btusb
    [    3.382361] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
    [    3.388023] usbcore: registered new interface driver ath3k
    [    3.393730] EDAC MC0: Giving out device to module 1 controller synps_ddr_controller: DEV synps_edac (INTERRUPT)
    [    3.403627] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [    3.415845] CPUidle arm: Failed to register cpuidle driver
    [    3.421178] sdhci: Secure Digital Host Controller Interface driver
    [    3.427168] sdhci: Copyright(c) Pierre Ossman
    [    3.431492] sdhci-pltfm: SDHCI platform and OF driver helper
    [    3.437459] ledtrig-cpu: registered to indicate activity on CPUs
    [    3.443124] zynqmp_firmware_probe Platform Management API v1.1
    [    3.448883] zynqmp_firmware_probe Trustzone version v1.0
    [    3.456697] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
    [    3.483145] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
    [    3.485843] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
    [    3.490964] zynqmp_aes zynqmp_aes: AES Successfully Registered
    [    3.490964]
    [    3.498476] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
    [    3.504594] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    3.510172] usbcore: registered new interface driver usbhid
    [    3.515523] usbhid: USB HID core driver
    [    3.526735] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [    3.527992] usbcore: registered new interface driver snd-usb-audio
    [    3.535460] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [    3.541548] Initializing XFRM netlink socket
    [    3.545507] NET: Registered protocol family 10
    [    3.550192] Segment Routing with IPv6
    [    3.553569] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    3.559688] NET: Registered protocol family 17
    [    3.563789] NET: Registered protocol family 15
    [    3.568203] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [    3.581279] can: controller area network core (rev 20170425 abi 9)
    [    3.587291] NET: Registered protocol family 29
    [    3.591636] can: raw protocol (rev 20170425)
    [    3.595871] can: broadcast manager protocol (rev 20170425 t)
    [    3.601496] can: netlink gateway (rev 20170425) max_hops=1
    [    3.607025] Bluetooth: RFCOMM TTY layer initialized
    [    3.611793] Bluetooth: RFCOMM socket layer initialized
    [    3.616900] Bluetooth: RFCOMM ver 1.11
    [    3.620616] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    3.625887] Bluetooth: BNEP filters: protocol multicast
    [    3.631078] Bluetooth: BNEP socket layer initialized
    [    3.636007] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    3.641891] Bluetooth: HIDP socket layer initialized
    [    3.646912] 9pnet: Installing 9P2000 support
    [    3.651067] NET: Registered protocol family 36
    [    3.655483] Key type dns_resolver registered
    [    3.660192] registered taskstats version 1
    [    3.663777] Loading compiled-in X.509 certificates
    [    3.668834] Btrfs loaded, crc32c=crc32c-generic
    [    3.678939] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 23, base_baud = 6249999) is a xuartps
    [    3.688282] console [ttyPS0] enabled
    [    3.691881] bootconsole [cdns0] disabled
    [    3.700125] GPIO line 13 (ulpi-phy-reset) hogged as output/high
    [    3.709369] of-fpga-region fpga-full: FPGA Region probed
    [    3.716152] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
    [    3.722841] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes
    [    3.732208] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Failed to get required clock freq
    [    3.742315] xilinx-dp-snd-codec: probe of fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0 failed with error -22
    [    3.752416] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
    [    3.760469] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
    [    3.768522] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    3.778593] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
    [    3.785635] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    3.792238] [drm] No driver support for vblank timestamp query.
    [    3.798205] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008d92d70)
    [    4.882268] [drm] Cannot find any crtc or sizes
    [    4.887005] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
    [    4.895105] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
    [    4.905167] adrv9009 spi1.0: adrv9009_probe : enter
    [    4.910931] adrv9009 spi1.1: adrv9009_probe : enter
    [    4.963315] jesd204: /amba/spi@ff040000/hmc7044-car@3,jesd204:3,parent=spi1.3: Using as sec SYSREF provider
    [    4.974021] adrv9009 spi2.0: adrv9009_probe : enter
    [    4.979431] adrv9009 spi2.1: adrv9009_probe : enter
    [    5.032609] macb ff0b0000.ethernet: Not enabling partial store and forward
    [    5.039985] libphy: MACB_mii_bus: probed
    [    5.083958] macb ff0e0000.ethernet: Not enabling partial store and forward
    [    5.091297] libphy: MACB_mii_bus: probed
    [    5.166699] Marvell 88E1510 ff0e0000.ethernet-ffffffff:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:00, irq=POLL)
    [    5.180607] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 13 (00:ae:99:a1:34:af)
    [    5.190745] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
    [    5.197254] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
    [    5.203721] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
    [    5.210190] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
    [    5.218078] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
    [    5.223935] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:0 protocol:3 pll_locked:yes
    [    5.234022] OF: graph: no port node found in /amba/zynqmp_phy@fd400000/lane1
    [    5.243771] random: fast init done
    [    5.340029] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write
    [    5.346777] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 15
    [    5.354072] i2c i2c-1: Added multiplexed i2c bus 3
    [    5.359015] i2c i2c-1: Added multiplexed i2c bus 4
    [    5.363960] i2c i2c-1: Added multiplexed i2c bus 5
    [    5.395533] i2c i2c-1: Added multiplexed i2c bus 6
    [    5.427089] i2c i2c-1: Added multiplexed i2c bus 7
    [    5.458365] i2c i2c-1: Added multiplexed i2c bus 8
    [    5.463294] i2c i2c-1: Added multiplexed i2c bus 9
    [    5.468235] i2c i2c-1: Added multiplexed i2c bus 10
    [    5.473104] pca954x 1-0070: registered 8 multiplexed busses for I2C switch pca9548
    [    5.480700] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 16
    [    5.487119] axi_fan_control_driver 80000000.axi-fan-control: Failed to initialize device
    [    5.495233] axi_fan_control_driver: probe of 80000000.axi-fan-control failed with error -22
    [    5.504007] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
    [    5.511494] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1333333 KHz
    [    5.518891] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1333333320 (-34)
    [    5.527621] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz
    [    5.536150] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1333333320 (-34)
    [    5.577057] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
    [    5.594020] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    5.604191] adrv9009 spi1.0: adrv9009_probe : enter
    [    5.609758] adrv9009 spi1.1: adrv9009_probe : enter
    [    5.662384] adrv9009 spi2.0: adrv9009_probe : enter
    [    5.671919] adrv9009 spi2.1: adrv9009_probe : enter
    [    5.681676] macb ff0b0000.ethernet: Not enabling partial store and forward
    [    5.689061] libphy: MACB_mii_bus: probed
    [    5.723297] mmc0: new high speed SDHC card at address e624
    [    5.729253] mmcblk0: mmc0:e624 SB16G 14.8 GiB
    [    5.737721]  mmcblk0: p1 p2 p3
    [    5.774687] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL)
    [    5.788600] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 12 (42:b9:2e:d5:d6:66)
    [    5.801209] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A40000 mapped to 0x(____ptrval____). Number of lanes: 8.
    [    5.816289] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using GTH4 at 0x84A60000 mapped to 0x(____ptrval____). Number of lanes: 8.
    [    5.830496] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0x84A20000 mapped to 0x(____ptrval____). Number of lanes: 16.
    [    5.846005] asoc-simple-card talise_sound: adau-hifi <-> 82000000.axi-i2s-adi mapping ok
    [    5.857439] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    5.867611] adrv9009 spi1.0: adrv9009_probe : enter
    [    5.877428] adrv9009 spi1.1: adrv9009_probe : enter
    [    5.908313] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0x(____ptrval____), probed ADC ADRV9009-X4 as MASTER
    [    5.943781] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0x(____ptrval____), probed DDS ADRV9009-X4
    [    5.958625] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition initialized -> probed
    [    5.969743] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition initialized -> probed
    [    5.980861] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition initialized -> probed
    [    5.992033] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition probed -> idle
    [    6.002545] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition probed -> idle
    [    6.013056] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition probed -> idle
    [    6.023620] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition idle -> device_init
    [    6.034565] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition idle -> device_init
    [    6.045510] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition idle -> device_init
    [    6.056511] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition device_init -> link_init
    [    6.067888] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition device_init -> link_init
    [    6.079267] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition device_init -> link_init
    [    6.090703] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_init -> link_supported
    [    6.102349] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_init -> link_supported
    [    6.113988] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_init -> link_supported
    [    6.125663] [drm] Cannot find any crtc or sizes
    [    6.130798] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_supported -> link_pre_setup
    [    6.142880] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_supported -> link_pre_setup
    [    6.154959] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_supported -> link_pre_setup
    [    6.202308] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    [    6.214471] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    [    6.226632] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    [    6.238792] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] paused at state clk_sync_stage1
    [    6.249823] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] paused at state clk_sync_stage1
    [    6.260855] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] paused at state clk_sync_stage1
    [    6.272346] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    6.282540] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    6.295089] input: gpio_keys as /devices/platform/gpio_keys/input/input0
    [    6.302024] hctosys: unable to open rtc device (rtc0)
    [    6.307071] of_cfs_init
    [    6.309526] of_cfs_init: OK
    [    6.312513] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    6.320563] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
    [    6.448428] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    6.455663] ALSA device list:
    [    6.458621]   #0: ADRV9009 ZU11EG ADAU1761
    [    6.463042] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [    6.471648] cfg80211: failed to load regulatory.db
    [    6.490427] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    6.498528] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    6.513225] devtmpfs: mounted
    [    6.516346] Freeing unused kernel memory: 832K
    [    6.530300] Run /sbin/init as init process
    [    6.764590] random: init: uninitialized urandom read (12 bytes read)
    [    6.849870] init: hwclock main process (2333) terminated with status 1
    [    6.968417] random: mountall: uninitialized urandom read (12 bytes read)
    [    7.303059] systemd-udevd[2432]: starting version 204
    [    7.434115] random: dbus-daemon: uninitialized urandom read (12 bytes read)
    [    7.830865] systemd-udevd[3425]: could not open moddep file '/lib/modules/4.19.0-76513-g94ad18a0619b-dirty/modules.dep.bin'
    [    8.106029] urandom_read: 2 callbacks suppressed
    [    8.106033] random: avahi-daemon: uninitialized urandom read (4 bytes read)
    [    8.282627] init: udev-fallback-graphics main process (3548) terminated with status 1
    [    8.416114] init: failsafe main process (3527) killed by TERM signal
    [    8.532146] random: dd: uninitialized urandom read (512 bytes read)
    [    9.297638] random: sshd: uninitialized urandom read (32 bytes read)
    [    9.350464] random: smbd: uninitialized urandom read (0 bytes read)
    [    9.373180] random: samba: uninitialized urandom read (1 bytes read)
    [    9.558990] init: tty1 main process (3830) killed by TERM signal
    [    9.779684] pps pps0: new PPS source ptp0
    [    9.779696] macb ff0b0000.ethernet: gem-ptp-timer ptp clock registered.
    [    9.779806] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
    [    9.810676] pps pps1: new PPS source ptp1
    [    9.810687] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered.
    [    9.810797] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [    9.991561] init: samba-ad-dc main process (3794) terminated with status 1
    [   13.974797] macb ff0e0000.ethernet eth0: link up (1000/Full)
    [   13.974816] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [   27.311866] random: crng init done

  • What SOM version do you have? Are you using the external HMC7044 as described in the setup?

    -Travis

  • The SOMs are all rev B, and yes I'm using the external HMC7044 as described.

    My setup has been running successfully since June.  The problems began when I attempted to upgrade to the new files.

    I can continue running on my old setup but my understanding was that there have been significant synchronization improvements.

  • Hi,

    The new files use the jesd204-fsm framework - please see wiki page below.

    The link points to the Synchronizing distributed multi-topology systems section but the whole page is relevant.

    https://wiki.analog.com/resources/tools-software/linux-drivers/jesd204/jesd204-fsm-framework#synchronizing_distributed_multi-topology_systems

    Your trace shows that the device has enter a stop state:

    [    6.260855] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] paused at state clk_sync_stage1

    Basically all devices should wait here, until the external manager resumes all devices in from the paused states. 

    It's important to know, while the devices are not yet fully initialized, they must not be accessed via their regular API, since they are not yet fully initialized.

    You need to make sure:

    1) OSC doesn't start automatically remove it from /home/analog/.config/autostart/ADI IIO Oscilloscope

    2) No other script starts automatically which tries to access the adrv9009-phy IIO devices.

    3) You use the latest python example from master : https://github.com/analogdevicesinc/pyadi-iio/blob/master/examples/adrv9009_som_multi.py

    4) You have loaded the device tree named .._primary onto the board with the external HMC7044 clock chip connected. And that you use it's IP in the script.

    -Michael

  • I still haven't had any success.  Regarding your list:

    1) I've removed everything from the /home/analog/config/autostart and /root/.config/autostart directories on both primary and secondary devices.

    2) I don't have any scripts configured to start automatically -- are there any that start on the image provided here? https://wiki.analog.com/resources/tools-software/linux-software/zynq_images

    3.) I have tried using the adrv9009_som_multi.py file you linked, by changing the IP addresses to match those of my network.

    4) I have added the BOOT.BIN, Image, system.dtb, and uEnv.txt files for primary to the primary device and those for secondary to the secondary device.

    When I run "adrv9009_som_multi.py" I receive this output:

    --Connecting to devices


    Iteration# 0
    ip:192.168.1.21: DEVICE0: Is <Paused> in state <clk_sync_stage1> with status <0>
    ip:192.168.1.20: DEVICE1: Is <Paused> in state <clk_sync_stage1> with status <0>
    ip:192.168.1.21: DEVICE0: Is <Paused> in state <clk_sync_stage2> with status <0>
    ip:192.168.1.20: DEVICE1: Is <Paused> in state <clk_sync_stage2> with status <0>
    ip:192.168.1.21: DEVICE0: Is <Paused> in state <clk_sync_stage3> with status <0>
    Re-initializing due to lock-up
    Traceback (most recent call last):
      File "adrv9009_som_multi.py", line 116, in <module>
        x = multi.rx()
      File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/adrv9009_zu11eg_multi.py", line 423, in rx
        self._pre_rx_setup()
      File "/home/ubuntu/.local/lib/python3.8/site-packages/adi/adrv9009_zu11eg_multi.py", line 411, in _pre_rx_setup
        raise Exception("Unable to initialize (Board reboot required)")
    Exception: Unable to initialize (Board reboot required)

    There are references in the adrv9009_som_multi.py file to fmcomms8 devices.  However those aren't detailed on the "syncronization" page I listed on the first post.  I don't have any fmcomms8 devices so I haven't been able to try with them installed.

    Are there steps I could try at a python prompt to verify this is working, as Travis suggested above?

  • If you do not use the attached FMComms8's set the fmcomms8 input to False here: https://github.com/analogdevicesinc/pyadi-iio/blob/master/examples/adrv9009_som_multi.py#L58

    There was a minor bug fix we added you can try, it's in master now.

    Related PR: https://github.com/analogdevicesinc/pyadi-iio/pull/160

    -Travis