Zedboard interfacing with AD-FCOMMS3-EBZ

I need to interface Zedboard with AD-FCOMMS3-EBZ.  I have prepared the SD card image as mentioned in the link: https://wiki.analog.com/resources/tools-software/linux-software/zynq_images.  The images which I have tried are : 22 June 2020 release (2019_R1) and 04 February 2020 release (2019_R1 RC). 

But the Zedboard is not booting. The following is observed on the console:

U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21)

Board: Xilinx Zynq
I2C: ready
DRAM: ECC disabled 512 MiB
MMC: zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SC16G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
reading uEnv.txt
392 bytes read in 9 ms (42 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
reading uImage
** Unable to read file uImage **
Copying Linux from SD to RAM...
reading uImage
** Unable to read file uImage **
zynq-uboot>

It is given on the link mentioned above (reproduced below in bold text), to copy the images from subdirectory into the base directory. But there are no images files in the subdirectory corresponding to Zedboard+ADV7511+ADFCOMMS3-EBZ board file. The subdirectory has only BOOT.BIN file and a devicetree.dtb file and a zip file. I am not able to find the uImage in the subdirectory.  

The SD card includes a few images on it's BOOT partition. One of these images needs to be selected before the system will boot properly. In order to run any of these images, just copy the images from the subdirectory into the base directory, and then boot it. For newer versions of the SD card, uImage files are in subdirectories for FPGA board generation. Be sure to move the correct uImage into the root of the BOOT partition as well.

Please clarify whether base directory means BOOT partition of the SD card. What do you mean by "root of the BOOT partition"? Please let me know where the correct uImage can be found?

Parents
  • 0
    •  Analog Employees 
    on Oct 28, 2020 7:30 AM

    Hi Rajesh,

    On the SD card there are 2 paritions visible a BOOT and a rootfs. If you use windows you will only see the BOOT partition. Inside it are a number of folders with the names of different projects along with the name of the board that they are designed for.

    For FMCOMMS3 you must copy the files from zynq-zed-adv7511-ad9361-fmcomms2-3 into the BOOT root outside of this folder. Another thing to copy is the uImage from the zynq-common folder, again in the root of the BOOT parittion.

    Regards,

    Mircea

Reply
  • 0
    •  Analog Employees 
    on Oct 28, 2020 7:30 AM

    Hi Rajesh,

    On the SD card there are 2 paritions visible a BOOT and a rootfs. If you use windows you will only see the BOOT partition. Inside it are a number of folders with the names of different projects along with the name of the board that they are designed for.

    For FMCOMMS3 you must copy the files from zynq-zed-adv7511-ad9361-fmcomms2-3 into the BOOT root outside of this folder. Another thing to copy is the uImage from the zynq-common folder, again in the root of the BOOT parittion.

    Regards,

    Mircea

Children