Hi,I have designed a custom board based on AD-FMCOMMS1-EBZ.The modification i did was instead of using two ADF4351s, i'm using one ADF5355 to supply LO for both Modulator and Demodulator.
I have below questions1. Can the board power up correctly without FRU?2. Where does the FRU information stored in the AD-FMCOMMS1-EBZ ?
Thanks !
Regards,Anojh
Hi Anojh,
Yes, it looks good. You can double check by looking into the device tree: https://github.com/analogdevicesinc/linux/blob/master/arch/arm/boot/dts/adi-fmcomms1.dtsi
-Istvan
You can find more info about FRU here: https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/applications/fru_dump
"1. Can the board power up correctly without FRU?" -- as far as I know it depends on the carrier. There are carriers which checking the FRU image, mainly to check the VADJ level, there are others that don't.
Let us know if you still have questions.
Thanks,
Hi Istvan,
Thanks for your reply.
So far all the supplies are correct. but i encounter a problem with the AD9122. it doesn't show up in the iio:devices I get below kernel messages at boot-up
cf_axi_dds 74204000.cf-ad9122-core-lpc: DRP unlocked.cf_axi_dds: probe of 74204000.cf-ad9122-core-lpc failed with error -110
I'm attaching the entire log for your reference.
U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21) Board: Xilinx Zynq I2C: r3▒AM: ECC disabled 512 MiB MMC: zynq_s root@analog:~# U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21) Board: Xilinx Zynq I2C: ready DRAM: ECC disabled 512 MiB MMC: zynq_sdhci: 0 SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Net: Gem.e000b000 Hit any key to stop autoboot: 0 Device: zynq_sdhci Manufacturer ID: 12 OEM: 5678 Name: ASTCTran Speed: 50000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 14.6 GiB Bus Width: 4-bit reading uEnv.txt 380 bytes read in 9 ms (41 KiB/s) Loaded environment from uEnv.txt Importing environment from SD ... Running uenvcmd ... Copying Linux from SD to RAM... reading uImage 3586384 bytes read in 323 ms (10.6 MiB/s) reading devicetree.dtb 18424 bytes read in 39 ms (460.9 KiB/s) reading uramdisk.image.gz ** Unable to read file uramdisk.image.gz ** ## Booting kernel from Legacy Image at 03000000 ... Image Name: Linux-4.6.0-gca4cf2a Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3586320 Bytes = 3.4 MiB Load Address: 00008000 Entry Point: 00008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 02a00000 Booting using the fdt blob at 0x2a00000 Loading Kernel Image ... OK Loading Device Tree to 1ed1b000, end 1ed227f7 ... OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Linux version 4.6.0-gca4cf2a (jenkins@romlx1) (gcc version 4.8.3 20140320 (prerelease) (Sourcery CodeBench Lite 2014.05-29) ) #21 SMP PREEMPT Mon Nov 21 14:17:49 GMT 2016 CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Xilinx Zynq ZED bootconsole [earlycon0] enabled cma: Reserved 128 MiB at 0x16c00000 Memory policy: Data cache writealloc percpu: Embedded 12 pages/cpu @dfb8e000 s19456 r8192 d21504 u49152 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait PID hash table entries: 2048 (order: 1, 8192 bytes) Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) Memory: 380852K/524288K available (4800K kernel code, 244K rwdata, 1940K rodata, 248K init, 136K bss, 12364K reserved, 131072K cma-reserved, 0K highmem) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) modules : 0xbf000000 - 0xbfe00000 ( 14 MB) .text : 0xc0008000 - 0xc069d3e8 (6741 kB) .init : 0xc069e000 - 0xc06dc000 ( 248 kB) .data : 0xc06dc000 - 0xc07192a0 ( 245 kB) .bss : 0xc07192a0 - 0xc073b4b0 ( 137 kB) Preemptible hierarchical RCU implementation. Build-time adjustment of leaf fanout to 32. RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2. RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2 NR_IRQS:16 nr_irqs:16 16 slcr mapped to e0800000 L2C: platform modifies aux control register: 0x72360000 -> 0x72760000 L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000 L2C-310 erratum 769419 enabled L2C-310 enabling early BRESP for Cortex-A9 L2C-310 full line of zeros enabled for Cortex-A9 L2C-310 ID prefetch enabled, offset 1 lines L2C-310 dynamic clock gating enabled, standby mode enabled L2C-310 cache controller enabled, 8 ways, 512 kB L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001 zynq_clock_init: clkc starts at e0800100 Zynq clock init ps_clk frequency not specified, using 33 MHz. sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns Switching to timer-based delay loop, resolution 3ns clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns timer #0 at e0808000, irq=17 Console: colour dummy device 80x30 Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 Setting up static identity map for 0x82c0 - 0x8318 CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 Brought up 2 CPUs SMP: Total of 2 processors activated (1333.33 BogoMIPS). CPU: All CPU(s) started in SVC mode. devtmpfs: initialized VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations cpuidle: using governor ladder hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. hw-breakpoint: maximum watchpoint size is 4 bytes. zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0880000 zynq-pinctrl 700.pinctrl: zynq pinctrl initialized SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb media: Linux media interface: v0.10 Linux video capture interface: v2.00 EDAC MC: Ver: 3.0.0 Advanced Linux Sound Architecture Driver Initialized. clocksource: Switched to clocksource arm_global_timer NET: Registered protocol family 2 TCP established hash table entries: 4096 (order: 2, 16384 bytes) TCP bind hash table entries: 4096 (order: 3, 32768 bytes) TCP: Hash tables configured (established 4096 bind 4096) UDP hash table entries: 256 (order: 1, 8192 bytes) UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) NET: Registered protocol family 1 hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available futex hash table entries: 512 (order: 3, 32768 bytes) workingset: timestamp_bits=28 max_order=17 bucket_order=0 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) Error: Driver 'mwipcore' is already registered, aborting... dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330 dma-pl330 f8003000.dmac: DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16 xilinx-vdma 43000000.axivdma: missing xlnx,flush-fsync property xilinx-vdma 43000000.axivdma: missing xlnx,addrwidth property xilinx-vdma 43000000.axivdma: Xilinx AXI VDMA Engine Driver Probed!! e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 143, base_baud = 3125000) is a xuartps ▒console [ttyPS0] enabled console [ttyPS0] enabled bootconsole [earlycon0] disabled bootconsole [earlycon0] disabled xdevcfg f8007000.devcfg: ioremap 0xf8007000 to e081a000 [drm] Initialized drm 1.1.0 20060810 brd: module loaded loop: module loaded m25p80 spi32766.0: found s25fl256s1, expected n25q128a11 m25p80 spi32766.0: s25fl256s1 (32768 Kbytes) 5 ofpart partitions found on MTD device spi32766.0 Creating 5 MTD partitions on "spi32766.0": 0x000000000000-0x000000500000 : "boot" 0x000000500000-0x000000520000 : "bootenv" 0x000000520000-0x000000540000 : "config" 0x000000540000-0x000000fc0000 : "image" 0x000000fc0000-0x000002000000 : "spare" libphy: XEMACPS mii bus: probed xemacps e000b000.eth: pdev->id -1, baseaddr 0xe000b000, irq 163 ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver usbcore: registered new interface driver usb-storage usbcore: registered new interface driver usbserial usbcore: registered new interface driver usbserial_generic usbserial: USB Serial support registered for generic usbcore: registered new interface driver ftdi_sio usbserial: USB Serial support registered for FTDI USB Serial Device e0002000.usb supply vbus not found, using dummy regulator ULPI transceiver vendor/product ID 0x0451/0x1507 Found TI TUSB1210 ULPI transceiver. ULPI integrity check: passed. ci_hdrc ci_hdrc.0: EHCI Host Controller ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected mousedev: PS/2 mouse device common for all mice i2c /dev entries driver at24 1-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write at24 1-0054: 256 byte 24c02 EEPROM, writable, 1 bytes/write Xilinx Zynq CpuIdle Driver started sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman sdhci-pltfm: SDHCI platform and OF driver helper mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA ledtrig-cpu: registered to indicate activity on CPUs hidraw: raw HID events driver (C) Jiri Kosina usbcore: registered new interface driver usbhid usbhid: USB HID core driver spi32765.6 supply vcc not found, using dummy regulator spi32765.3 supply vcc not found, using dummy regulator mmc0: Problem switching card into high-speed mode! mmc0: new SDHC card at address 0001 mmcblk0: mmc0:0001 ASTC 14.6 GiB mmcblk0: p1 p2 p3 ad9523 spi32765.3: probed ad9523-lpc ad9548 spi32765.2: Rev. 0xC6 probed spi32765.5 supply vcc not found, using dummy regulator NET: Registered protocol family 17 Registering SWP/SWPB emulation handler axi-hdmi 70e00000.axi_hdmi: No connectors reported connected with modes [drm] Cannot find any crtc or sizes - going 1024x768 Console: switching to colour frame buffer device 128x48 axi-hdmi 70e00000.axi_hdmi: fb0: frame buffer device [drm] Initialized axi_hdmi_drm 1.0.0 20120930 on minor 0 cf_axi_dds 74204000.cf-ad9122-core-lpc: DRP unlocked. cf_axi_dds: probe of 74204000.cf-ad9122-core-lpc failed with error -110 asoc-simple-card fpga-axi@0:adv7511_hdmi_snd: adv7511 <-> 75c00000.axi-spdif-tx mapping ok asoc-simple-card fpga-axi@0:zed_sound: adau-hifi <-> 77600000.axi-i2s mapping ok oooooo|ooooo--------------------- DCO 0x85 CLK 245760000 Hz cf_axi_adc 79020000.cf-ad9643-core-lpc: ADI AIM (9.00.b) at 0x79020000 mapped to 0xe0a00000, probed ADC AD9643 as MASTER hctosys: unable to open rtc device (rtc0) ALSA device list: #0: HDMI monitor #1: ZED ADAU1761 EXT4-fs (mmcblk0p2): recovery complete EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) VFS: Mounted root (ext4 filesystem) on device 179:2. devtmpfs: mounted Freeing unused kernel memory: 248K (c069e000 - c06dc000) This architecture does not have kernel memory protection. Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory +Bݍ▒▒▒▒j▒▒▒▒ɽ▒▒▒▒B¢▒J▒▒ɵ▒▒▒ѕ▒▒▒ѡ▒х▒▒͊▒ * Setting up X socket directories..[ OK ] * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting * Starting IIO Daemon iiod [ OK ] Last login: Thu Jan 1 00:00:10 UTC 1970 on ttyPS0 Welcome to Linaro 14.04 (GNU/Linux 4.6.0-gca4cf2a armv7l)
Hi Istvan,When i remove the output termination resistors (100 Ohm) of AD9523 clocks, the DAC started working. The ref schematic doesn't have these resistors. But i have added them in my design and mistakenly inserted them.
Can you verify that below devices are correct and i'm not missing any further devices ?
root@analog:~# grep "" /sys/bus/iio/devices/iio\:device*/name/sys/bus/iio/devices/iio:device0/name:xadc/sys/bus/iio/devices/iio:device1/name:ad8366-lpc/sys/bus/iio/devices/iio:device2/name:ad9523-lpc/sys/bus/iio/devices/iio:device3/name:adf5355/sys/bus/iio/devices/iio:device4/name:cf-ad9122-core-lpc/sys/bus/iio/devices/iio:device5/name:cf-ad9643-core-lpc
Regards,
Anojh