AD-FMCDAQ2-EBZ KC705 SW

Dear ADI Support, I'm using the AD-FMCDAQ2-EBZ board, I want to build the hardware on KC705 xilinxs Board I found the hardware project (hdl-master or hdl-2016_r2 ), but I could find the sofware project source files   for kc705 (Microblaze), please can you help me .. thanks very much

Top Replies

Parents
  • hi Rejeesh, i made another FMC DAQ2 SETUP where I explained what I did,  I prepare a system to evaluate the FMC Daq2 board and adding some hardware (Dsp) stuff in KC705, I'm not ready. I did some measurement on AD6684-500 + ADS7-V2-EBZ, but KC705+FMCDAQ2 is more suitable for a real time system since I can integrate my HW in the chain.

    If the IIO oscilloscope works for bare metall no-os, that would be great. I don't what are the other possibilities for having the stuff working on windows: IIO Osc source code + no-os  doing myself, or is it reasonable to go directly to linux ?

    please have look to my other post "FMC DAQ2 Setup". thanks a lot

Reply
  • hi Rejeesh, i made another FMC DAQ2 SETUP where I explained what I did,  I prepare a system to evaluate the FMC Daq2 board and adding some hardware (Dsp) stuff in KC705, I'm not ready. I did some measurement on AD6684-500 + ADS7-V2-EBZ, but KC705+FMCDAQ2 is more suitable for a real time system since I can integrate my HW in the chain.

    If the IIO oscilloscope works for bare metall no-os, that would be great. I don't what are the other possibilities for having the stuff working on windows: IIO Osc source code + no-os  doing myself, or is it reasonable to go directly to linux ?

    please have look to my other post "FMC DAQ2 Setup". thanks a lot

Children
No Data