AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
Hi all,
Hoping someone could clear something up for me... Working with the AD9371, and ADI has developed a whole slew of JESD204 interface cores, specifically:
What is the recommendation in terms of using these vs. the Xilinx JESD PHY and core? I already have the Xilinx license, so cost isn't relevant to this particular application.
Hi ,
I am using a VCXO of 80MHz generating a device clock of 80MHz (9528 is redundant in my case yet still I am using it) that is used as reference in both AD9371 and FPGA transceivers. the transceivers lane rate is 3.2GHz.
On the AD9371 I use a VCO=9.6GHz and divide by 3 to generate the 3.2GHz lane rate:
static mykonosDigClocks_t mykonosClocks =
{
80000, /* CLKPLL and device reference clock frequency in kHz*/
9600000, /* CLKPLL VCO frequency in kHz*/
VCODIV_3, /* CLKPLL VCO divider*/
5 /* CLKPLL high speed clock divider*/
};
static mykonosRxProfile_t rxProfile =
{/* RX 80MHz, Iqrate 160MSPS, DEC5 */
1, /* The divider used to generate the ADC clock*/
&rxFir, /* Pointer to Rx FIR filter structure*/
1, /* Rx FIR decimation (1,2,4)*/
4, /* Decimation of Dec5 or Dec4 filter (5,4)*/
0, /* If set, and DEC5 filter used, will use a higher rejection DEC5 FIR filter (1=Enabled, 0=Disabled)*/
1, /* RX Half band 1 decimation (1 or 2)*/
160000, /* Rx IQ data rate in kHz*/
80000000, /* The Rx RF passband bandwidth for the profile*/
80000, /* Rx BBF 3dB corner in kHz*/
&rxAdcCustom[0] /* pointer to custom ADC profile*/
};
On the FPGA side the XCVR block generates the 3.2GHz using the CPLL.
After initialization and bypassing of few AGC and TXIQC calibration related errors I get :
Please wait...
RX_XCVR initialization OK
TX_XCVR initialization OK
RX_OS_XCVR initialization OK
MCS successful
CLKPLL locked
AD9371 ARM version 5.1.1
PLLs locked
Calibrations completed successfully
DeframerStatus = 0x61
dac_setup dac core initialized (160 MHz).
adc_setup adc core initialized (160 MHz).
Done
when using the ILA to view the rx clock and rxos generators output I see completely random wave forms as shown below. What am I doing wrong ?
Hi ,
I am using a VCXO of 80MHz generating a device clock of 80MHz (9528 is redundant in my case yet still I am using it) that is used as reference in both AD9371 and FPGA transceivers. the transceivers lane rate is 3.2GHz.
On the AD9371 I use a VCO=9.6GHz and divide by 3 to generate the 3.2GHz lane rate:
static mykonosDigClocks_t mykonosClocks =
{
80000, /* CLKPLL and device reference clock frequency in kHz*/
9600000, /* CLKPLL VCO frequency in kHz*/
VCODIV_3, /* CLKPLL VCO divider*/
5 /* CLKPLL high speed clock divider*/
};
static mykonosRxProfile_t rxProfile =
{/* RX 80MHz, Iqrate 160MSPS, DEC5 */
1, /* The divider used to generate the ADC clock*/
&rxFir, /* Pointer to Rx FIR filter structure*/
1, /* Rx FIR decimation (1,2,4)*/
4, /* Decimation of Dec5 or Dec4 filter (5,4)*/
0, /* If set, and DEC5 filter used, will use a higher rejection DEC5 FIR filter (1=Enabled, 0=Disabled)*/
1, /* RX Half band 1 decimation (1 or 2)*/
160000, /* Rx IQ data rate in kHz*/
80000000, /* The Rx RF passband bandwidth for the profile*/
80000, /* Rx BBF 3dB corner in kHz*/
&rxAdcCustom[0] /* pointer to custom ADC profile*/
};
On the FPGA side the XCVR block generates the 3.2GHz using the CPLL.
After initialization and bypassing of few AGC and TXIQC calibration related errors I get :
Please wait...
RX_XCVR initialization OK
TX_XCVR initialization OK
RX_OS_XCVR initialization OK
MCS successful
CLKPLL locked
AD9371 ARM version 5.1.1
PLLs locked
Calibrations completed successfully
DeframerStatus = 0x61
dac_setup dac core initialized (160 MHz).
adc_setup adc core initialized (160 MHz).
Done
when using the ILA to view the rx clock and rxos generators output I see completely random wave forms as shown below. What am I doing wrong ?