Error in FPGA design of ADRV9371 for A10GX

Hello.

 

Now, I go thru building and checking AD FPGA AD9371 project on my development kits Arria 10 GX and ADRV9371-W / PCBZ.

 

My current configuration is:

 

Project: hdl \ projects \ adrv9371x \ a10gx

Project brunch: Master

Nios project: no-OS \ ad9371 \ sw \

NIOS branch: 2016_R2

Quartus Prime: 16.0.2.222 standard edition

Eclipse (comes with quartus): Kepler Service Release 2 Build id: 20140224-0627

 

I spent 2 days to debug the following error, which I found in platform_drivers.c downloaded from Git.

 

The symptom is: when NIOS wrote SPI configuration words to AD9528, they really get to AD9371. The reading is doing the same from AD9371. And vice versa.

The cause is: Wrong selection of CS signal in platform_drivers.c:

 

IOWR_32DIRECT (SPI_BASEADDR, ALT_AVL_SPI_SLAVE_SEL_REG, ~ (dev-> chip_select));

 

Here, no need to inverse (dev-> chip_select), because selection of active masters in slaveselect register of the Altera SPI Core is made by mask with positive logic:

https://www.altera.com/documentation/sfo1400787952932.html#iga1405558422226

CS definitions from platform_drivers.h are:

#define AD9528_CHIP_SELECT    2
#define AD9371_CHIP_SELECT    1

And this is right because of pin assignments on board.

 

Right selection of master CS is:

IOWR_32DIRECT (SPI_BASEADDR, ALT_AVL_SPI_SLAVE_SEL_REG, dev-> chip_select);

 

P.S.

Now I go futher and get next error:

device-> rx-> rxAgcCtrl-> agcGainUpdateTime_us out of range in MYKONOS_setupRxAgc ()

Hope, it will not take much time to debug ...

Parents
  • Hi
    I returned to work with this project after a pause. As I understand, last time, I'd got JESD synchronization error:
    ....
    RX_XCVR initialization OK
    TX_XCVR initialization OK
    RX_OS_XCVR initialization OK
    RxFramerStatus = 0x20
    OrxFramerStatus = 0x20
    DeframerStatus = 0x21
    ....
    Could it be result of not updated project on your Git repository?
    Will you plan to update master branch of hdl and no-os driver with new A10GX supported project?

    My current configuration is:
    Project: hdl\projects\adrv9371x\a10gx\
    Altera project brunch: Master
    No-OS project brunch: 2016_R2
    Quartus Prime: 16.0.0 build 211 standart edition
    Eclipse (comes with quartus): Version: Kepler Service Release 2 Build id: 20140224-0627

Reply
  • Hi
    I returned to work with this project after a pause. As I understand, last time, I'd got JESD synchronization error:
    ....
    RX_XCVR initialization OK
    TX_XCVR initialization OK
    RX_OS_XCVR initialization OK
    RxFramerStatus = 0x20
    OrxFramerStatus = 0x20
    DeframerStatus = 0x21
    ....
    Could it be result of not updated project on your Git repository?
    Will you plan to update master branch of hdl and no-os driver with new A10GX supported project?

    My current configuration is:
    Project: hdl\projects\adrv9371x\a10gx\
    Altera project brunch: Master
    No-OS project brunch: 2016_R2
    Quartus Prime: 16.0.0 build 211 standart edition
    Eclipse (comes with quartus): Version: Kepler Service Release 2 Build id: 20140224-0627

Children
No Data