Post Go back to editing

AD9121-M5372-EBZ based on AD-FMCOMMS1-EBZ

Hello,

I’m using the AD9121-M5372-EBZ evaluation board connected by FMC with a ZedBoard. By using these instructions:

  1. https://wiki.analog.com/resources/fpga/docs/build#folded_1
  2. https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/software/linux/zynq
  3. https://wiki.analog.com/resources/tools-software/linux-drivers/iio-dds/axi-dac-dds-hdl

I try to launch LINUX – DAC working system without any success. First of all I modify HDL reference design by deleting the ADC IP blocks from block design and change pinout on FMC Connector. Then I have modified and generated the device tree file but unfortunately no communication has been established between the ARM and DAC (but the HDMI working perfectly). So I made some mistake, but I have no idea where. The differences between both evaluation boards (AD9121 and FMCOMMS1) are mainly in connection number in FMC connector. I only want to send data samples from Linux to 9121.

My board don’t have IIC connection whatsoever with AD9121. I also don’t see the my device on the list in /sys/bus/iio/devices .

After launching the Linux there are two alarming messages:

  1. UART:

spi_master spi32765: failed to transfer one message from queue

iio iio:device1: write failed (-5)

 mmcblk0: p1 p2

ad9523: probe of spi32765.3 failed with error -5

spi_master spi32765: failed to transfer one message from queue

ad9548: probe of spi32765.2 failed with error -5

spi_master spi32765: failed to transfer one message from queue

ad9122: probe of spi32765.0 failed with error -5

  1. HDMI Monitor:

Modprobe: FATAL: Could not load /lib/modules/4.6.0-ga8f23b8/modules.dep: No such file or directory

I have been researching and working on it from a long time, and I’ve exhausted all my ideas how to make this connection working.  Can anyone help me? Is someone working on this “changes” in reference design with a success?

 

Thank you in advance.

Parents
  • FMCOMMS1 used to use a AD9122 not the AD9121.

    Also this board doesn't have AD9523, AD9548 clock chips, it uses the AD9516.

    Why is it still probing them?

    Error: -5 is EIO (I/O error) which means the drivers can't talk to the HW.

    How did you connect the SPI to FPGA?

    Without knowing your connections, FPGA design and device tree we can't really provide you more help.

    -Michael 

Reply
  • FMCOMMS1 used to use a AD9122 not the AD9121.

    Also this board doesn't have AD9523, AD9548 clock chips, it uses the AD9516.

    Why is it still probing them?

    Error: -5 is EIO (I/O error) which means the drivers can't talk to the HW.

    How did you connect the SPI to FPGA?

    Without knowing your connections, FPGA design and device tree we can't really provide you more help.

    -Michael 

Children
No Data