Post Go back to editing

no-OS code of AD9379A?

Thread Summary

The user encountered issues with the AD9739A FMC evaluation board on the Xilinx ZC706, including missing 'spi.h' and 'DAC Core Status errors'. The problem was resolved by using the 2018_R2 branch of no-OS and ensuring the correct clock path (ADCLK914) was enabled. A new issue with inconsistent behavior of the LD light and DLL lock was identified, but the user confirmed the AD9739A is now working.
AI Generated Content

Hello! I'm using the Xilinx ZC706 evaluation board and AD9379A FMC evaluation board.

According to https://wiki.analog.com/resources/fpga/docs/build#windows_environment_setup, I have built a vivado HDL project.

Besides, I have built a no-OS project in SDK according to https://github.com/analogdevicesinc/no-OS/tree/master/ad9739a-fmc-ebz. But the makefile can't  be used because "spi.h" is missed. I'm sure that I used the latest version.

So I add these .c and .h files to SDK project manually. And I have seen that the "spi.h" in https://github.com/analogdevicesinc/no-OS/tree/master/include isn't right and it can be represented by the "platform_drivers.h" in https://github.com/analogdevicesinc/no-OS/tree/master/common_drivers/platform_drivers. So the "include spi.h" in some .c files are modified to "include platform_drivers.h" by myself.

And I found that the "config.h" needs to be modified to meet the corresponding development board. After all the steps are done, I run the debug. But when running to the "dac_setup(&ad9739a_core)", "DAC Core Status errors" is shown in the SDK terminal. I don't know why.

Parents Reply Children
  • I thought I seemed to find the problem.

    These pictures above are the power supply on AD9739A evaluation board. I have found that there are no connection between JP1 and JP2 on the board. Besides, I have measured the TP12 TP2 TP1 TP3. And there is no voltage on the board! Does it mean I must solder a 0 ohm resistance on JP1 and JP2 pad?

  • Hi, I've solved the problem and it's working. Thank you for helping me!

  • Hi, I have a new problem!

    I've tried to write the verilog code about spi configuration of the ad9739a evaluation board which has two spi devices (adf4350 and ad9739a). I'm sure that the spi code is working normally because the spi data read from ad9739a is right. But the adf4350 spi doesn't work normally. After I configure the register in adf4350, the LD light on the board isn't on. The debug picture of adf4350 spi are as follows:

    the clock frequency of ILA is 200MHz. According to the datasheet of adf4350, the timing is correct.

    The data written to r0-r5 register of adf4350 is 0x00320000, 0x00008009, 0x00006e42, 0x00000003, 0x008c823c and 0x00580005.

    I don't know why it isn't working.

  • Hi, I have met an interesting problem.

    When I download and debug the ADI reference design (hdl and no-os projiect), sometimes the LD light is on, sometimes it isn't. Besides, sometimes the chip_id of ad9739a can be read successfully, sometimes it can't. But the DLL of ad9739a always can't be locked. I'm sure I'm using the same code and the jumper jumps to FMC source.