AD9361 TXFIR int 0 RXFIR dec 0 mode Highest OSR

Hi,

These are the inputs given by us for configuring AD9361.

{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies 

{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies

AD9361_TXFIRConfig tx_fir_config = {    // BPF PASSBAND 3/20 fs to 1/4 fs
    1, // tx
    -6,  tx_gain
    2 ,//tx_int
{1,-6,-28,-62,-80,-56,11,68,54,-29,-98,-61,64,142,59,-122,-195,-35,210,246,-26,-329,-280,141,476,273,-326,-636,-193,595,786,3,-957,-889,351,1424,890,-953,-2027,-696,1997,2886,76,-4178,-4612,2199,13771,22755,22755,13771,2199,-4612,-4178,76,2886,1997,-696,-2027,-953,890,1424,351,-889,-957,3,786,595,-193,-636,-326,273,476,141,-280,-329,-26,246,210,-35,-195,-122,59,142,64,-61,-98,-29,54,68,11,-56,-80,-62,-28,-6,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    128, // tx_coef_size
    {1024000000, 64000000, 32000000, 16000000, 8000000, 4000000}, //{0, 0, 0, 0, 0, 0}, // tx_path_clks[6]
     1330000 // tx_bandwidth
};

but we are getting error ad9361_calculate_rf_clock_chain: requested rate 4000000 TXFIR int 0 RXFIR dec 0 mode Highest OSR
ad9361_calculate_rf_clock_chain: Failed to find suitable dividers: ADC clock below limit".

please give the feedback how to solve thiis error.

Top Replies

Parents
  • we used  this function in main.c ad9361_trx_load_enable_fir(ad9361_phy, rx_fir_config, tx_fir_config)" ,and still we got same error "ad9361_calculate_rf_clock_chain: Failed to find suitable dividers: ADC clock below limit.

  • Hi,

    Sampling rates for both transmit and receive chain are same.

    I tried out thisad9361_trx_load_enable_fir(ad9361_phy, rx_fir_config, tx_fir_config)  function earlier itself.

    Still getting same error only.

    ad9361_calculate_rf_clock_chain: requested rate 4000000 TXFIR int 0 RXFIR dec 0 mode Highest OSR

    ad9361_calculate_rf_clock_chain: Failed to find suitable dividers: ADC clock below limit.

    What about the changes which I made in block design.All are correct,  right?

  • 0
    •  Analog Employees 
    on Oct 1, 2019 7:16 AM over 1 year ago in reply to mgeorge@cdot.in

    Hi,

    First of all never modify the rates in the init structure.

    Then design a filter for both RX and TX paths. If you load it and then enable it simultaneously there shouldn't be any error.

    Can you please provide your entire setup code snippet?

    -Michael

  • 0
    •  Analog Employees 
    on Oct 1, 2019 7:20 AM over 1 year ago in reply to mgeorge@cdot.in

    Hello,

    Regarding removing the DDR and using 512K memory, if it's enough memory to fit the software, it should be ok.

    Regarding streaming data through RAM, it should work, if the data is provided when the IP needs it. Some description regarding the data streams can be found at https://wiki.analog.com/resources/fpga/docs/axi_ad9361 

    Regards,

    Adrian

  • Hi,

    I'm attaching main.c file from SDK.

    We changed the rx_path_clock_frequencies[6],tx_path_clock_frequencies[6],rf_rx_bandwidth_hz,rf_tx_bandwidth_hz are  made to zero in default_init_param  in SDK. Desired values are given in tx_fir_config,rx_fir_config structure.

    /***************************************************************************//**
     *   @file   main.c
     *   @brief  Implementation of Main Function.
     *   @author DBogdan (dragos.bogdan@analog.com)
    ********************************************************************************
     * Copyright 2013(c) Analog Devices, Inc.
     *
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions are met:
     *  - Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *  - Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in
     *    the documentation and/or other materials provided with the
     *    distribution.
     *  - Neither the name of Analog Devices, Inc. nor the names of its
     *    contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *  - The use of this software may or may not infringe the patent rights
     *    of one or more patent holders.  This license does not release you
     *    from the requirement that you obtain separate licenses from these
     *    patent holders to use this software.
     *  - Use of the software either in source or binary form, must be run
     *    on or directly connected to an Analog Devices Inc. component.
     *
     * THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR
     * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT,
     * MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
     * IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT,
     * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     * LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR
     * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
     * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
     * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *******************************************************************************/
    
    /******************************************************************************/
    /***************************** Include Files **********************************/
    /******************************************************************************/
    #include "config.h"
    #include "ad9361_api.h"
    #include "parameters.h"
    #include "platform.h"
    #ifdef CONSOLE_COMMANDS
    #include "command.h"
    #include "console.h"
    #endif
    #ifdef XILINX_PLATFORM
    #include <xil_cache.h>
    #endif
    #if defined XILINX_PLATFORM || defined LINUX_PLATFORM || defined ALTERA_PLATFORM
    #include "adc_core.h"
    #include "dac_core.h"
    #endif
    
    /******************************************************************************/
    /************************ Variables Definitions *******************************/
    /******************************************************************************/
    #ifdef CONSOLE_COMMANDS
    extern command	  	cmd_list[];
    extern char			cmd_no;
    extern cmd_function	cmd_functions[11];
    unsigned char		cmd				 =  0;
    double				param[5]		 = {0, 0, 0, 0, 0};
    char				param_no		 =  0;
    int					cmd_type		 = -1;
    char				invalid_cmd		 =  0;
    char				received_cmd[30] = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
    										0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
    										0, 0, 0, 0, 0, 0, 0, 0, 0, 0};
    #endif
    
    
    ///////////////////////////////////////////////////////////
    //Added by Mable for Debug
    uint32_t	fn1,fn2,fn3;
    uint8_t tx_ch=0;
    uint8_t en_dis_fir;
    /////////////////////////////////////////////////////////////////////////////////////////
    AD9361_InitParam default_init_param = {
    	/* Device selection */
    	ID_AD9361,	// dev_sel
    	/* Identification number */
    	0,		//id_no
    	/* Reference Clock */
    	40000000UL,	//reference_clk_rate
    	/* Base Configuration */
    	0,//1,		//two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable
    	0,//1,		//one_rx_one_tx_mode_use_rx_num *** adi,1rx-1tx-mode-use-rx-num
    	0,//1,		//one_rx_one_tx_mode_use_tx_num *** adi,1rx-1tx-mode-use-tx-num
    	1,		//frequency_division_duplex_mode_enable *** adi,frequency-division-duplex-mode-enable
    	0,		//frequency_division_duplex_independent_mode_enable *** adi,frequency-division-duplex-independent-mode-enable
    	0,		//tdd_use_dual_synth_mode_enable *** adi,tdd-use-dual-synth-mode-enable
    	0,		//tdd_skip_vco_cal_enable *** adi,tdd-skip-vco-cal-enable
    	0,		//tx_fastlock_delay_ns *** adi,tx-fastlock-delay-ns
    	0,		//rx_fastlock_delay_ns *** adi,rx-fastlock-delay-ns
    	0,		//rx_fastlock_pincontrol_enable *** adi,rx-fastlock-pincontrol-enable
    	0,		//tx_fastlock_pincontrol_enable *** adi,tx-fastlock-pincontrol-enable
    	0,		//external_rx_lo_enable *** adi,external-rx-lo-enable
    	0,		//external_tx_lo_enable *** adi,external-tx-lo-enable
    	5,		//dc_offset_tracking_update_event_mask *** adi,dc-offset-tracking-update-event-mask
    	6,		//dc_offset_attenuation_high_range *** adi,dc-offset-attenuation-high-range
    	5,		//dc_offset_attenuation_low_range *** adi,dc-offset-attenuation-low-range
    	0x28,	//dc_offset_count_high_range *** adi,dc-offset-count-high-range
    	0x32,	//dc_offset_count_low_range *** adi,dc-offset-count-low-range
    	0,		//split_gain_table_mode_enable *** adi,split-gain-table-mode-enable
    	MAX_SYNTH_FREF,	//trx_synthesizer_target_fref_overwrite_hz *** adi,trx-synthesizer-target-fref-overwrite-hz
    	0,		// qec_tracking_slow_mode_enable *** adi,qec-tracking-slow-mode-enable
    	/* ENSM Control */
    	0,		//ensm_enable_pin_pulse_mode_enable *** adi,ensm-enable-pin-pulse-mode-enable
    	0,		//ensm_enable_txnrx_control_enable *** adi,ensm-enable-txnrx-control-enable
    	/* LO Control */
    	1450000000UL,//,	//rx_synthesizer_frequency_hz *** adi,rx-synthesizer-frequency-hz
    	1450000000UL,//1450000000UL,	//tx_synthesizer_frequency_hz *** adi,tx-synthesizer-frequency-hz
    	1,				//tx_lo_powerdown_managed_enable *** adi,tx-lo-powerdown-managed-enable
    	/* Rate & BW Control */
    	{0, 0, 0, 0, 0, 0},//{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies
    	{0, 0, 0, 0, 0, 0},//{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies
    	0,//3362055,//rf_rx_bandwidth_hz *** adi,rf-rx-bandwidth-hz
    	0,//3362055,//rf_tx_bandwidth_hz *** adi,rf-tx-bandwidth-hz
    	/* RF Port Control */
    	0,		//rx_rf_port_input_select *** adi,rx-rf-port-input-select
    	0,		//tx_rf_port_input_select *** adi,tx-rf-port-input-select
    	/* TX Attenuation Control */
    	7500,//7500,//10000,//1000,	//tx_attenuation_mdB *** adi,tx-attenuation-mdB
    	0,		//update_tx_gain_in_alert_enable *** adi,update-tx-gain-in-alert-enable
    	/* Reference Clock Control */
    	0,		//xo_disable_use_ext_refclk_enable *** adi,xo-disable-use-ext-refclk-enable
    	{7,5900},//{8, 5920},	//dcxo_coarse_and_fine_tune[2] *** adi,dcxo-coarse-and-fine-tune
    	CLKOUT_DISABLE,	//clk_output_mode_select *** adi,clk-output-mode-select
    	/* Gain Control */
    	2,		//gc_rx1_mode *** adi,gc-rx1-mode
    	2,		//gc_rx2_mode *** adi,gc-rx2-mode
    	58,		//gc_adc_large_overload_thresh *** adi,gc-adc-large-overload-thresh
    	4,		//gc_adc_ovr_sample_size *** adi,gc-adc-ovr-sample-size
    	47,		//gc_adc_small_overload_thresh *** adi,gc-adc-small-overload-thresh
    	8192,	//gc_dec_pow_measurement_duration *** adi,gc-dec-pow-measurement-duration
    	0,		//gc_dig_gain_enable *** adi,gc-dig-gain-enable
    	800,	//gc_lmt_overload_high_thresh *** adi,gc-lmt-overload-high-thresh
    	704,	//gc_lmt_overload_low_thresh *** adi,gc-lmt-overload-low-thresh
    	24,		//gc_low_power_thresh *** adi,gc-low-power-thresh
    	15,		//gc_max_dig_gain *** adi,gc-max-dig-gain
    	/* Gain MGC Control */
    	2,		//mgc_dec_gain_step *** adi,mgc-dec-gain-step
    	2,		//mgc_inc_gain_step *** adi,mgc-inc-gain-step
    	0,		//mgc_rx1_ctrl_inp_enable *** adi,mgc-rx1-ctrl-inp-enable
    	0,		//mgc_rx2_ctrl_inp_enable *** adi,mgc-rx2-ctrl-inp-enable
    	0,		//mgc_split_table_ctrl_inp_gain_mode *** adi,mgc-split-table-ctrl-inp-gain-mode
    	/* Gain AGC Control */
    	10,		//agc_adc_large_overload_exceed_counter *** adi,agc-adc-large-overload-exceed-counter
    	2,		//agc_adc_large_overload_inc_steps *** adi,agc-adc-large-overload-inc-steps
    	0,		//agc_adc_lmt_small_overload_prevent_gain_inc_enable *** adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable
    	10,		//agc_adc_small_overload_exceed_counter *** adi,agc-adc-small-overload-exceed-counter
    	4,		//agc_dig_gain_step_size *** adi,agc-dig-gain-step-size
    	3,		//agc_dig_saturation_exceed_counter *** adi,agc-dig-saturation-exceed-counter
    	1000,	// agc_gain_update_interval_us *** adi,agc-gain-update-interval-us
    	0,		//agc_immed_gain_change_if_large_adc_overload_enable *** adi,agc-immed-gain-change-if-large-adc-overload-enable
    	0,		//agc_immed_gain_change_if_large_lmt_overload_enable *** adi,agc-immed-gain-change-if-large-lmt-overload-enable
    	10,		//agc_inner_thresh_high *** adi,agc-inner-thresh-high
    	1,		//agc_inner_thresh_high_dec_steps *** adi,agc-inner-thresh-high-dec-steps
    	12,		//agc_inner_thresh_low *** adi,agc-inner-thresh-low
    	1,		//agc_inner_thresh_low_inc_steps *** adi,agc-inner-thresh-low-inc-steps
    	10,		//agc_lmt_overload_large_exceed_counter *** adi,agc-lmt-overload-large-exceed-counter
    	2,		//agc_lmt_overload_large_inc_steps *** adi,agc-lmt-overload-large-inc-steps
    	10,		//agc_lmt_overload_small_exceed_counter *** adi,agc-lmt-overload-small-exceed-counter
    	5,		//agc_outer_thresh_high *** adi,agc-outer-thresh-high
    	2,		//agc_outer_thresh_high_dec_steps *** adi,agc-outer-thresh-high-dec-steps
    	18,		//agc_outer_thresh_low *** adi,agc-outer-thresh-low
    	2,		//agc_outer_thresh_low_inc_steps *** adi,agc-outer-thresh-low-inc-steps
    	1,		//agc_attack_delay_extra_margin_us; *** adi,agc-attack-delay-extra-margin-us
    	0,		//agc_sync_for_gain_counter_enable *** adi,agc-sync-for-gain-counter-enable
    	/* Fast AGC */
    	64,		//fagc_dec_pow_measuremnt_duration ***  adi,fagc-dec-pow-measurement-duration
    	260,	//fagc_state_wait_time_ns ***  adi,fagc-state-wait-time-ns
    	/* Fast AGC - Low Power */
    	0,		//fagc_allow_agc_gain_increase ***  adi,fagc-allow-agc-gain-increase-enable
    	5,		//fagc_lp_thresh_increment_time ***  adi,fagc-lp-thresh-increment-time
    	1,		//fagc_lp_thresh_increment_steps ***  adi,fagc-lp-thresh-increment-steps
    	/* Fast AGC - Lock Level (Lock Level is set via slow AGC inner high threshold) */
    	1,		//fagc_lock_level_lmt_gain_increase_en ***  adi,fagc-lock-level-lmt-gain-increase-enable
    	5,		//fagc_lock_level_gain_increase_upper_limit ***  adi,fagc-lock-level-gain-increase-upper-limit
    	/* Fast AGC - Peak Detectors and Final Settling */
    	1,		//fagc_lpf_final_settling_steps ***  adi,fagc-lpf-final-settling-steps
    	1,		//fagc_lmt_final_settling_steps ***  adi,fagc-lmt-final-settling-steps
    	3,		//fagc_final_overrange_count ***  adi,fagc-final-overrange-count
    	/* Fast AGC - Final Power Test */
    	0,		//fagc_gain_increase_after_gain_lock_en ***  adi,fagc-gain-increase-after-gain-lock-enable
    	/* Fast AGC - Unlocking the Gain */
    	0,		//fagc_gain_index_type_after_exit_rx_mode ***  adi,fagc-gain-index-type-after-exit-rx-mode
    	1,		//fagc_use_last_lock_level_for_set_gain_en ***  adi,fagc-use-last-lock-level-for-set-gain-enable
    	1,		//fagc_rst_gla_stronger_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable
    	5,		//fagc_optimized_gain_offset ***  adi,fagc-optimized-gain-offset
    	10,		//fagc_rst_gla_stronger_sig_thresh_above_ll ***  adi,fagc-rst-gla-stronger-sig-thresh-above-ll
    	1,		//fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable
    	1,		//fagc_rst_gla_engergy_lost_goto_optim_gain_en ***  adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable
    	10,		//fagc_rst_gla_engergy_lost_sig_thresh_below_ll ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll
    	8,		//fagc_energy_lost_stronger_sig_gain_lock_exit_cnt ***  adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt
    	1,		//fagc_rst_gla_large_adc_overload_en ***  adi,fagc-rst-gla-large-adc-overload-enable
    	1,		//fagc_rst_gla_large_lmt_overload_en ***  adi,fagc-rst-gla-large-lmt-overload-enable
    	0,		//fagc_rst_gla_en_agc_pulled_high_en ***  adi,fagc-rst-gla-en-agc-pulled-high-enable
    	0,		//fagc_rst_gla_if_en_agc_pulled_high_mode ***  adi,fagc-rst-gla-if-en-agc-pulled-high-mode
    	64,		//fagc_power_measurement_duration_in_state5 ***  adi,fagc-power-measurement-duration-in-state5
    	/* RSSI Control */
    	1,		//rssi_delay *** adi,rssi-delay
    	1000,	//rssi_duration *** adi,rssi-duration
    	3,		//rssi_restart_mode *** adi,rssi-restart-mode
    	0,		//rssi_unit_is_rx_samples_enable *** adi,rssi-unit-is-rx-samples-enable
    	1,		//rssi_wait *** adi,rssi-wait
    	/* Aux ADC Control */
    	256,	//aux_adc_decimation *** adi,aux-adc-decimation
    	40000000UL,	//aux_adc_rate *** adi,aux-adc-rate
    	/* AuxDAC Control */
    	1,		//aux_dac_manual_mode_enable ***  adi,aux-dac-manual-mode-enable
    	0,		//aux_dac1_default_value_mV ***  adi,aux-dac1-default-value-mV
    	0,		//aux_dac1_active_in_rx_enable ***  adi,aux-dac1-active-in-rx-enable
    	0,		//aux_dac1_active_in_tx_enable ***  adi,aux-dac1-active-in-tx-enable
    	0,		//aux_dac1_active_in_alert_enable ***  adi,aux-dac1-active-in-alert-enable
    	0,		//aux_dac1_rx_delay_us ***  adi,aux-dac1-rx-delay-us
    	0,		//aux_dac1_tx_delay_us ***  adi,aux-dac1-tx-delay-us
    	0,		//aux_dac2_default_value_mV ***  adi,aux-dac2-default-value-mV
    	0,		//aux_dac2_active_in_rx_enable ***  adi,aux-dac2-active-in-rx-enable
    	0,		//aux_dac2_active_in_tx_enable ***  adi,aux-dac2-active-in-tx-enable
    	0,		//aux_dac2_active_in_alert_enable ***  adi,aux-dac2-active-in-alert-enable
    	0,		//aux_dac2_rx_delay_us ***  adi,aux-dac2-rx-delay-us
    	0,		//aux_dac2_tx_delay_us ***  adi,aux-dac2-tx-delay-us
    	/* Temperature Sensor Control */
    	256,	//temp_sense_decimation *** adi,temp-sense-decimation
    	1000,	//temp_sense_measurement_interval_ms *** adi,temp-sense-measurement-interval-ms
    	0xCE,	//temp_sense_offset_signed *** adi,temp-sense-offset-signed
    	1,		//temp_sense_periodic_measurement_enable *** adi,temp-sense-periodic-measurement-enable
    	/* Control Out Setup */
    	0xFF,	//ctrl_outs_enable_mask *** adi,ctrl-outs-enable-mask
    	0,		//ctrl_outs_index *** adi,ctrl-outs-index
    	/* External LNA Control */
    	0,		//elna_settling_delay_ns *** adi,elna-settling-delay-ns
    	0,		//elna_gain_mdB *** adi,elna-gain-mdB
    	0,		//elna_bypass_loss_mdB *** adi,elna-bypass-loss-mdB
    	0,		//elna_rx1_gpo0_control_enable *** adi,elna-rx1-gpo0-control-enable
    	0,		//elna_rx2_gpo1_control_enable *** adi,elna-rx2-gpo1-control-enable
    	0,		//elna_gaintable_all_index_enable *** adi,elna-gaintable-all-index-enable
    	/* Digital Interface Control */
    	0,//2,//0,		//digital_interface_tune_skip_mode *** adi,digital-interface-tune-skip-mode
    	0,		//digital_interface_tune_fir_disable *** adi,digital-interface-tune-fir-disable
    	1,		//pp_tx_swap_enable *** adi,pp-tx-swap-enable
    	1,		//pp_rx_swap_enable *** adi,pp-rx-swap-enable
    	0,		//tx_channel_swap_enable *** adi,tx-channel-swap-enable
    	0,		//rx_channel_swap_enable *** adi,rx-channel-swap-enable
    	1,		//rx_frame_pulse_mode_enable *** adi,rx-frame-pulse-mode-enable
    	0,		//two_t_two_r_timing_enable *** adi,2t2r-timing-enable
    	0,		//invert_data_bus_enable *** adi,invert-data-bus-enable
    	0,		//invert_data_clk_enable *** adi,invert-data-clk-enable
    	0,		//fdd_alt_word_order_enable *** adi,fdd-alt-word-order-enable
    	0,		//invert_rx_frame_enable *** adi,invert-rx-frame-enable
    	0,		//fdd_rx_rate_2tx_enable *** adi,fdd-rx-rate-2tx-enable
    	0,		//swap_ports_enable *** adi,swap-ports-enable
    	0,		//single_data_rate_enable *** adi,single-data-rate-enable
    	1,		//lvds_mode_enable *** adi,lvds-mode-enable
    	0,		//half_duplex_mode_enable *** adi,half-duplex-mode-enable
    	0,		//single_port_mode_enable *** adi,single-port-mode-enable
    	0,		//full_port_enable *** adi,full-port-enable
    	0,		//full_duplex_swap_bits_enable *** adi,full-duplex-swap-bits-enable
    	0,		//delay_rx_data *** adi,delay-rx-data
    	0,		//rx_data_clock_delay *** adi,rx-data-clock-delay
    	4,		//rx_data_delay *** adi,rx-data-delay
    	7,		//tx_fb_clock_delay *** adi,tx-fb-clock-delay
    	0,		//tx_data_delay *** adi,tx-data-delay
    #ifdef ALTERA_PLATFORM
    	300,	//lvds_bias_mV *** adi,lvds-bias-mV
    #else
    	150,	//lvds_bias_mV *** adi,lvds-bias-mV
    #endif
    	1,		//lvds_rx_onchip_termination_enable *** adi,lvds-rx-onchip-termination-enable
    	0,		//rx1rx2_phase_inversion_en *** adi,rx1-rx2-phase-inversion-enable
    	0xFF,	//lvds_invert1_control *** adi,lvds-invert1-control
    	0x0F,	//lvds_invert2_control *** adi,lvds-invert2-control
    	/* GPO Control */
    	0,		//gpo0_inactive_state_high_enable *** adi,gpo0-inactive-state-high-enable
    	0,		//gpo1_inactive_state_high_enable *** adi,gpo1-inactive-state-high-enable
    	0,		//gpo2_inactive_state_high_enable *** adi,gpo2-inactive-state-high-enable
    	0,		//gpo3_inactive_state_high_enable *** adi,gpo3-inactive-state-high-enable
    	0,		//gpo0_slave_rx_enable *** adi,gpo0-slave-rx-enable
    	0,		//gpo0_slave_tx_enable *** adi,gpo0-slave-tx-enable
    	0,		//gpo1_slave_rx_enable *** adi,gpo1-slave-rx-enable
    	0,		//gpo1_slave_tx_enable *** adi,gpo1-slave-tx-enable
    	0,		//gpo2_slave_rx_enable *** adi,gpo2-slave-rx-enable
    	0,		//gpo2_slave_tx_enable *** adi,gpo2-slave-tx-enable
    	0,		//gpo3_slave_rx_enable *** adi,gpo3-slave-rx-enable
    	0,		//gpo3_slave_tx_enable *** adi,gpo3-slave-tx-enable
    	0,		//gpo0_rx_delay_us *** adi,gpo0-rx-delay-us
    	0,		//gpo0_tx_delay_us *** adi,gpo0-tx-delay-us
    	0,		//gpo1_rx_delay_us *** adi,gpo1-rx-delay-us
    	0,		//gpo1_tx_delay_us *** adi,gpo1-tx-delay-us
    	0,		//gpo2_rx_delay_us *** adi,gpo2-rx-delay-us
    	0,		//gpo2_tx_delay_us *** adi,gpo2-tx-delay-us
    	0,		//gpo3_rx_delay_us *** adi,gpo3-rx-delay-us
    	0,		//gpo3_tx_delay_us *** adi,gpo3-tx-delay-us
    	/* Tx Monitor Control */
    	37000,	//low_high_gain_threshold_mdB *** adi,txmon-low-high-thresh
    	0,		//low_gain_dB *** adi,txmon-low-gain
    	24,		//high_gain_dB *** adi,txmon-high-gain
    	0,		//tx_mon_track_en *** adi,txmon-dc-tracking-enable
    	0,		//one_shot_mode_en *** adi,txmon-one-shot-mode-enable
    	511,	//tx_mon_delay *** adi,txmon-delay
    	8192,	//tx_mon_duration *** adi,txmon-duration
    	2,		//tx1_mon_front_end_gain *** adi,txmon-1-front-end-gain
    	2,		//tx2_mon_front_end_gain *** adi,txmon-2-front-end-gain
    	48,		//tx1_mon_lo_cm *** adi,txmon-1-lo-cm
    	48,		//tx2_mon_lo_cm *** adi,txmon-2-lo-cm
    	/* GPIO definitions */
    	-1,		//gpio_resetb *** reset-gpios
    	/* MCS Sync */
    	-1,		//gpio_sync *** sync-gpios
    	-1,		//gpio_cal_sw1 *** cal-sw1-gpios
    	-1,		//gpio_cal_sw2 *** cal-sw2-gpios
    	/* External LO clocks */
    	NULL,	//(*ad9361_rfpll_ext_recalc_rate)()
    	NULL,	//(*ad9361_rfpll_ext_round_rate)()
    	NULL	//(*ad9361_rfpll_ext_set_rate)()
    };
    
    /*AD9361_RXFIRConfig rx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // rx
    	0, // rx_gain
    	1, // rx_dec
    	{-4, -6, -37, 35, 186, 86, -284, -315,
    	 107, 219, -4, 271, 558, -307, -1182, -356,
    	 658, 157, 207, 1648, 790, -2525, -2553, 748,
    	 865, -476, 3737, 6560, -3583, -14731, -5278, 14819,
    	 14819, -5278, -14731, -3583, 6560, 3737, -476, 865,
    	 748, -2553, -2525, 790, 1648, 207, 157, 658,
    	 -356, -1182, -307, 558, 271, -4, 219, 107,
    	 -315, -284, 86, 186, 35, -37, -6, -4,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0}, // rx_coef[128]
    	 64, // rx_coef_size
    	 {0, 0, 0, 0, 0, 0}, //rx_path_clks[6]
    	 0 // rx_bandwidth
    };*/
    
    AD9361_RXFIRConfig rx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // rx
    	-6,//0, // rx_gain
    	2,//1,//2, // rx_dec
    	//{70,408,1071,1658,1335,-170,-1704,-1373,1077,2998,1213,-3542,-5574,627,13584,24378,24378,13584,627,-5574,-3542,1213,2998,1077,-1373,-1704,-170,1335,1658,1071,408,70,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	//{340,468,-408,-6,577,-846,406,676,-1673,1567,157,-2784,4305,-2210,-4932,21291,21291,-4932,-2210,4305,-2784,157,1567,-1673,676,406,-846,577,-6,-408,468,340,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0}, //DVBS2 Mod Data
    	{-18,-14,21,119,206,199,50,-130,-170,1,213,211,-61,-324,-240,174,467,232,-359,-628,-153,631,784,-40,-1006,-897,404,1498,909,-1031,-2144,-725,2124,3074,118,-4401,-4971,2029,14037,23383,23383,14037,2029,-4971,-4401,118,3074,2124,-725,-2144,-1031,909,1498,404,-897,-1006,-40,784,631,-153,-628,-359,232,467,174,-240,-324,-61,211,213,1,-170,-130,50,199,206,119,21,-14,-18,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	128,//128,//64, // rx_coef_size
    	{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},//{0, 0, 0, 0, 0, 0}, //rx_path_clks[6]
    	3362055 // rx_bandwidth
    };
    
    /*AD9361_TXFIRConfig tx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // tx
    	-6, // tx_gain
    	1, // tx_int
    	{-4, -6, -37, 35, 186, 86, -284, -315,
    	 107, 219, -4, 271, 558, -307, -1182, -356,
    	 658, 157, 207, 1648, 790, -2525, -2553, 748,
    	 865, -476, 3737, 6560, -3583, -14731, -5278, 14819,
    	 14819, -5278, -14731, -3583, 6560, 3737, -476, 865,
    	 748, -2553, -2525, 790, 1648, 207, 157, 658,
    	 -356, -1182, -307, 558, 271, -4, 219, 107,
    	 -315, -284, 86, 186, 35, -37, -6, -4,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0,
    	 0, 0, 0, 0, 0, 0, 0, 0}, // tx_coef[128]
    	 64, // tx_coef_size
    	 {0, 0, 0, 0, 0, 0}, // tx_path_clks[6]
    	 0 // tx_bandwidth
    };*/
    
    AD9361_TXFIRConfig tx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // tx
    	0,//0, // tx_gain
    	2,//1,//2 // tx_int
    	//{-8,-26,19,264,625,553,-358,-1236,-404,1875,2222,-1631,-5440,-1129,12640,25564,25564,12640,-1129,-5440,-1631,2222,1875,-404,-1236,-358,553,625,264,19,-26,-8,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},   //DVBS2 Mod Data
    	//{313,432,-346,-4,492,-731,364,562,-1432,1372,77,-2343,3749,-2133,-3769,20303,20303,-3769,-2133,3749,-2343,77,1372,-1432,562,364,-731,492,-4,-346,432,313,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	//{82,423,1069,1606,1262,-181,-1597,-1236,1063,2780,1014,-3413,-5103,1035,13477,23761,23761,13477,1035,-5103,-3413,1014,2780,1063,-1236,-1597,-181,1262,1606,1069,423,82,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	//{1,-6,-28,-62,-80,-56,11,68,54,-29,-98,-61,64,142,59,-122,-195,-35,210,246,-26,-329,-280,141,476,273,-326,-636,-193,595,786,3,-957,-889,351,1424,890,-953,-2027,-696,1997,2886,76,-4178,-4612,2199,13771,22755,22755,13771,2199,-4612,-4178,76,2886,1997,-696,-2027,-953,890,1424,351,-889,-957,3,786,595,-193,-636,-326,273,476,141,-280,-329,-26,246,210,-35,-195,-122,59,142,64,-61,-98,-29,54,68,11,-56,-80,-62,-28,-6,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	{0,-1,-4,-8,-10,-5,5,12,6,-10,-19,-6,19,28,2,-35,-37,8,57,45,-30,-86,-44,66,118,28,-120,-146,12,191,160,-85,-273,-145,197,353,83,-348,-412,44,531,423,-253,-730,-353,555,918,159,-958,-1052,211,1472,1078,-840,-2125,-900,1920,3034,290,-4144,-4814,1970,13765,22989,22989,13765,1970,-4814,-4144,290,3034,1920,-900,-2125,-840,1078,1472,211,-1052,-958,159,918,555,-353,-730,-253,423,531,44,-412,-348,83,353,197,-145,-273,-85,160,191,12,-146,-120,28,118,66,-44,-86,-30,45,57,8,-37,-35,2,28,19,-6,-19,-10,6,12,5,-5,-10,-8,-4,-1,0},
    	128,//64,//128,// 64, // tx_coef_size
    	{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000}, //{0, 0, 0, 0, 0, 0}, // tx_path_clks[6]
    	3362055 // tx_bandwidth
    };
    struct AD9361_TXFIRConfig *t1;
    struct ad9361_rf_phy *ad9361_phy;
    struct ad9361_rf_phy *phy1;
    #ifdef FMCOMMS5
    struct ad9361_rf_phy *ad9361_phy_b;
    #endif
    
    /***************************************************************************//**
     * @brief main
    *******************************************************************************/
    int main(void)
    {
    #ifdef XILINX_PLATFORM
    	Xil_ICacheEnable();
    	Xil_DCacheEnable();
    #endif
    
    #ifdef ALTERA_PLATFORM
    	if (altera_bridge_init()) {
    		printf("Altera Bridge Init Error!\n");
    		return -1;
    	}
    #endif
    
    	// NOTE: The user has to choose the GPIO numbers according to desired
    	// carrier board.
    	default_init_param.gpio_resetb = GPIO_RESET_PIN;
    #ifdef FMCOMMS5
    	default_init_param.gpio_sync = GPIO_SYNC_PIN;
    	default_init_param.gpio_cal_sw1 = GPIO_CAL_SW1_PIN;
    	default_init_param.gpio_cal_sw2 = GPIO_CAL_SW2_PIN;
    	default_init_param.rx1rx2_phase_inversion_en = 1;
    #else
    	default_init_param.gpio_sync = -1;
    	default_init_param.gpio_cal_sw1 = -1;
    	default_init_param.gpio_cal_sw2 = -1;
    #endif
    
    #ifdef LINUX_PLATFORM
    	gpio_init(default_init_param.gpio_resetb);
    #else
    	gpio_init(GPIO_DEVICE_ID);
    #endif
    	gpio_direction(default_init_param.gpio_resetb, 1);
    
    	spi_init(SPI_DEVICE_ID, 1, 0);
    
    	if (AD9364_DEVICE)
    		default_init_param.dev_sel = ID_AD9364;
    	if (AD9363A_DEVICE)
    		default_init_param.dev_sel = ID_AD9363A;
    
    #if defined FMCOMMS5 || defined ADI_RF_SOM || defined ADI_RF_SOM_CMOS
    	default_init_param.xo_disable_use_ext_refclk_enable = 1;
    #endif
    
    #ifdef ADI_RF_SOM_CMOS
    	default_init_param.swap_ports_enable = 1;
    	default_init_param.lvds_mode_enable = 0;
    	default_init_param.lvds_rx_onchip_termination_enable = 0;
    	default_init_param.full_port_enable = 1;
    	default_init_param.digital_interface_tune_fir_disable = 1;
    #endif
    
    	ad9361_init(&ad9361_phy, &default_init_param);
    
    	//ad9361_set_tx_fir_config(ad9361_phy, tx_fir_config);
    	//ad9361_set_rx_fir_config(ad9361_phy, rx_fir_config);
    	////////////////////////////////////////////////////////////////////////////////////////////////////
    	//Added by Mable
    	ad9361_trx_load_enable_fir(ad9361_phy, rx_fir_config, tx_fir_config) ;
    
        fn1=ad9361_get_tx_fir_en_dis(phy1,en_dis_fir);
    	fn2=ad9361_get_tx_fir_config(  phy1,  tx_ch,  t1);
    	printf("%d %d : fn1,fn2\n",fn1,fn2);
    
    	//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
    #ifdef FMCOMMS5
    #ifdef LINUX_PLATFORM
    	gpio_init(default_init_param.gpio_sync);
    #endif
    	gpio_direction(default_init_param.gpio_sync, 1);
    	default_init_param.id_no = 1;
    	default_init_param.gpio_resetb = GPIO_RESET_PIN_2;
    #ifdef LINUX_PLATFORM
    	gpio_init(default_init_param.gpio_resetb);
    #endif
    	default_init_param.gpio_sync = -1;
    	default_init_param.gpio_cal_sw1 = -1;
    	default_init_param.gpio_cal_sw2 = -1;
    	default_init_param.rx_synthesizer_frequency_hz = 2300000000UL;
    	default_init_param.tx_synthesizer_frequency_hz = 2300000000UL;
    	gpio_direction(default_init_param.gpio_resetb, 1);
    	ad9361_init(&ad9361_phy_b, &default_init_param);
    
    	ad9361_set_tx_fir_config(ad9361_phy_b, tx_fir_config);
    	ad9361_set_rx_fir_config(ad9361_phy_b, rx_fir_config);
    #endif
    
    #ifndef AXI_ADC_NOT_PRESENT
    #if defined XILINX_PLATFORM || defined LINUX_PLATFORM || defined ALTERA_PLATFORM
    #ifdef DAC_DMA_EXAMPLE
    #ifdef FMCOMMS5
    	dac_init(ad9361_phy_b, DATA_SEL_DMA, 0);
    #endif
    	dac_init(ad9361_phy, DATA_SEL_DMA, 1);
    #else
    #ifdef FMCOMMS5
    	dac_init(ad9361_phy_b, DATA_SEL_DDS, 0);
    #endif
    	dac_init(ad9361_phy, DATA_SEL_DDS, 1);
    #endif
    #endif
    #endif
    
    #ifdef FMCOMMS5
    	ad9361_do_mcs(ad9361_phy, ad9361_phy_b);
    #endif
    
    /*
    #ifndef AXI_ADC_NOT_PRESENT
    #if (defined XILINX_PLATFORM || defined ALTERA_PLATFORM) && defined ADC_DMA_EXAMPLE
        // NOTE: To prevent unwanted data loss, it's recommended to invalidate
        // cache after each adc_capture() call, keeping in mind that the
        // size of the capture and the start address must be alinged to the size
        // of the cache line.
    	mdelay(1000);
    	adc_capture(16384, ADC_DDR_BASEADDR);
    #ifdef XILINX_PLATFORM
    #ifdef FMCOMMS5
    	Xil_DCacheInvalidateRange(ADC_DDR_BASEADDR, 16384 * 16);
    #else
    	Xil_DCacheInvalidateRange(ADC_DDR_BASEADDR,
    			ad9361_phy->pdata->rx2tx2 ? 16384 * 8 : 16384 * 4);
    #endif
    #endif
    #endif
    #endif
    */
    
    #ifdef CONSOLE_COMMANDS
    	get_help(NULL, 0);
    
    	while(1)
    	{
    		console_get_command(received_cmd);
    		invalid_cmd = 0;
    		for(cmd = 0; cmd < cmd_no; cmd++)
    		{
    			param_no = 0;
    			cmd_type = console_check_commands(received_cmd, cmd_list[cmd].name,
    											  param, &param_no);
    			if(cmd_type == UNKNOWN_CMD)
    			{
    				invalid_cmd++;
    			}
    			else
    			{
    				cmd_list[cmd].function(param, param_no);
    			}
    		}
    		if(invalid_cmd == cmd_no)
    		{
    			console_print("Invalid command!\n");
    		}
    	}
    #endif
    
    	printf("Done.\n");
    
    #ifdef TDD_SWITCH_STATE_EXAMPLE
    	uint32_t ensm_mode;
    	if (!ad9361_phy->pdata->fdd) {
    		if (ad9361_phy->pdata->ensm_pin_ctrl) {
    			gpio_direction(GPIO_ENABLE_PIN, 1);
    			gpio_direction(GPIO_TXNRX_PIN, 1);
    			gpio_set_value(GPIO_ENABLE_PIN, 0);
    			gpio_set_value(GPIO_TXNRX_PIN, 0);
    			udelay(10);
    			ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    			printf("TXNRX control - Alert: %s\n",
    					ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    			mdelay(1000);
    
    			if (ad9361_phy->pdata->ensm_pin_pulse_mode) {
    				while(1) {
    					gpio_set_value(GPIO_TXNRX_PIN, 0);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX Pulse control - RX: %s\n",
    							ensm_mode == ENSM_MODE_RX ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX Pulse control - Alert: %s\n",
    							ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_TXNRX_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX Pulse control - TX: %s\n",
    							ensm_mode == ENSM_MODE_TX ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX Pulse control - Alert: %s\n",
    							ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    					mdelay(1000);
    				}
    			} else {
    				while(1) {
    					gpio_set_value(GPIO_TXNRX_PIN, 0);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX control - RX: %s\n",
    							ensm_mode == ENSM_MODE_RX ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					udelay(10);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX control - Alert: %s\n",
    							ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_TXNRX_PIN, 1);
    					udelay(10);
    					gpio_set_value(GPIO_ENABLE_PIN, 1);
    					udelay(10);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX control - TX: %s\n",
    							ensm_mode == ENSM_MODE_TX ? "OK" : "Error");
    					mdelay(1000);
    
    					gpio_set_value(GPIO_ENABLE_PIN, 0);
    					udelay(10);
    					ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    					printf("TXNRX control - Alert: %s\n",
    							ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    					mdelay(1000);
    				}
    			}
    		} else {
    			while(1) {
    				ad9361_set_en_state_machine_mode(ad9361_phy, ENSM_MODE_RX);
    				ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    				printf("SPI control - RX: %s\n",
    						ensm_mode == ENSM_MODE_RX ? "OK" : "Error");
    				mdelay(1000);
    
    				ad9361_set_en_state_machine_mode(ad9361_phy, ENSM_MODE_ALERT);
    				ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    				printf("SPI control - Alert: %s\n",
    						ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    				mdelay(1000);
    
    				ad9361_set_en_state_machine_mode(ad9361_phy, ENSM_MODE_TX);
    				ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    				printf("SPI control - TX: %s\n",
    						ensm_mode == ENSM_MODE_TX ? "OK" : "Error");
    				mdelay(1000);
    
    				ad9361_set_en_state_machine_mode(ad9361_phy, ENSM_MODE_ALERT);
    				ad9361_get_en_state_machine_mode(ad9361_phy, &ensm_mode);
    				printf("SPI control - Alert: %s\n",
    						ensm_mode == ENSM_MODE_ALERT ? "OK" : "Error");
    				mdelay(1000);
    			}
    		}
    	}
    #endif
    
    #ifdef XILINX_PLATFORM
    	Xil_DCacheDisable();
    	Xil_ICacheDisable();
    #endif
    
    #ifdef ALTERA_PLATFORM
    	if (altera_bridge_uninit()) {
    		printf("Altera Bridge Uninit Error!\n");
    		return -1;
    	}
    #endif
    
    	return 0;
    }
    

    After making these changes, initialization error is coming and invalid command print is coming continuously.Please find the attached log.

    ad9361_reset: by GPIO
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_setup
    ad9361_set_dcxo_tune : coarse 7 fine 5900
    ad9361_set_trx_clock_chain
    ad9361_set_trx_clock_chain: 0 0 0 0 0 0
    ad9361_set_trx_clock_chain: 0 0 0 0 0 0
    ad9361_bbpll_set_rate: Rate 715000000 Hz Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 715000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_round_rate: divide by zero
    ad9361_clk_factor_set_rate: Rate 89375000 Hz Parent Rate 89375000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_dig_tune: freq 0 flags 0x10
    
    ad9361_set_tx_atten : attenuation 89750 mdB tx1=1 tx2=1
    ad9361_bist_loopback: mode 0
    ad9361_bist_prbs: mode 2
    Device is in 0 state, forcing to 5
    Device is in 5 state, forcing to a
    Failed to restore state
    Nothing to do, device is already in 5 state
    Device is in 5 state, forcing to a
    Failed to restore state
    SAMPL CLK: 89375000 tuning: RX
      0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # # 
    1:# # # # # # # # # # # # # # # # 
    ad9361_dig_tune_delay: Tuning RX FAILED!
    ad9361_bist_loopback: mode 0
    Nothing to do, device is already in 5 state
    Could not restore to 0 ENSM state
    ad9361_set_tx_atten : attenuation 0 mdB tx1=1 tx2=1
    ad9361_rssi_setup
    ad9361_auxadc_setup
    ad9361_rf_port_setup : INPUT_SELECT 0x3
    ad9361_pp_port_setup
    ad9361_auxdac_setup
    ad9361_auxdac_set DAC1 = 0 mV
    ad9361_auxdac_set DAC2 = 0 mV
    ad9361_auxadc_setup
    ad9361_ctrl_outs_setup
    ad9361_gpo_setup
    ad9361_set_ref_clk_cycles : ref_clk_hz 40000000
    ad9361_clk_factor_set_rate: Rate 80000000 Hz Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 40000000 Hz
    ad9361_clk_factor_set_rate: Rate 80000000 Hz Parent Rate 40000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_txrx_synth_cp_calib : ref_clk_hz 80000000 : is_tx 0
    ad9361_txrx_synth_cp_calib : ref_clk_hz 80000000 : is_tx 1
    ad9361_rfpll_int_round_rate: Rate 725000000 Hz
    ad9361_rfpll_int_round_rate: Rate 725000000 Hz
    ad9361_rfpll_int_set_rate: RX Rate 725000000 Hz Parent Rate 80000000 Hz
    ad9361_fastlock_prepare: RX Profile 0: Un-Prepare
    ad9361_rfpll_vco_init : vco_freq 11600000000 : ref_clk 80000000 : range 2
    ad9361_rfpll_vco_init : freq 11588 MHz : index 3
    ad9361_load_gt: frequency 1450000000
    ad9361_load_gt: frequency 1450000000 (band 1)
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_round_rate: Rate 725000000 Hz
    ad9361_rfpll_int_set_rate: TX Rate 725000000 Hz Parent Rate 80000000 Hz
    ad9361_fastlock_prepare: TX Profile 0: Un-Prepare
    ad9361_rfpll_vco_init : vco_freq 11600000000 : ref_clk 80000000 : range 2
    ad9361_rfpll_vco_init : freq 11588 MHz : index 3
    ad9361_rfpll_vco_init : vco_freq 11600000000 : ref_clk 80000000 : range 2
    ad9361_rfpll_vco_init : freq 11588 MHz : index 3
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_clk_mux_set_parent: index 0
    Nothing to do, device is already in 5 state
    ad9361_trx_ext_lo_control : RX state 0
    ad9361_clk_mux_set_parent: index 0
    Nothing to do, device is already in 5 state
    ad9361_trx_ext_lo_control : TX state 0
    ad9361_load_mixer_gm_subtable
    ad9361_gc_setup
    ad9361_rx_bb_analog_filter_calib : rx_bb_bw 0 bbpll_freq 715000000
    ad9361_run_calibration: CAL Mask 0x80
    ad9361_tx_bb_analog_filter_calib : tx_bb_bw 0 bbpll_freq 715000000
    ad9361_run_calibration: CAL Mask 0x40
    ad9361_rx_tia_calib : bb_bw_Hz 0
    ad9361_tx_bb_second_filter_calib : tx_bb_bw 0
    ad9361_rx_adc_setup : BBBW 199790 : ADCfreq 89375000
    c3_msb 0x30 : c3_lsb 0xD : r2346 0x4 : 
    invrc_tconst_1e6 1023801, sqrt_inv_rc_tconst_1e3 1011
    scaled_adc_clk_1e6 139648, inv_scaled_adc_clk_1e3 7161
    tmp_1e3 1016, sqrt_term_1e3 373, min_sqrt_term_1e3 747
    ad9361_bb_dc_offset_calib
    ad9361_run_calibration: CAL Mask 0x1
    ad9361_rfpll_int_recalc_rate: Parent Rate 80000000 Hz
    ad9361_rf_dc_offset_calib : rx_freq 1450000000
    ad9361_run_calibration: CAL Mask 0x2
    Calibration TIMEOUT (0x16, 0x2)
    ad9361_init : AD936x initialization error
    2 : set filter config tx_fir_int!
    ad9361_load_fir_filter_coef: TAPS 128, gain 0, dest 3
    Device is in 3 state, forcing to 5
    Failed to restore state
    Could not restore to 3 ENSM state
    2 : rx_fir_dec!
    ad9361_load_fir_filter_coef: TAPS 128, gain -6, dest 131
    Device is in 3 state, forcing to 5
    Failed to restore state
    Could not restore to 3 ENSM state
    ad9361_validate_enable_fir: TX FIR EN=1/TAPS128/INT2, RX FIR EN=1/TAPS128/DEC2
    ad9361_set_trx_clock_chain
    ad9361_set_trx_clock_chain: 1024000000 64000000 32000000 16000000 8000000 4000000
    ad9361_set_trx_clock_chain: 1024000000 64000000 32000000 16000000 8000000 4000000
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 277133312 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_clk_factor_set_rate: Rate 4294967274 Hz Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_rfpll_int_recalc_rate: Parent Rate 0 Hz
    ad9361_dig_tune: freq 0 flags 0x10
    
    ad9361_set_tx_atten : attenuation 89750 mdB tx1=1 tx2=1
    ad9361_bist_loopback: mode 0
    ad9361_bist_prbs: mode 2
    Device is in 3 state, forcing to 5
    Failed to restore state
    Device is in 3 state, forcing to a
    Failed to restore state
    Device is in 3 state, forcing to 5
    Failed to restore state
    Device is in 3 state, forcing to a
    Failed to restore state
    SAMPL CLK: 0 tuning: RX
      0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # # 
    1:# # # # # # # # # # # # # # # # 
    ad9361_dig_tune_delay: Tuning RX FAILED!
    ad9361_bist_loopback: mode -1342177277
    Device is in 3 state, forcing to 5
    Failed to restore state
    Could not restore to 3 ENSM state
    ad9361_set_tx_atten : attenuation 0 mdB tx1=1 tx2=1
    ad9361_rssi_setup
    ad9361_auxadc_setup
    ad9361_tracking_control : bbdc_track=0, rfdc_track=0, rxquad_track=0
    Device is in 3 state, forcing to 5
    Failed to restore state
    __ad9361_update_rf_bandwidth: 3362055 3362055
    ad9361_rx_bb_analog_filter_calib : rx_bb_bw 1681027 bbpll_freq 0
    ad9361_run_calibration: CAL Mask 0x80
    ad9361_tx_bb_analog_filter_calib : tx_bb_bw 1681027 bbpll_freq 0
    ad9361_run_calibration: CAL Mask 0x40
    ad9361_rx_tia_calib : bb_bw_Hz 1681027
    ad9361_tx_bb_second_filter_calib : tx_bb_bw 1681027
    ad9361_rx_adc_setup : BBBW 0 : ADCfreq 0
    c3_msb 0x0 : c3_lsb 0x0 : r2346 0x1 : 
    invrc_tconst_1e6 4507, sqrt_inv_rc_tconst_1e3 67
    scaled_adc_clk_1e6 0, inv_scaled_adc_clk_1e3 0
    tmp_1e3 1000, sqrt_term_1e3 0, min_sqrt_term_1e3 0
    ad9361_tx_quad_calib : bw_tx 1681027 clkrf 0 clktf 0
    Tx NCO frequency: 0 (BW/4: 420256) txnco_word 0
    ad9361_run_calibration: CAL Mask 0x10
    LO leakage: 1 Quadrature Calibration: 1 : rx_phase 14
    ad9361_tracking_control : bbdc_track=176, rfdc_track=0, rxquad_track=164
    Could not restore to 3 ENSM state
    2 : get filter config rx_fir_int!
    0 0 : fn1,fn2
    Available commands:
    help?  - Displays all available commands.
    register?  - Gets the specified register value.
    tx_lo_freq?  - Gets current TX LO frequency [MHz].
    tx_lo_freq=  - Sets the TX LO frequency [MHz].
    tx_samp_freq?  - Gets current TX sampling frequency [Hz].
    tx_samp_freq=  - Sets the TX sampling frequency [Hz].
    tx_rf_bandwidth?  - Gets current TX RF bandwidth [Hz].
    tx_rf_bandwidth=  - Sets the TX RF bandwidth [Hz].
    tx1_attenuation?  - Gets current TX1 attenuation [mdB].
    tx1_attenuation=  - Sets the TX1 attenuation [mdB].
    tx2_attenuation?  - Gets current TX2 attenuation [mdB].
    tx2_attenuation=  - Sets the TX2 attenuation [mdB].
    tx_fir_en?  - Gets current TX FIR state.
    tx_fir_en=  - Sets the TX FIR state.
    rx_lo_freq?  - Gets current RX LO frequency [MHz].
    rx_lo_freq=  - Sets the RX LO frequency [MHz].
    rx_samp_freq?  - Gets current RX sampling frequency [Hz].
    rx_samp_freq=  - Sets the RX sampling frequency [Hz].
    rx_rf_bandwidth?  - Gets current RX RF bandwidth [Hz].
    rx_rf_bandwidth=  - Sets the RX RF bandwidth [Hz].
    rx1_gc_mode?  - Gets current RX1 GC mode.
    rx1_gc_mode=  - Sets the RX1 GC mode.
    rx2_gc_mode?  - Gets current RX2 GC mode.
    rx2_gc_mode=  - Sets the RX2 GC mode.
    rx1_rf_gain?  - Gets current RX1 RF gain.
    rx1_rf_gain=  - Sets the RX1 RF gain.
    rx2_rf_gain?  - Gets current RX2 RF gain.
    rx2_rf_gain=  - Sets the RX2 RF gain.
    rx_fir_en?  - Gets current RX FIR state.
    rx_fir_en=  - Sets the RX FIR state.
    dds_tx1_tone1_freq?  - Gets current DDS TX1 Tone 1 frequency [Hz].
    dds_tx1_tone1_freq=  - Sets the DDS TX1 Tone 1 frequency [Hz].
    dds_tx1_tone2_freq?  - Gets current DDS TX1 Tone 2 frequency [Hz].
    dds_tx1_tone2_freq=  - Sets the DDS TX1 Tone 2 frequency [Hz].
    dds_tx1_tone1_phase?  - Gets current DDS TX1 Tone 1 phase [degrees].
    dds_tx1_tone1_phase=  - Sets the DDS TX1 Tone 1 phase [degrees].
    dds_tx1_tone2_phase?  - Gets current DDS TX1 Tone 2 phase [degrees].
    dds_tx1_tone2_phase=  - Sets the DDS TX1 Tone 2 phase [degrees].
    dds_tx1_tone1_scale?  - Gets current DDS TX1 Tone 1 scale.
    dds_tx1_tone1_scale=  - Sets the DDS TX1 Tone 1 scale.
    dds_tx1_tone2_scale?  - Gets current DDS TX1 Tone 2 scale.
    dds_tx1_tone2_scale=  - Sets the DDS TX1 Tone 2 scale.
    dds_tx2_tone1_freq?  - Gets current DDS TX2 Tone 1 frequency [Hz].
    dds_tx2_tone1_freq=  - Sets the DDS TX2 Tone 1 frequency [Hz].
    dds_tx2_tone2_freq?  - Gets current DDS TX2 Tone 2 frequency [Hz].
    dds_tx2_tone2_freq=  - Sets the DDS TX2 Tone 2 frequency [Hz].
    dds_tx2_tone1_phase?  - Gets current DDS TX2 Tone 1 phase [degrees].
    dds_tx2_tone1_phase=  - Sets the DDS TX2 Tone 1 phase [degrees].
    dds_tx2_tone2_phase?  - Gets current DDS TX2 Tone 2 phase [degrees].
    dds_tx2_tone2_phase=  - Sets the DDS TX2 Tone 2 phase [degrees].
    dds_tx2_tone1_scale?  - Gets current DDS TX2 Tone 1 scale.
    dds_tx2_tone1_scale=  - Sets the DDS TX2 Tone 1 scale.
    dds_tx2_tone2_scale?  - Gets current DDS TX2 Tone 2 scale.
    dds_tx2_tone2_scale=  - Sets the DDS TX2 Tone 2 scale.
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    Invalid command!
    

  • Hi,

    Waiting for the response from your side.

    Thanks,

    Mable George

Reply Children
  • 0
    •  Analog Employees 
    on Oct 3, 2019 11:41 AM over 1 year ago in reply to mgeorge@cdot.in

    You can't initialize the part to a 0 Hz sampling rate.

    Don't modify anything to default_init_param - generate your own FIR configuration files and load/enable them using ad9361_trx_load_enable_fir().

    Dragos

  • Hi,

    If we don't modify anything in default_init_param , where we  can set rx_synthesizer_frequency_hz,tx_synthesizer_frequency_hz,tx_attenuation_mdB?

    As per your suggestion without modifying anything in default_init_param and loaded using ad9361_trx_load_enable_fir(). Instead of  taking tx_samp_freq,rx_samp_freq, etc from FIR filter structure  it is  taking from  default_init_param.

    Please see the attached filter structures and provide the feedback.

    AD9361_TXFIRConfig tx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // tx
    	0, // tx_gain
    	2,// tx_int
    	{0,-1,-4,-8,-10,-5,5,12,6,-10,-19,-6,19,28,2,-35,-37,8,57,45,-30,-86,-44,66,118,28,-120,-146,12,191,160,-85,-273,-145,197,353,83,-348,-412,44,531,423,-253,-730,-353,555,918,159,-958,-1052,211,1472,1078,-840,-2125,-900,1920,3034,290,-4144,-4814,1970,13765,22989,22989,13765,1970,-4814,-4144,290,3034,1920,-900,-2125,-840,1078,1472,211,-1052,-958,159,918,555,-353,-730,-253,423,531,44,-412,-348,83,353,197,-145,-273,-85,160,191,12,-146,-120,28,118,66,-44,-86,-30,45,57,8,-37,-35,2,28,19,-6,-19,-10,6,12,5,-5,-10,-8,-4,-1,0},
    	128, // tx_coef_size
    	{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},  // tx_path_clks[6]
    	3362055 // tx_bandwidth
    };
    
    AD9361_RXFIRConfig rx_fir_config = {	// BPF PASSBAND 3/20 fs to 1/4 fs
    	3, // rx
    	-6,// rx_gain
    	2, // rx_dec
    	{-18,-14,21,119,206,199,50,-130,-170,1,213,211,-61,-324,-240,174,467,232,-359,-628,-153,631,784,-40,-1006,-897,404,1498,909,-1031,-2144,-725,2124,3074,118,-4401,-4971,2029,14037,23383,23383,14037,2029,-4971,-4401,118,3074,2124,-725,-2144,-1031,909,1498,404,-897,-1006,-40,784,631,-153,-628,-359,232,467,174,-240,-324,-61,211,213,1,-170,-130,50,199,206,119,21,-14,-18,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    	128, // rx_coef_size
    	{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000}, //rx_path_clks[6]
    	3362055 // rx_bandwidth
    };

  • 0
    •  Analog Employees 
    on Oct 8, 2019 3:02 PM over 1 year ago in reply to mgeorge@cdot.in
    If we don't modify anything in default_init_param , where we  can set rx_synthesizer_frequency_hz,tx_synthesizer_frequency_hz,tx_attenuation_mdB?

    You need to use the regular driver API to do that.

  • Hi,

    Problem got resolved. Thanks for the help.

    Thanks,

    Mable George