AD9361 TXFIR int 0 RXFIR dec 0 mode Highest OSR

Hi,

These are the inputs given by us for configuring AD9361.

{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies 

{1024000000, 64000000, 32000000, 16000000, 8000000, 4000000},// tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies

AD9361_TXFIRConfig tx_fir_config = {    // BPF PASSBAND 3/20 fs to 1/4 fs
    1, // tx
    -6,  tx_gain
    2 ,//tx_int
{1,-6,-28,-62,-80,-56,11,68,54,-29,-98,-61,64,142,59,-122,-195,-35,210,246,-26,-329,-280,141,476,273,-326,-636,-193,595,786,3,-957,-889,351,1424,890,-953,-2027,-696,1997,2886,76,-4178,-4612,2199,13771,22755,22755,13771,2199,-4612,-4178,76,2886,1997,-696,-2027,-953,890,1424,351,-889,-957,3,786,595,-193,-636,-326,273,476,141,-280,-329,-26,246,210,-35,-195,-122,59,142,64,-61,-98,-29,54,68,11,-56,-80,-62,-28,-6,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0},
    128, // tx_coef_size
    {1024000000, 64000000, 32000000, 16000000, 8000000, 4000000}, //{0, 0, 0, 0, 0, 0}, // tx_path_clks[6]
     1330000 // tx_bandwidth
};

but we are getting error ad9361_calculate_rf_clock_chain: requested rate 4000000 TXFIR int 0 RXFIR dec 0 mode Highest OSR
ad9361_calculate_rf_clock_chain: Failed to find suitable dividers: ADC clock below limit".

please give the feedback how to solve thiis error.

Top Replies

Parents Reply Children
  • 0
    •  Analog Employees 
    on Sep 20, 2019 12:15 PM over 1 year ago in reply to mgeorge@cdot.in

    Can you please share the profile you have generated from filter wizard tool?

  • 2388.rx_profile.txt
    Filter = 2
    Phase Equalization = 0
    Use AD936x FIR = 1
    Fpass = 1.333300e+00
    Fstop = 1.666700e+00
    Apass = 5.000000e-01
    Astop = 80
    Param = 0.000000
    PLL rate  = 1024
    Converter = 64
    Data rate = 4
    
    4380.tx_profile.txt
    Filter = 2
    Phase Equalization = 0
    Use AD936x FIR = 1
    Fpass = 1.333300e+00
    Fstop = 1.666700e+00
    Apass = 5.000000e-01
    Astop = 80
    Param = 0.000000
    PLL rate  = 1024
    Converter = 64
    Data rate = 4
    

    Please find the attached document with filter parameters for both transmit and receive .

  • This is the settings provided in AD9361_Filter_Wizard GUI

  • One of the observation which I made now is

    While setting FIR filter parameters I'm using the function of ad9361_set_tx_fir_config(ad9361_phy, tx_fir_config);. That time I'm setting tx_int as 2. But While reading back using fn2=ad9361_get_tx_fir_config(  phy1,  tx_ch,  t1); I'm getting interpolation as 0. What might be the possible  reasons for that? Why assigned value is not reflecting ?

    How can I verify the other parameters which I used to initialize AD9361 has reflected or not?

  • 0
    •  Analog Employees 
    on Sep 23, 2019 12:11 PM over 1 year ago in reply to mgeorge@cdot.in

    6431.ezone1.txt
    # Generated with AD9361 Filter Design Wizard 16.1.3
    # MATLAB 9.0.0.341360 (R2016a), 23-Sep-2019 11:41:42
    # Inputs:
    # Data Sample Frequency = 4000000 Hz
    TX 3 GAIN 0 INT 2
    RX 3 GAIN -6 DEC 2
    RTX 1024000000 64000000 32000000 16000000 8000000 4000000
    RRX 1024000000 64000000 32000000 16000000 8000000 4000000
    BWTX 3362055
    BWRX 3362068
    0,-18
    -1,-14
    -4,21
    -8,119
    -10,206
    -5,199
    5,50
    12,-130
    6,-170
    -10,1
    -19,213
    -6,211
    19,-61
    28,-324
    2,-240
    -35,174
    -37,467
    8,232
    57,-359
    45,-628
    -30,-153
    -86,631
    -44,784
    66,-40
    118,-1006
    28,-897
    -120,404
    -146,1498
    12,909
    191,-1031
    160,-2144
    -85,-725
    -273,2124
    -145,3074
    197,118
    353,-4401
    83,-4971
    -348,2029
    -412,14037
    44,23383
    531,23383
    423,14037
    -253,2029
    -730,-4971
    -353,-4401
    555,118
    918,3074
    159,2124
    -958,-725
    -1052,-2144
    211,-1031
    1472,909
    1078,1498
    -840,404
    -2125,-897
    -900,-1006
    1920,-40
    3034,784
    290,631
    -4144,-153
    -4814,-628
    1970,-359
    13765,232
    22989,467
    22989,174
    13765,-240
    1970,-324
    -4814,-61
    -4144,211
    290,213
    3034,1
    1920,-170
    -900,-130
    -2125,50
    -840,199
    1078,206
    1472,119
    211,21
    -1052,-14
    -958,-18
    159,0
    918,0
    555,0
    -353,0
    -730,0
    -253,0
    423,0
    531,0
    44,0
    -412,0
    -348,0
    83,0
    353,0
    197,0
    -145,0
    -273,0
    -85,0
    160,0
    191,0
    12,0
    -146,0
    -120,0
    28,0
    118,0
    66,0
    -44,0
    -86,0
    -30,0
    45,0
    57,0
    8,0
    -37,0
    -35,0
    2,0
    28,0
    19,0
    -6,0
    -19,0
    -10,0
    6,0
    12,0
    5,0
    -5,0
    -10,0
    -8,0
    -4,0
    -1,0
    0,0
    

    Can you try loading the attached filter file and check. It is created with the same settings as yours.