KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hello,
We are using the ADRV9361-Z7035 with the FMC carrier in LVDS mode. We are trying to insert a custom IP block between the AXI_AD9361 and the adjacent FIFO IP blocks that performs RX to TX loopback with a user-controlled phase shift. Our custom IP block accepts adc_data_i0 and adc_data_q0 and returns the phase-shifted I/Q samples to dac_data_i0 and dac_data_q0. It is my understanding that by default, adc_data_* is 12-bit 2's compliment sign-extended to 16-bits and dac_data_* is 16-bit 2's compliment where only the upper 12 bits are used by the AXI_AD9361 core. However, it appears that when our IP block writes negative values to dac_data_* the AD9361 interface can't handle the data format.
As a quick example, suppose the incoming I/Q sample from AXI_AD9361 is (1000,0) and we phase shift it by 180 degrees. Only focusing on the I-component...
adc_data_i0 = +1000 or 0x03e8
180 degree phase shift results in -1000 or 0xfc18
and dac_data_i0 gets 0xc180 (left shifted by 4 bits)
1. Is this the correct understanding of how the 16-bit I/Q samples get read and written to the AXI_AD9361 block?
2. Can you confirm the following for RX and TX paths?
RX: LVDS -> 12 bit offset binary -> 16 bit 2's compliment
TX: 16 bit 2's compliment -> 12 bit 2's compliment (top 12 bits) -> LVDS
3. For the built-in RX -> TX loopback, can you confirm that the 48-bit "adc_data" loopback signal always contains 12-bit offset binary?
Thanks,
Glen
Hi,
even if the HDL contains programmable formatter cores to support both 2's complement and offset binary, the Rx chain is configured to 2's complement by software. See how the formatter is configured in no-Os here: https://github.com/analogdevicesinc/linux/blob/master/drivers/iio/adc/ad9361_conv.c#L705
From what I see the loopback should be as follows:
(RX) LVDS -> 12 bit 2's compliment -> 16 bit 2's compliment -> take 12 LSB [your IP] drive 12 MSB -> 16 bit 2's compliment -> 12 bit 2's compliment (top 12 bits) -> LVDS (TX)
Laszlo