Post Go back to editing

ADRV9009 Rebro on Modified Reference HDL

Hi,

I'm using a ZCU102 +ADRV9009 combination, using the reference hdl design and no-os SDK setup. I'm trying to setup a design that does receives the RX signal all the signal processing on the FPGA PL fabric and sends it back into the TX chain to transmit out. 

from what i understand so far

  • the clock on the rx is 122.88MHz, which is double the one on the tx which is running on 61.44MHz
  • but the data rate of the ADC and DACs on the adrv9009 is at 122.88MHz at 16 bit resolution
  • hence, the data on the tx is 2 samples of 32 bits per channel per clock cycle (2 samples*2 channels*2IQ*16bits=128 bits)
  • whereas, data on the rx is 1 sample of 32 bits per channel per clock cycle (1 samples*2 channels*2IQ*16bits=64 bits)

please correct me if there is any mistakes in my assumptions so far. 

I have pulled out the RX signal from the axi_adrv9009_core module in the block design and have managed to observe the signal in the FPGA. I am experimenting on how to reinject this signal back into the TX chain within the FPGA, but to no avail. I'll probably need information on the following:

  • the bit-level arrangement/format of the tx input
    • how the IQ data fits into the 128 bits per clock cycle, if there is an IQ stream of data
  • the location where i can inject a RF signal into the TX chain
  • how do we pack the Tx samples appropriately (i.e. how does the tx on the adrv9009 read the 2 samples in the frame & in which order?)

Thanks in advance

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.