Post Go back to editing

ADRV9009 Rebro on Modified Reference HDL

Hi,

I'm using a ZCU102 +ADRV9009 combination, using the reference hdl design and no-os SDK setup. I'm trying to setup a design that does receives the RX signal all the signal processing on the FPGA PL fabric and sends it back into the TX chain to transmit out. 

from what i understand so far

  • the clock on the rx is 122.88MHz, which is double the one on the tx which is running on 61.44MHz
  • but the data rate of the ADC and DACs on the adrv9009 is at 122.88MHz at 16 bit resolution
  • hence, the data on the tx is 2 samples of 32 bits per channel per clock cycle (2 samples*2 channels*2IQ*16bits=128 bits)
  • whereas, data on the rx is 1 sample of 32 bits per channel per clock cycle (1 samples*2 channels*2IQ*16bits=64 bits)

please correct me if there is any mistakes in my assumptions so far. 

I have pulled out the RX signal from the axi_adrv9009_core module in the block design and have managed to observe the signal in the FPGA. I am experimenting on how to reinject this signal back into the TX chain within the FPGA, but to no avail. I'll probably need information on the following:

  • the bit-level arrangement/format of the tx input
    • how the IQ data fits into the 128 bits per clock cycle, if there is an IQ stream of data
  • the location where i can inject a RF signal into the TX chain
  • how do we pack the Tx samples appropriately (i.e. how does the tx on the adrv9009 read the 2 samples in the frame & in which order?)

Thanks in advance

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.