ADRV9009 SPI error -5

Hello,

We have the ADRV9009+ZCU102 example design working fine. We made some changes to it and now we're getting AD9528 failed with error -5.

We probed the AD9528 CSN, SCLK, DIN and we are getting exactly the same waveforms.

In our modified design, the DOUT from AD9528 is always zero. Due to this, iio_driver fails with an error.

The other difference between the two designs is that in the working example design, the SPI activity is observed at time of 4 (after kernel starts), whereas in our modified design, the SPI activity happens immediately after the kernel starts. Probably at this time, AD9528 is not ready? Why is there this difference when only the bitstream is different (not the kernel image)?

How do we solve our problem? Can we somehow delay the iio_driver? Can we manually restart the iio_driver after the system boots completely?

Top Replies