AD9371 Zynq evaluation vs No-OS/hdl_2018_r1 design

The AD9371 Zynq evaluation code loaded from the SD card seems to be much more mature and fully functioning than the hdl_2018_r1 FPGA code and No-OS software available in the repository. For example, the No-OS/hdl_2018_r1 configuration seems to require a 2R2T configuration while the Zynq evaluation image seems to support a 1R1T configuration (using the Transceiver Evaluation Software for configuration).

1. Does the AD9371 Zynq evaluation platform use a different code base (HDL and API) than the No-OS/hdl_2018_r1 repository?

2. If so, is that code base available? for FPGA code? for API code? for TES application?

3. Does Analog Devices plan to modify the No-OS/hdl code to support the configuration options available in TES?

We're specifically interested in

1. moving to a 1R1T configuration with reduced JESD lane rates (using 4 JESD lanes)

2. supporting a 1R1T configuration over 2 JESD lanes

thanks.

Parents Reply Children
No Data