I am working on ADRV9361-z7035 with HDL release (2018_r1) . And I am using Linux version .
I want to verify the RX path . by injecting a RF signal of a particular frequency on RX port.bring received signal to
FFT core , and processing it . and verify the frequency component (using ILA ) .
So for my understing from the forum threads is
recommended place to put FFT IP is AD9361 Interface ---> FIFO ---> FFT IP ----> DMA controller ---> Interconnect back to PS.
So it is the correct dataflow to implement FFT core.
Note : I am using Linux version design . Not No-Os
Regards