AD-FMCOMMS4-EBZ with Xilinx Artix-7 FPGA AC701 Evaluation Kit

Good morning,

I have just received an AD-FMCOMMS4-EBZ FMC Module and I am trying to use the HDL Reference Designs provided by Analog (Reference link: wiki.analog.com/.../reference_hdl)

I am using Vivado 2018.1 and I the hdl-2017_r1 archive (because newer does not support anymore the AC701 board).

When I launch the make inside the projects/FMCOMMS2/ac701 folder, the process give an Error 139 which consists in an "Abnormal Program Termination (11)" in the log file of the axi_ad9361.

I have also tried to launch the single tcl scripts to build the libraries but after some seconds Vivado exits for a crash.

Have you got some suggestions to run this demo example?

One of the reason I have bought the FCM module is the compatibility with the AC701 board for SDR applications.

Otherwise, do you have an already compiled and working project for Vivado only for this specific platform?

Thank you in advance for cooperation.

Best Regards,

Andrea