Hi,
I'm unable to boot up ADRV9361-7035 board. This board was working fine previously but not booting up now. I have two boards. One is working fine and other got problem. I have checked all the switch positions and they are fine according to guide (snap attached). I connected this board to vivado but got error "No device Detected" (please check vivado.png attached). I tired to use serial console but got nothing on console. Currently, LED DS8 and DS3 is on and red, LED D3 is on and green. Image attached.
Please help me solve this problem.
BR
Hi,You need a JTAG cable to connect your device to Vivado. In the picture is not connected.I see you have a micro SD card can you plug it directly in the adrv9361_z7036 board, not in the carrier?Andrei
Now connected JTAG cable also and insert board also ,not in carrier ,previously it was in carrier .but still the board is not detected
Hi,It is hard to distinguish the position of the switches in the above pic.On the SOM you can see a small table to the right of the S4 and S3, under U13.You can choose between booting from SD card and using JTAG, not both.Starting from the last config (SD on SOM), can you set S1 to SDS, S3 and S4 to 1. What messages do you get on the UART?
https://wiki.analog.com/resources/tools-software/linux-software/embedded_arm_images?s[]=zynq&s[]=soc&s[]=quick
Is the CFG DONE blue LED on?For JTAG (only) S3 and S4 will be in position 0.Andrei
S4 and S3 are set to 1 (booting from SD card). S1 is set to SDS. CFG DONE blue led is off. I receive nothing on UART.
If you set the switches for JTAG, can you connect to the device?Andrei