| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
AD9528
Recommended for New Designs
The AD9528 is a two-stage PLL with an integrated JESD204B/JESD204C SYSREF generator for multiple device synchronization. The first stage phase-locked loop...
Datasheet
AD9528 on Analog.com
I'm interested in designing an FMC card with 4 RX coherent channels for MIMO using two ADRV9009 chips. Are there are any design considerations for doing so? My team has done this with the AD9361 using the FMCOMMS5 as a basis. The axi_ad9361 core provided the l_clk output and clk input ports to control clocking between two chips and software handled the multichip synchronization procedure to phase lock the RX clocks. Is there an equivalent with the axi_adrv9009 core?
My current design approach is as follows:
Here's a rough block diagram:

My questions for my clarification:
Hello,
We have under development a branch for a project that has two adrv9009's on the same board: https://github.com/analogdevicesinc/hdl/tree/prototype_som_2018_r2 .We are still working on software, testing and validation, but this is the architecture that we think will work with our JESD204B Interface framework.
Your approach seems fine.
For sample level deterministic latency, the device clock (driving what currently is driven by axi_adrv9009_rx_clkgen/clk_0) should be generated along with sysref by the AD9528, and not by clockgen. We are using it because we only have a reference clock and may configure RX/TX/OBS with different rates and we don't have additional clocks from the AD9528 to FPGA. Depending on the FPGA you are using and the sampling rates, the device clock can be the same with the transceiver reference clock or it can be a different clock all together, being fed to the FPGA through a clock capable pin.
Maybe somebody from the https://ez.analog.com/wide-band-rf-transceivers/design-support-adrv9008-1-adrv9008-2-adrv9009/ forum can give additional pointers regarding getting coherent RX data from the chip.
Regards,
Adrian
Hi,
On similar lines, we are working on a design that will have 4x adrv9009 for 8x coherent channels. Having a look at the prototype branch, at the moment that axi_adrv9009 core allows control allows for single or dual chips.
If we were to want to use 4 chips I guess we would need to expand this axi_adrv9009 IP to work with n channels effectively?
Do you have any plans to work on support for this yourself? I think that the proposed adrv9009-ZU11EG module would support adding an additional card for 4 chips in total?
Thanks,
Mark
Great, thanks
One more question, will there be support for this/any modifications required in the iio framework?
Yes, we'll continue to update the iio framework and use it as part of our projects, so that's going to use to test the changes.
Regards,
Adrian
There will be some support to sync multiple ADRV9009 device instances.
This is currently work in progress and basic support will be available in the coming weeks.
-Michael
Hi, what is the current status of the multi chip work?
Hello,
It is still under development.
The latest changes can be found at: https://github.com/analogdevicesinc/hdl/tree/talise_som , https://github.com/analogdevicesinc/linux/tree/adrv9009-zu11eg and https://github.com/analogdevicesinc/iio-oscilloscope .
Regards,
Adrian
Can someone please help me to access these links !
I'm always getting "page not found".
thanks
Hello,
Now you can find the sources in the links below, they've been merged into master.
And the documentation for them:
https://wiki.analog.com/resources/eval/user-guides/adrv9009-zu11eg
https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms8-ebz
Regards,
Iulia
Hello mhennerich AdrianC ,
I see the above links shows a design project for ADRV9009-ZU11EG. However I don't see a project inside.
Besides, I am interested on having a design for 2 ADRV9009's on a ZCU102.
any updates on the design for 2 ADRV9009's on ZCU102?
Thanks
Hello viggy ,
AD-FMCOMMS8 has 2 ADRV9009, and we support it on ZCU102. Check the link from my previous comment.
Regards,
Iulia
Hello viggy ,
AD-FMCOMMS8 has 2 ADRV9009, and we support it on ZCU102. Check the link from my previous comment.
Regards,
Iulia
Actually we have the ADRV9009-W/PCBZ board. Our intention is to use two of these boards on the same ZCU102 platform connected through HPC0 and HPC1 ports. Is it possible to do so? If yes, is any HDL design available for the same?
Thanks,
Vignesh
Hello, actually we have the same problem Viggy had, our intention is to use two ADRV9009-W/PCBZ board on the same ZCU102 platform connected through HPC0 and HPC1 ports. Is it possible to do so? If yes, is any HDL design available for this scope ?