Post Go back to editing

Square wave output using fmcdaq2

Thread Summary

The user wanted to output a 1 kHz square wave from the AD9144 DAC on the FMCDAQ2 board. The solution involved modifying the HDL to add a square wave generator using the `dac_dds_phase_0_0` signal and setting the `dac_data_sel_s` to `4'h3` to select the square wave output. The user also needed to ensure the JESD link was properly configured and the DDS frequency was set correctly. Oscillations in the square wave output were resolved by further adjustments to the HDL and ensuring the DAC's output filters were appropriate for the low-frequency square wave.
AI Generated Content

Dear EngineerZone community


Please support.

I am currently creating a communication system.
The concept is to generate an information signal with vc707 and output it as a Square wave from the DAC (ad 9144) of fmcdaq2. Then, the output Square wave is input to the modulator and communication is carried out.

Before that, I am trying to output a Square wave of 1 kHz (offset 0V) from DAC (AD9144) of fmcdaq2.
How can I do it?

Can you create a design as per the user guide and store a Square wave in the buffer?

I can use both Linux / no-OS.

Yuta

Parents
  • Hi,

    I'm confused, ad9144 is a high speed dac (1GSPS), why do you want it to output a squarewave of 1KHz?
    The daq2 board has some filters on the output, you will have to change those to be able to transmit a sqare wave.

    Take a look at https://ez.analog.com/fpga/f/q-a/81027/daq2-kcu105-send-data-to-dac


    Are you familiar with our RF designs? If not, it may be of interest to you.

    www.analog.com/en/products/adrv9008-2.html

    www.analog.com/.../ad9361.html
    wiki.analog.com/.../adrv936x_rfsom

    Andrei

  • Thank you,Andrei

    I am sorry for confusing you.I wanted to generate a square wave of 1 kHz because the modulator used operates by inputting a square wave of about 1 kHz to 2 kHz.

    However, since the ADC/DAC I have is fmcdaq2, I would like to know haw to output a 1 kHz Square wave using fmcdaq2.

    I'm sorry. I looked at https://ez.analog.com/fpga/f/q-a/81027/daq2-kcu105-send-data-to-dac and I saw the URL and could understand changing the filter of fmcdaq2, but I could not understand which part to change specifically.

    Please tell me.

    Yuta

  • Hi,

    After programming to the FPGA, I tried using xdbd.
    The results are shown below.

    xsdb% connect                                                                   
    tcfchan#0                                                                       
    xsdb% target                                                                    
      1  xc7vx485t
         2  MicroBlaze Debug Module at USER2
            3  MicroBlaze #0 (Stop)
    xsdb% target 3                                                                  
    xsdb% mrd -force 0x44A00000                                                     
    44A00000:   DEADDEAD
    
    xsdb% mrd -force 0x44A10000                                                     
    44A10000:   000A0062
    
    xsdb% mrd -force 0x44A04418                                                     
    44A04418:   00000000
    
    xsdb% mwr -force 0x44A04418 0x3                                                 
    xsdb% mrd -force 0x44A04418                                                     
    44A04418:   00000003
    
    xsdb% exit                                                                      
    exit

    After that I ran with SDK, but as before, PN mismatch occurred.

    Available sampling rates:
    	1 - ADC 1000 MSPS; DAC 1000 MSPS
    	2 - ADC  500 MSPS; DAC 1000 MSPS
    	3 - ADC  500 MSPS; DAC  500 MSPS
    	4 - ADC  600 MSPS; DAC  600 MSPS
    choose an option [default 1]:
    3 - ADC  500 MSPS; DAC  500 MSPS
    
    CPLL ENABLE
    
    CPLL ENABLE
    Tx link is enabled
    Measured Link Clock: 125 MHz
    Link status: DATA
    SYSREF captured: Yes
    SYSREF alignment ERROR
    Rx link is enabled
    Measured Link Clock: 125 MHz
    Link status: DATA
    SYSREF captured: Yes
    SYSREF alignment ERROR
    adc_setup adc core initialized (500 MHz).
    dac_setup dac core initialized (500 MHz).
    main ad9680 - PN9 sequence mismatch!
    main ad9680 - PN23 sequence mismatch!
    daq2: RX capture done.

    No waveform was output at all.

    After that, if you rewrite 0x44A04418 to 0x0 with xsbd, the sine waveform was output.

    Yuta

  • Hi,

    Any changes to hardware or clock/rates that you haven't mentioned?
    I've seen in other threads problems caused by ILA's with no timing issue reported. Do you have ILA's in the system?
    Better of can you start fresh on a new workspace hdl_2018_r1 and no-Os 2018_r1? Validate that the design is working, then add only the last discussed square wave generator in HDL.

    Andrei

  • Hi, thank you for your reply.

    There is not any change in hardware or clock / rate that I do not mention.

    There is no ILA in my system. Should I add ILA? Please tell me how to add if I should add ILA.

    I will try to start with a new workspace hdl_2018_r1 and no-Os 2018_r1.

    Yuta

  • Hi,

    Don't add any ILA's.
    Can you make a testbench and simulate the square wave generator?

    Andrei

  • Hi,

    I understood not adding ILA.
    Since I have not made a test bench, I am not simulating a square wave generator.
    I will try to create the test bench.

    Yuta

  • Hi, 

    I tried to start with a new workspace hdl_2018_r1 and no-Os 2018_r1.

    As a result of the execution, no error appeared on the UART screen, but the waveform was still not output.

  • And I tried creating a test bench, but I could not make it well. How should I change it?

    //square_wave.v
    
    
    `timescale 1ns / 1ps
    
    module square_wave(
    CLK,
    increment,
    dout
    );
    input  CLK;
    input [31:0]  increment;
    reg  [15:0]  wave = 0;
    reg  [15:0]  sawtooth_wave = 'd0;
    output dout;
    
    always @(posedge CLK)begin
      sawtooth_wave <= sawtooth_wave + increment;
      wave <= {16{sawtooth_wave[31]}};
    end
    
    square_wave i_square_wave(
    CLK,
    increment,
    //wave,
    //sawtooth_wave,
    dout
    );
    endmodule
    

    //square_wave_tb.v  //testbench
    
    `timescale 1ns / 1ps
     
    
    module square_wave_tb();
    reg          CLK;
    reg  [31:0]  increment;
    reg  [15:0]  wave = 0;
    reg  [15:0]  sawtooth_wave = 'd0;
    wire dout;
    square_wave i_square_wave(
    .CLK (CLK),
    .increment (increment),
    .wave (wave),
    .sawtooth_wave (sawtooth_wave),
    .dout (dout)
    );
    
    always
      begin
        #50 CLK =~CLK;
      end
       
    always @(posedge CLK)begin
      sawtooth_wave <= sawtooth_wave + increment;
      wave <= {16{sawtooth_wave[31]}};
    end
    
    endmodule

    Yuta

  • Hi,

    Use 16 bits for increment.
    Fix sawtooth_wave[31], you only have 16 bits there.

    Andrei

  • Hi, Thank you for your reply.

    I had a lot of misunderstandings.
    After changing the bit number to 16, I improved the testbench and it worked correctly.

    I checked the NCO implemented in axi_ad 9144_channel.v on the test bench before, but square wave output was not obtained. Therefore I think that I failed even if I reworked the workspace.

    I changed the increment to "16'd1" and simulated the test bench. As a result, it was confirmed that the square wave was outputted on the simulation.

    Like the testbench, I added these to axi_ad 9144_channel.v, changed sawtooth_wave to dac_dds_phase_0_0, then built again, but the following error occurred.

    *** Running vivado
        with args -log system_top.vdi -applog -m64 -product Vivado -messageDb vivado.pb -mode batch -source system_top.tcl -notrace
    
    
    ****** Vivado v2017.4.1 (64-bit)
      **** SW Build 2117270 on Tue Jan 30 15:31:13 MST 2018
      **** IP Build 2095745 on Tue Jan 30 17:13:15 MST 2018
        ** Copyright 1986-2017 Xilinx, Inc. All Rights Reserved.
    
    source system_top.tcl -notrace
    Command: open_checkpoint /home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/system_top.dcp
    
    Starting open_checkpoint Task
    
    Time (s): cpu = 00:00:00.04 ; elapsed = 00:00:00.10 . Memory (MB): peak = 1159.902 ; gain = 0.000 ; free physical = 1330 ; free virtual = 4428
    INFO: [Netlist 29-17] Analyzing 5575 Unisim elements for replacement
    INFO: [Netlist 29-28] Unisim Transformation completed in 1 CPU seconds
    INFO: [Project 1-479] Netlist was created with Vivado 2017.4.1
    INFO: [Device 21-403] Loading part xc7vx485tffg1761-2
    INFO: [Project 1-570] Preparing netlist for logic optimization
    Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_board.xdc]
    Finished Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_board.xdc]
    Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_early.xdc]
    INFO: [Timing 38-35] Done setting XDC timing constraints. [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.srcs/sources_1/bd/system/ip/system_sys_mb_debug_0/system_sys_mb_debug_0.xdc:50]
    get_clocks: Time (s): cpu = 00:00:18 ; elapsed = 00:00:40 . Memory (MB): peak = 2698.164 ; gain = 712.832 ; free physical = 131 ; free virtual = 3028
    INFO: [Timing 38-2] Deriving generated clocks [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.srcs/sources_1/bd/system/ip/system_axi_ethernet_0/bd_0/ip/ip_2/synth/bd_55cd_pcs_pma_0.xdc:42]
    Finished Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_early.xdc]
    Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top.xdc]
    Finished Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top.xdc]
    Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_late.xdc]
    Finished Parsing XDC File [/home/aoyagi/work/square_8/hdl/projects/daq2/vc707/daq2_vc707.runs/impl_1/.Xil/Vivado-22481-aoyagi-VirtualBox/dcp1/system_top_late.xdc]
    Reading XDEF placement.
    Reading placer database...
    Reading XDEF routing.
    Read XDEF File: Time (s): cpu = 00:00:00.12 ; elapsed = 00:00:00.41 . Memory (MB): peak = 2822.234 ; gain = 0.000 ; free physical = 175 ; free virtual = 2975
    Restored from archive | CPU: 0.130000 secs | Memory: 0.013687 MB |
    Finished XDEF File Restore: Time (s): cpu = 00:00:00.12 ; elapsed = 00:00:00.42 . Memory (MB): peak = 2822.234 ; gain = 0.000 ; free physical = 175 ; free virtual = 2975
    INFO: [Project 1-111] Unisim Transformation Summary:
      A total of 1148 instances were transformed.
      IOBUF => IOBUF (IBUF, OBUFT): 57 instances
      IOBUFDS_DIFF_OUT_DCIEN => IOBUFDS_DIFF_OUT_DCIEN (IBUFDS_IBUFDISABLE_INT, IBUFDS_IBUFDISABLE_INT, INV, OBUFTDS_DCIEN, OBUFTDS_DCIEN): 8 instances
      IOBUF_DCIEN => IOBUF_DCIEN (IBUF_IBUFDISABLE, OBUFT_DCIEN): 64 instances
      LUT6_2 => LUT6_2 (LUT5, LUT6): 108 instances
      OBUFDS => OBUFDS_DUAL_BUF (INV, OBUFDS, OBUFDS): 1 instances
      RAM32M => RAM32M (RAMD32, RAMD32, RAMD32, RAMD32, RAMD32, RAMD32, RAMS32, RAMS32): 649 instances
      RAM32X1D => RAM32X1D (RAMD32, RAMD32): 32 instances
      RAM64M => RAM64M (RAMD64E, RAMD64E, RAMD64E, RAMD64E): 69 instances
      RAM64X1D => RAM64X1D (RAMD64E, RAMD64E): 160 instances
    
    INFO: [Project 1-604] Checkpoint was created with Vivado v2017.4.1 (64-bit) build 2117270
    open_checkpoint: Time (s): cpu = 00:01:05 ; elapsed = 00:03:05 . Memory (MB): peak = 2822.234 ; gain = 1662.332 ; free physical = 217 ; free virtual = 3014
    Command: opt_design
    Attempting to get a license for feature 'Implementation' and/or device 'xc7vx485t'
    INFO: [Common 17-349] Got license for feature 'Implementation' and/or device 'xc7vx485t'
    INFO: [Common 17-86] Your Implementation license expires in 3 day(s)
    INFO: [Common 17-1223] The version limit for your license is '2018.11' and will expire in 5 days. A version limit expiration means that, although you may be able to continue to use the current version of tools or IP with this license, you will not be eligible for any updates or new releases.
    Running DRC as a precondition to command opt_design
    
    Starting DRC Task
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[0] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[0]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[0]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[10] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[10]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[10]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[11] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[11]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[11]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[12] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[12]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[12]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[13] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[13]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[13]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[14] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[14]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[14]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[15] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[15]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[15]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[1] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[1]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[1]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[2] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[2]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[2]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[3] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[3]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[3]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[4] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[4]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[4]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[5] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[5]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[5]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[6] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[6]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[6]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[7] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[7]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[7]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[8] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[8]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[8]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0[9] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[9]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_0/dac_dds_phase_0_0_reg[9]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[0] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[0]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[0]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[10] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[10]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[10]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[11] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[11]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[11]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[12] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[12]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[12]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[13] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[13]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[13]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[14] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[14]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[14]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[15] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[15]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[15]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[1] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[1]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[1]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[2] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[2]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[2]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[3] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[3]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[3]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[4] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[4]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[4]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[5] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[5]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[5]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[6] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[6]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[6]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[7] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[7]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[7]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[8] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[8]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[8]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0[9] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[9]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_1/dac_dds_phase_0_0_reg[9]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[0] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[0]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[0]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[10] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[10]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[10]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[11] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[11]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[11]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[12] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[12]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[12]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[13] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[13]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[13]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[14] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[14]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[14]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[15] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[15]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[15]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[1] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[1]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[1]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[2] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[2]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[2]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[3] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[3]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[3]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[4] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[4]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[4]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[5] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[5]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[5]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[6] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[6]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[6]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[7] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[7]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[7]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[8] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[8]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[8]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0[9] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[9]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_2/dac_dds_phase_0_0_reg[9]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[0] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[0]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[0]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[10] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[10]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[10]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[11] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[11]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[11]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[12] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[12]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[12]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[13] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[13]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[13]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[14] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[14]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[14]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[15] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[15]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[15]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[1] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[1]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[1]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[2] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[2]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[2]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[3] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[3]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[3]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[4] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[4]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[4]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[5] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[5]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[5]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[6] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[6]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[6]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[7] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[7]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[7]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[8] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[8]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[8]__0/Q.
    ERROR: [DRC MDRV-1] Multiple Driver Nets: Net i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0[9] has multiple drivers: i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[9]/Q, and i_system_wrapper/system_i/axi_ad9144_core/inst/i_core/i_channel_3/dac_dds_phase_0_0_reg[9]__0/Q.
    INFO: [Project 1-461] DRC finished with 64 Errors
    INFO: [Project 1-462] Please refer to the DRC report (report_drc) for more information.
    ERROR: [Vivado_Tcl 4-78] Error(s) found during DRC. Opt_design not run.
    
    Time (s): cpu = 00:00:00.73 ; elapsed = 00:00:01 . Memory (MB): peak = 2830.238 ; gain = 8.000 ; free physical = 205 ; free virtual = 3011
    INFO: [Common 17-83] Releasing license: Implementation
    15 Infos, 0 Warnings, 0 Critical Warnings and 65 Errors encountered.
    opt_design failed
    ERROR: [Common 17-39] 'opt_design' failed due to earlier errors.
    
    INFO: [Common 17-206] Exiting Vivado at Sun Nov 25 01:22:07 2018...
    [Sun Nov 25 01:22:10 2018] impl_1 finished
    wait_on_run: Time (s): cpu = 00:01:18 ; elapsed = 00:03:41 . Memory (MB): peak = 3424.977 ; gain = 0.000 ; free physical = 1799 ; free virtual = 4636
    ERROR: [Common 17-69] Command failed: Run 'impl_1' failed. Unable to open
    INFO: [Common 17-206] Exiting Vivado at Sun Nov 25 01:22:14 2018...
    

    What is wrong?

    Yuta

  • Hi Yuta,

    The axi_ad9144_core runs at 250 MHz for maximum sampling rate (1GHz), this means to keep up with the DAC you must have 4 parallel data paths.

    I see some strange errors in your code.
    This is a diff to something I've written, that has built successfully.

    diff --git a/library/axi_ad9144/axi_ad9144_channel.v b/library/axi_ad9144/axi_ad9144_channel.v
    index 75635a40..5a93392c 100644
    --- a/library/axi_ad9144/axi_ad9144_channel.v
    +++ b/library/axi_ad9144/axi_ad9144_channel.v
    @@ -82,6 +82,10 @@ module axi_ad9144_channel #(
       reg     [15:0]  dac_dds_incr_0 = 'd0;
       reg     [15:0]  dac_dds_incr_1 = 'd0;
       reg     [63:0]  dac_dds_data = 'd0;
    +  reg     [15:0]  square_wave_0 = 'd0;
    +  reg     [15:0]  square_wave_1 = 'd0;
    +  reg     [15:0]  square_wave_2 = 'd0;
    +  reg     [15:0]  square_wave_3 = 'd0;
     
       // internal signals
     
    @@ -176,7 +180,7 @@ module axi_ad9144_channel #(
           pn7 = dout;
         end
       endfunction
    -  
    +
       // PN15 function
     
       function [63:0] pn15;
    @@ -266,7 +270,7 @@ module axi_ad9144_channel #(
           4'h6: dac_data <= dac_pn7_data_s;
           4'h5: dac_data <= dac_pn15_data_i_s;
           4'h4: dac_data <= dac_pn7_data_i_s;
    -      4'h3: dac_data <= 64'd0;
    +      4'h3: dac_data <= {square_wave_3,square_wave_2,square_wave_1,square_wave_0};
           4'h2: dac_data <= dma_data;
           4'h1: dac_data <= { dac_pat_data_2_s, dac_pat_data_1_s,
                               dac_pat_data_2_s, dac_pat_data_1_s};
    @@ -286,6 +290,13 @@ module axi_ad9144_channel #(
         end
       end
     
    +  always @(posedge dac_clk) begin
    +    square_wave_0 <= {16{dac_dds_phase_0_0[15]}};
    +    square_wave_1 <= {16{dac_dds_phase_1_0[15]}};
    +    square_wave_2 <= {16{dac_dds_phase_2_0[15]}};
    +    square_wave_3 <= {16{dac_dds_phase_3_0[15]}};
    +  end
    +
       // dds
     
       always @(posedge dac_clk) begin
    @@ -331,7 +342,7 @@ module axi_ad9144_channel #(
         .dds_data (dac_dds_data_0_s));
       end
       endgenerate
    -  
    +
       generate
       if (DATAPATH_DISABLE == 1) begin
       assign dac_dds_data_1_s = 16'd0;
    @@ -346,7 +357,7 @@ module axi_ad9144_channel #(
    


    Can you compare what you have whit this, and let me know if have questions about it.

    Andrei

Reply
  • Hi Yuta,

    The axi_ad9144_core runs at 250 MHz for maximum sampling rate (1GHz), this means to keep up with the DAC you must have 4 parallel data paths.

    I see some strange errors in your code.
    This is a diff to something I've written, that has built successfully.

    diff --git a/library/axi_ad9144/axi_ad9144_channel.v b/library/axi_ad9144/axi_ad9144_channel.v
    index 75635a40..5a93392c 100644
    --- a/library/axi_ad9144/axi_ad9144_channel.v
    +++ b/library/axi_ad9144/axi_ad9144_channel.v
    @@ -82,6 +82,10 @@ module axi_ad9144_channel #(
       reg     [15:0]  dac_dds_incr_0 = 'd0;
       reg     [15:0]  dac_dds_incr_1 = 'd0;
       reg     [63:0]  dac_dds_data = 'd0;
    +  reg     [15:0]  square_wave_0 = 'd0;
    +  reg     [15:0]  square_wave_1 = 'd0;
    +  reg     [15:0]  square_wave_2 = 'd0;
    +  reg     [15:0]  square_wave_3 = 'd0;
     
       // internal signals
     
    @@ -176,7 +180,7 @@ module axi_ad9144_channel #(
           pn7 = dout;
         end
       endfunction
    -  
    +
       // PN15 function
     
       function [63:0] pn15;
    @@ -266,7 +270,7 @@ module axi_ad9144_channel #(
           4'h6: dac_data <= dac_pn7_data_s;
           4'h5: dac_data <= dac_pn15_data_i_s;
           4'h4: dac_data <= dac_pn7_data_i_s;
    -      4'h3: dac_data <= 64'd0;
    +      4'h3: dac_data <= {square_wave_3,square_wave_2,square_wave_1,square_wave_0};
           4'h2: dac_data <= dma_data;
           4'h1: dac_data <= { dac_pat_data_2_s, dac_pat_data_1_s,
                               dac_pat_data_2_s, dac_pat_data_1_s};
    @@ -286,6 +290,13 @@ module axi_ad9144_channel #(
         end
       end
     
    +  always @(posedge dac_clk) begin
    +    square_wave_0 <= {16{dac_dds_phase_0_0[15]}};
    +    square_wave_1 <= {16{dac_dds_phase_1_0[15]}};
    +    square_wave_2 <= {16{dac_dds_phase_2_0[15]}};
    +    square_wave_3 <= {16{dac_dds_phase_3_0[15]}};
    +  end
    +
       // dds
     
       always @(posedge dac_clk) begin
    @@ -331,7 +342,7 @@ module axi_ad9144_channel #(
         .dds_data (dac_dds_data_0_s));
       end
       endgenerate
    -  
    +
       generate
       if (DATAPATH_DISABLE == 1) begin
       assign dac_dds_data_1_s = 16'd0;
    @@ -346,7 +357,7 @@ module axi_ad9144_channel #(
    


    Can you compare what you have whit this, and let me know if have questions about it.

    Andrei

Children