Post Go back to editing

AD-FMCDAQ2-EBZ on VC707 problem

Hi,

i have a problem with the AD-FMCDAQ2-EBZ on Xilinx VC707, short description:

  • make capture outputs the same data for terminated ADC inputs and DAC -> ADC loopback
  • SDK project get's SPI errors (AD9523: SPI write-verify failed (0x605) / AD9680: Invalid CHIP ID (0x4))

Detailed description:

Development-System Ubuntu 16.04
Vivado / SDK Version 2017.4
Development-Board Xilinx VC707
Evaluation-Board AD-FMCDAQ2-EBZ Rev. E on VC707 FMC1-HPC
Operationsystem-Type NO-OS
Processor MICROBLAZE

Source folder structure:

~/.../analog_jesd/app-manual [SDK workspace]
~/.../analog_jesd/hdl         [HDL Git folder: master branch]
~/.../analog_jesd/no-OS       [no-OS Git folder: master branch]

Build steps for HDL:

/.../analog_jesd/hdl/projects/daq2/vc707/make [build successful]

Build steps for no-OS:

Edit config.h [uncomment #define XILINX and #define MICROBLAZE]
/.../analog_jesd/no-OS/fmcdaq2/vc707/make log_make @ codepad
/.../analog_jesd/no-OS/fmcdaq2/vc707/make run log_make-run @ codepad
/.../analog_jesd/no-OS/fmcdaq2/vc707/make capture log_make-capture @ codepad

SDK.log @ codepad

Test 1: DAC outputs connected with ADC inputs

capture_ch1_loopback.csv
capture_ch2_loopback.csv

Test 2: ADC inputs terminated

capture_ch1_terminated.csv
capture_ch2_terminated.csv

The results of test1 and test2 are identical, i would expect  different results for loopback and terminated inputs!

 

Build steps for manual SDK project:

Workspace: ~/.../analog_jesd/app-manual
File->New Application Project->new Hardware Plattform(~/.../analog_jesd/hdl/projects/daq2/vc707/daq2_vc707.sdk)
Import all files (from ~/.../analog_jesd/no-OS/fmcdaq2/vc707/sw/src) into project src directory
Edit lscript.ld [change Heap Size to 0x100000]
Build successful

Debug steps for manual SDK project:

Create Debug Configuration [Xilinx C/C++ application (System Debugger), Standalone Application Debug, Local]
Debug

SDK-Terminal-Output:

Connected to /dev/ttyUSB0 at 115200
Available sampling rates:
  1 - ADC 1000 MSPS; DAC 1000 MSPS
  2 - ADC  500 MSPS; DAC 1000 MSPS
  3 - ADC  500 MSPS; DAC  500 MSPS
  4 - ADC  600 MSPS; DAC  600 MSPS
  5 - ADC 1000 MSPS; DAC 2000 MSPS (2x interpolation)
choose an option [default 1]:
1 - ADC 1000 MSPS; DAC 1000 MSPS
AD9523: SPI write-verify failed (0x605)!

AD9680: Invalid CHIP ID (0x4).
xcvr_setup ERROR: XCVR initialization failed!
xcvr_setup ERROR: XCVR initialization failed!
ad9144_setup : Invalid CHIP ID (0x4).
Tx link is disabled
Measured Link Clock: off
External reset is deasserted
Rx link is disabled
Measured Link Clock: off
External reset is deasserted
adc_setup adc core Status errors.
dac_setup DAC Core Status errors.

I have build everything like described in the tutorial but can't get the project running.

Can anybody help me or knows what the problem is?

Regards,

Andreas

Edit Notes

added branch information
[edited by: ansc at 11:55 AM (GMT -4) on 19 Sep 2018]
Parents Reply Children
No Data