KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADM2867E
Recommended for New Designs
The ADM2861E, ADM2863E, ADM2865E, and ADM2867E are 5.7 kV rms signal and power isolated RS-485 transceivers. These devices are designed for balanced transmission...
Datasheet
ADM2867E on Analog.com
ADM2795E
Production
The ADM2795E is a 5 kV rms signal isolated RS-485 transceiver that features up to ±42 V of ac/dc peak bus overvoltage fault protection on the RS-485 bus...
Datasheet
ADM2795E on Analog.com
ADM485
Production
The ADM485 is a differential line transceiver suitable for high speed bidirectional data communication on multipoint bus transmission lines. It is designed...
Datasheet
ADM485 on Analog.com
Remember those colored building bricks from our childhood? Countless hours spent clicking, creating, and then dismantling to start again. The ease in which we could create a world and then take it apart just as quickly. What if evaluating tech solutions could be that easy - just a click away?
Analog Devices is known for creating some of the best technology on the market, but accessing our latest innovations sometimes requires learning about boards and tools specific to each technology or manufacturer. With the explosion of innovation in the market being challenged by staffing and shrinking engineering budgets, the search began to find a better way to give customers a starting point to interfacing our technologies with those from other manufacturers.
It turns out that others were seeing the same trend, that is when one young, innovative partner suggested we join forces and combine our brand philosophies of “saving time” and “Ahead of what’s possible” the solution seemed obvious.
The partner was MikroElektronika (MikroE) who has built an ecosystem of development boards and compilers for microcontrollers with the ability to add LEGO like blocks called “Click boardsTM to measure and quantify the world around you. What MikroElektronika needed was the best technology to keep pace with the needs of their growing customer base.

Analog Devices shares their technology and domain knowledge with MikroElektronika so it can be incorporated into one of the largest and fastest growing development ecosystems. This ecosystem enables users to access an expanding portfolio of technologies in a highly productive and easy to use environment.
Now our customers can achieve the best of both worlds by using over 50 Click boards that feature Analog Devices technologies within MikroE’s ecosystem. Users can also establish a bridge with other established processor ecosystems through mikroBUSTM shields. mikroBUS quickly connects new and existing ecosystems together, speeding the adoption of the latest products, as well as sensing, signal chain, and power technologies. Curious how this might help you? Let’s look at examples of our products that are leveraging the Click board ecosystem.
Users can establish a bridge with other processor ecosystems like Arduino and Raspberry Pi though mikroBUS shields.
First, we will look at iCoupler® digital Isolation, which ensures trusted safety and data integrity for applications such as smart manufacturing, vehicle electrification, and digital health. Our isolation product portfolio is robust but evaluating all the options is no easy task. Historically, customers would consider our multiple RS-485 Isolation devices and evaluate the pro’s and con’s by reviewing datasheets or invest time trying to re-purpose our evaluation board for development. MikroE’s responsive and cutting-edge nature, allows us to work together to add even the latest products such as the ADM2867E Click Board. Using the Click board ecosystem, customers now have many of our RS-485 options as “LEGO like blocks” where they can create and recreate configurations, saving them precious time in development.
|
|
|
|
|
Another technology example within the Click board ecosystem is our software configurable input/output (SWIO) solutions, which allow any industrial I/O function to be accessed on any pin, allowing channels to be configured at any time. This means customization can happen right at the time of installation—resulting in faster time to market, fewer design resources, and universal products that can be implemented broadly across projects and customers. With options such as the SWIO Click board, the power of these programmable devices can be harnessed and even connected side by side with other devices to ensure they measure up to customers’ needs.
Want to take the easy route to access technology? Consider “Click”ing to speed your evaluation efforts. Not seeing what you need yet? Don’t worry, we have a pipeline of over 50 new technologies and welcome your inputs in the comments below for what should be next.