Why Long Battery Life is the Lifeblood of Thread IoT Sensors

Why Long Battery Life is the Lifeblood of Thread IoT Sensors

By providing secure IPv6-based low-power wireless technology, ThreadRegistered enables tamper-proof home sensors for comfort, entertainment, security, and energy efficiency. With its origins in home and building automation, Thread enables IoT applications in diverse consumer, wearable, medical, and industrial markets. Google has also released a lightweight open-source implementation of Thread called OpenThread. While it is not exactly akin to what Android was for smartphones, OpenThread promises to be an excellent enabler for Thread adoption. Thread joins several other networking standards including Zigbee, NB-IoT, LoRa, SigFox, and Bluetooth LE.

When thinking of wireless mesh networks for the IoT, many people think of issues such as MAC protocols, open IP stack, interoperability, application layer, security, and ability to support peer-to-peer as well as end-point to cloud communication. These are all important issues and are addressed by the Thread Group. But since the core foundation of these applications is to operate energy efficiently, power management is the most critical one left for system designers to solve! Ignore it at your peril. While the issues on power may be common to other IoT standards, we will focus on Thread in this post.

How Thread Enables the IoT

IoT and smart node devices are built on few key requirements:

  • Simple and quick installation
  • Secure communications
  • Scalability in adding new end-point devices and application layers
  • Open source for interoperability and large ecosystem
  • Low power to extend battery life

Thread uses the proven 2.4GHz 802.15.4 radio (868MHz/915MHz bands optional) combined with IPv6 and AES encryption as the foundation and enables a scalable wireless mesh network where new authenticated nodes can be added on demand. A node can be a router or an end-point device. Several types of end-point devices and routers are defined. A Thread Leader is a router that is self-elected and manages all the routers in a single network. While there are limits on the number of nodes per network, Thread networks can be grown with multiple Thread Leaders. Thread relies on the 802.15.4 group of standards for radio (PHY) and MAC. It is application layer-agnostic or, rather, blind to it; any application can be run on it if it is low bandwidth and supports IPv6.


Thread mesh networks in a large-scale connected domain. Image courtesy of Thread Group.


Layers governed by Thread. Image courtesy of Thread Group.

A Look at IEEE 802.15 Standards

802.15 standards for wireless personal area networks (WPAN) include:

  • Bluetooth or 802.15.1
  • UWB high-data-rate standards like 802.15.3 for video and music
  • Low-data-rate and low-power 802.15.4 group of standards for radio (PHY) and MAC layers, which has variants, upper-layer enhancements, and related standards such as Zigbee, 6LowPAN (IPv6 over low-power personal area networks), Wireless HART, MiWiTm and ISA100.11A
  • 802.15.5 is a wireless mesh version of 802.15.4
  • Body area networks or 802.15.6

By leveraging 802.15.4 radio architecture, Thread systems take advantage of a low-power, low-bandwidth framework while supporting multiple frequency bands in the 20-30m range for data rates up to 250Kbps. With TDMA and CSMA options, 802.15.4 provides real-time communication capability as well.

6LowPAN for Secure Communication

Thread uses 6LowPAN or IPv6 over Low-power Personal Area Networks. 6LowPAN was developed by the Internet Engineering Task Force (IETF) to enable Internet Protocol (IP) traffic not just on traditional Ethernet-based WAN/LAN networks, but also on low-power Personal Area Networks (PAN) such as Bluetooth LE and 802.15.4 for a host of diverse, low-power applications, such as consumer wearables and factory automation. It defines an edge router for connectivity. A router can connect to multiple end devices and other routers. A Border Router, as it is called by the Thread Group, connects a Thread network to a non-Thread network like, say, Wi-Fi. By adopting 6LowPAN, Thread brings all the benefits of secure communications to wireless mesh networks where all devices are authenticated, all communications are encrypted, and new devices can be added on demand.

Extending Battery Life for Thread IoT Devices

How do you extended battery life for portable applications? Thread does not define battery life – this is left to the system architect. When our team at Maxim invented nanoPower power management products, the engineers primarily kept in mind two main objectives:

  1. Reduce quiescent current (IQ) to nano-Amperes (nA) in order to extend battery life
  2. Deliver a flat high efficiency across the load from less than 1% all the way to full load – critical for plugged-in applications


Flat efficiency across load critical for plugged-in applications (buck with 1.2VOUT).

Not easy challenges, but that is what is needed for you to succeed. When thinking of power needs, a slew of always-on, Thread-enabled IoT devices stay in a light-load condition most of the time (in shutdown) with occasional low-power data acquisition consuming few µA of load current (stand by). Finally, in full load condition, once in a blue moon when data is transmitted, these devices need 500mA to 1A. An IC that consumes only nA of current on average across the three modes of load current that always-on IoT devices demand dramatically increases battery life for portable applications. While today Thread sensors are mostly powered by batteries, it is expected that some will be plugged-in even though communication is wireless as adoption continues. It is important to have flat efficiency across load profiles to reduce phantom power consumption even for plugged-in applications.

More Reading

Anonymous