Formula One Race Competition

When Polynomials Hit the Wall and Why Your PA Needs a Brain: Part 1 of 3

In the race to unlock next-generation wireless communication, power amplifiers (PAs) face a tough balancing act: maximizing efficiency while avoiding signal distortion that can degrade communication quality. Digital predistortion (DPD) technology has long been the answer, pre-correcting signals so PAs can operate at peak efficiency without sacrificing linearity. But traditional polynomial-based DPD methods are hitting their limits, struggling to keep pace with the complex nonlinearities modern PAs demand.

That’s where artificial intelligence (AI) and neural networks (NNs) come in. We’ll explore why DPD matters, where conventional approaches fall short, and how intelligent, adaptive DPD engines are changing the game.

PAs at the Edge of Efficiency

PAs are fundamental in RF transmitter chains, but exhibit nonlinear behavior, especially near their saturation point. This manifests in three interconnected ways: signal distortion corrupts the integrity of transmitted data; spectral regrowth causes the signal to spread beyond its intended bandwidth, interfering with adjacent channels; and reduced energy efficiency increases costs and thermal loads. These issues become more pronounced in high-bandwidth systems employing complex modulation schemes like orthogonal frequency division multiplexing (OFDM), which demand high linearity.

Traditional DPD methods combat this by modeling the PA’s inverse behavior; essentially undoing its nonlinear effects through polynomial-based predistorters. The input signal is modified such that after amplification, the output signal looks clean and linear.

Generic Concept of DPD for Linearizing the PA Response

Figure 1: Generic Concept of DPD for Linearizing the PA Response:
(a) Typical AM-to-AM Curve Showing the Overall Linear Region Is in Green
(b) Basic Concept of DPD and How it Improves Power Amplifier Efficiency

While effective, these polynomial-based solutions assume the PA behaves as a static, memoryless system. This assumption falls short. Real-world impairments, including I/Q imbalance, phase shifts, temperature variations, and hardware aging, introduce memory effects and dynamic nonlinearities that static polynomial models simply cannot track. Each of these factors can shift the PA’s operating characteristics in unpredictable ways, making a fixed mathematical model increasingly inadequate over time.

AI and Neural Networks: The Smart DPD Revolution

Artificial NNs offer a powerful alternative. Inspired by the human brain, NNs excel at modeling complex, nonlinear relationships without requiring explicit mathematical formulations. Rather than relying on a predefined polynomial structure, a neural network learns the PA’s behavior directly from data: adapting to dynamic conditions in real time, capturing nonlinearities and memory effects simultaneously, and reducing error in gain and phase distortions more effectively than traditional polynomial models. The result is a DPD engine that is continuously learning and evolving by analyzing extensive PA performance data to deliver efficiency and signal fidelity.

How AI-Driven DPD Works: The Three-Step Framework

At the heart of the AI-powered DPD system is a three-step process:

  1. PA Characterization Data Collection
  2. Neural Network Model Training
  3. Model Validation and Deployment

We’ll cover the first step extensively here.

Step 1: PA Characterization Data Collection

Building an AI model requires a rich dataset that accurately reflects the PA’s behavior under various operating conditions.

Measurement setup for wideband PA characterization.

Figure 2: Measurement setup for wideband PA characterization.

This setup enables engineers to extract critical metrics such as S-parameters, input/output power metrics, power-added efficiency (PAE), AM-to-AM and AM-to-PM distortion characteristics, linearity metrics such as adjacent channel power ratio (ACPR) and error vector magnitude (EVM), thermal performance and environmental effects, and noise characteristics.

Table 1 summarizes the key measurement areas and descriptions, illustrating the depth and breadth of data needed to train an effective NN model.

Table 1. Measurement Areas and Descriptions

Areas

Description and Details

Small-Signal Characterization

S-parameters measured across frequencies and biasing conditions to assess input/output matching and frequency response.

Nonlinear Behavior and Large-Signal Data

Input-output power relationships, gain compression points, and AM-to-AM/AM-to-PM distortion under high power levels.

Efficiency Metrics

Measurements of drain and overall efficiency across various load and temperature conditions.

Linearity and Signal Integrity

Metrics like ACPR, EVM, and intermodulation distortion (IMD) to quantify signal distortion.

Thermal Performance

Thermal sensor data to understand heat dissipation and reliability under different conditions.

Environmental and Aging Data

Effects of temperature, humidity, and accelerated aging tests for long-term performance prediction.

Noise Characteristics

Noise figure and phase noise spectrum, crucial for assessing signal quality.

 

This rigorous data collection forms the foundation for AI models that can predict and counteract PA nonlinearities dynamically.

Why This Matters: The Future of Wireless Efficiency

Traditional DPD methods are no longer sufficient to meet the demands of ultra-high bandwidth, low-latency, and energy-efficient wireless communication systems. AI-driven DPD engines promise:

  • Enhanced signal quality and spectral efficiency
  • Greater adaptability to changing PA conditions
  • Reduced computational complexity in real-time use
  • The ability to push PAs closer to their saturation point without compromising linearity

Analog Devices, with its cutting-edge RF transceiver platforms like the ADRV9040, is pioneering this transition by integrating AI-driven DPD solutions that empower engineers to build smarter, more efficient communication systems.

The Dawn of Intelligent DPD

DPD is critical to unlocking the full efficiency of PAs in modern wireless systems. But as these systems grow more complex, traditional polynomial-based methods hit a wall. AI and NNs offer a bold new path forward: transforming DPD engines from static correction tools into dynamic, adaptive, and intelligent systems. Part 2 will explore the NN architectures powering these smart DPD engines and dive into the training and optimization processes that make them tick.

Read the full technical article Toward Smarter Digital Predistortion Engines: A Neural Network-Based Approach.

Read all the blogs in the Smarter DPD Engines series.