A fork in the road with a sign showing either direction.

When “Good Enough” Is Not Enough: µModules in Industrial Design: Part 1 of 3

In much of today’s industrial market, “good-enough” performance is the dominant design target, with long product lifecycles, tight cost pressures, and conservative qualification processes driving engineering decisions. In many cases, discrete signal chains optimized for cost are the right choice, and there is no reason to change what already works. 

Not All Industrial Applications Are Created Equal

 
Figure 1: Comparison of signal chains 

As shown in Figure 1, the discrete setup (top rectangle) requires multiple separate components-amplifier, filter, ADC, Temp sensor, and MCU-while the ADAQ4224 µModule (bottom rectangle) integrates the signal chain into a single factory-trimmed block, simplifying design and improving predictability. 

As systems move toward higher accuracy, higher channel density, and tighter reliability requirements, the discrete approach can introduce hidden challenges. Calibration effort increases, layout sensitivity becomes significant, and small variations between boards can lead to extended validation cycles. In these cases, the full cost is no longer limited to the bill of materials; it is measured in engineering time, project risk, and delayed time to market. 

Precision Data Acquisition is an application area where integrated signal chain solutions, such as precision µModules, make sense because they minimize layout sensitivity, reduce calibration overhead, and accelerate system validation. 

Solutions like the ADAQ4224 are not intended as generic replacements for discrete ADCs. Instead, they provide a system-level approach that integrates the critical front-end signal chain into a single, factory-trimmed solution. The results are predictable and repeatable, independent of board layout and component selection. For industrial teams facing long qualification cycles, this predictability can significantly reduce validation effort and risk. 

 
 Performance consistency across temperature and multiple boards

Figure 2: Performance consistency across temperature and multiple boards 

 As shown in Figure 2, the ADAQ4224 µModule (green line) maintains stable measurement accuracy, whereas the discrete signal chains (blue-shaded area) exhibit higher variability, illustrating the benefits of factory-trimmed integration. 

Precision, Reliability, and Stability  

In high-end industrial systems, precision, reliability, and long-term stability have the biggest impact on performance. Factory automation, CBM solutions, precision instrumentation, and robotics all demand highly stable, repeatable measurements. In these environments, reducing front‑end uncertainty, such as sensor drift, offset, and gain errors, analog‑front‑end noise, and unit‑to‑unit variation often matters more than small BOM savings.

 
 Total system cost reduction using a uModule

Figure 3: Total system cost reduction using a uModule 

As shown in Figure 3, although the BOM cost of the µModule (green bar) may be slightly higher than the discrete solution (blue bar), the total system cost is lower due to reduced engineering, calibration, and validation effort. 

Pricing discussions often arise when comparing integrated solutions to discrete implementations. While the unit cost of an integrated signal-chain solution may be higher, a fair comparison must consider total system cost. Reduced engineering time, fewer board spins, faster qualification, and earlier revenue generation can outweigh the initial component cost difference, particularly in low to mid-volume, high-performance industrial designs. 

Understanding Priorities Early On  

The key is to understand customer priorities early in the qualification process. If an application is driven purely by achieving the lowest BOM cost, then highly integrated solutions are unlikely to be the best fit. However, when accuracy, reliability, and time‑to‑market become the primary design goals, integrated signal‑chain solutions offer a powerful and practical alternative. Aligning these priorities early helps us guide the customer to the solution that delivers the most value for their specific needs. 

In industrial design, “good enough” is often good enough. The real value comes from knowing when it is not the case, because in demanding environments, eliminating front-end uncertainty can outweigh incremental BOM savings. 


Read all the blogs in the Precision Chain Technology series


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.