Viewing the sunset through a camera filter

​​​What Your I/O Card Knows: Diagnostics for Smarter System Health​

“Wait... I don’t need a multimeter?” The commissioning engineer paused, half surprised and half suspicious. Years of experience had taught him the familiar routine for a new I/O card: measure the field supply, check the analog rails, verify the channel voltage, confirm the output current, look for wiring mistakes, and make sure that nothing runs hotter than expected.  

Not this time. The story was different: an intelligent I/O card built around the AD74416H was already providing extensive diagnostics and system insight. The meter still has an essential place for independent verification and difficult fault-finding. But before and during commissioning or during operation, many questions can be answered from inside the intelligent I/O card itself.  

Earlier Configurability IQ posts explored what a software-configurable channel can do. This article asks what the device can see about itself, its power environment, and each connected channel.  

How Far Can Self-Diagnostics Go? 

The AD74416H diagnostic ADC inputs operate independently of the four channel measurements. You can enable four diagnostic selections in the same conversion sequence while the four main channels continue to deliver their application measurements. 

To give users and engineers a fuller view of system health, the diagnostics can monitor channel voltage and current, reveal the state of connected sensors or actuators, measure internal device temperature, and check both digital and analog supply levels. This information helps the controller make better-informed decisions and makes servicing or debugging faults smoother. 

 

 

  Overview of diagnostics

Figure 1: Overview of diagnostics available at the AD74416H chip 

ADC Diagnostic Measurements Plus Immediate Status  

Measurements are only one layer. The AD74416H also reports open-circuit and short-circuit conditions where supported by the configured channel function. It also reports supply alerts, channel alerts, reset occurrence, watchdog activity, and communication integrity through SPI CRC checking.  

LIVE_STATUS identifies conditions that are still present, while latched alert-status registers preserve events for firmware review. This creates a useful two-step conversation. A status bit says, 'look here.' A measured value says, 'this is what the hardware is seeing.' For example, firmware can relate a channel open-circuit indication to the measured sense-node voltage, compare a digital output event with the measured source current, or check whether unusual behavior coincides with supply movement or rising chip temperature.  

Exploring the Diagnostics Hands-On 

Connect the EV-AD74416H-ARDZ to the SDP-K1 and open the AD74416H ACE plug-in. To configure diagnostic measurements, click the “Diagnostic Channel” block, set CONV_SEQ to CONTINUOUS, enable the corresponding diagnostics, then from the drop-down menu (DIAG0, DIAG1, etc.) select each diagnostic type and click the “Apply” button. After enabling diagnostic readings, you can view them in the “Diagnostics Results” tab.  

 ACE AD74416H Diagnostics configuration

Figure 2: ACE AD74416H Diagnostics configuration 

The EV-AD74416H-ARDZ includes an onboard thermistor connected to the LVIN input, typically used for cold-junction compensation in thermocouple applications. Heating RT1, for example by blowing warm air onto it, causes the LVIN voltage to change accordingly. 

  ACE AD74416H Diagnostic Results Tab

Figure 3: ACE AD74416H Diagnostic Results Tab 

Putting Diagnostics to Work 

The AD74416H gives the system a rich diagnostic foundation: measurements, monitors, and status evidence that help reveal what is happening inside the device and at each configured channel. The host firmware then adds the application context: expected ranges, persistence time, comparison with the commanded mode, trend history, and what response to take. 

Instead of a single generic fault lamp, the controller can build a more nuanced health picture: Is the chip getting hotter? Are the supplies stable? Does the field voltage match the configured function? Is the digital output delivering the expected current? Intelligent I/O is therefore not only about changing what a channel does. It is also about changing what the system chooses to observe.  

So, the next time that familiar instinct says, “reach for the multimeter,” the first answer may already be waiting inside the I/O card. With the AD74416H, diagnostics are not just a follow-up step after something goes wrong; they become part of how the system understands, explains, and responds to what is happening in the field. 

Read all the blogs in the Configurability IQ series.


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.