KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAXQ1065
Not Recommended for New Designs
The MAXQ1065 is a security coprocessor that provides turnkey cryptographic functions for root-of-trust, mutual authentication, data confidentiality and...
Datasheet
MAXQ1065 on Analog.com
MAX32672
Recommended for New Designs
In the DARWIN family, the MAX32672 is an ultra-low-power, cost-effective, highly integrated, and highly reliable 32-bit microcontroller enabling designs...
Datasheet
MAX32672 on Analog.com
DS28S60
Recommended for New Designs
The DS28S60 DeepCover® cryptographic coprocessor easily integrates into embedded systems enabling confidentiality, authentication and integrity of information...
Datasheet
DS28S60 on Analog.com
By Brian Condell & Conal Watterson
Guaranteeing the authenticity of an edge device and the data it provides is increasingly critical as the potential for security threats grows. In the fifth blog of our remote IO blog series, we will discuss how cybersecurity is a topic of concern within the industry as connectivity and IP addressability opens up the possibility of hacking and system attacks. With edge-to-cloud connected factories generating larger volumes of data in remote locations across the factory, automation vendors must consider how to overcome several new design challenges which weren’t a problem years ago.
Why is security a problem now?
We all have heard about the connected factory of the future; well, the future is here today with all types of sensors and actuators connected together and sharing information to help the factory run as efficiently and as flexible as possible. Realizing Industry 4.0 involves increased access to edge devices in the factory and accessibility in controlling them. The resulting transparency and data insights can reduce network planning, CapEx and OpEx. Increased bandwidth and optimized machine interworking are also enabled. With that, the famous quote from the Spiderman movie comes to mind, “With great power, there must also come great responsibility.” Similarly, you cannot have all this interconnectivity that provides the power to make smarter decisions without considering the consequences.
Providing a data path from edge to cloud introduces new threat vectors, meaning that cyber security risks to Industrial Control Systems (ICS) must be reassessed. ICS cyber security solutions need to adapt to address the changing risk, and traditional countermeasures applied to the system, such as firewalls and placing a device behind a locked door, are counterintuitive to the goals of Industry 4.0. This means devices will need to be security hardened to enable increased functionality in a secure method. Identity and integrity will be at the core of every device in the field to enable trusted data and secure operation.
System designers for automation vendors, and system integrators may encounter the following issues as they are planning their system’s design (see figures 1 & 2).

Figure 1- Common Design Challenges Parts 1 - 4
Authenticity
Third-party clones or counterfeit components could enter the system and pose safety risks while not meeting the customer’s expectations and specifications, affecting system integrity and reliability.

Figure 2 - Common Design Challenges Parts 5 – 8
IoT security
A variety of security techniques to protect against malware attacking an entire infrastructure that has not been properly secured.

Figure 3 - Moving Security Closer to the Edge where the Data is Born
Is there a solution?
The ultra-low power MAXQ1065 Cryptographic Controller with ChipDNATM is an ideal security coprocessor for embedded devices. It can provide turnkey cryptographic functions for root-of-trust, mutual authentication, data confidentiality and integrity, secure boot, secure firmware update, and secure communications with generic key exchange and bulk encryption or complete TLS support.

Figure 4 - MAXQ1065 Block Diagram
DeepCover® embedded security solutions cloak sensitive data under multiple layers of advanced security including active die shield, encrypted storage of keys using the ChipDNATM PUF technology, and externally callable algorithmic subroutines. Along with this, the MAXQ1065 has 8 KB of secure flash memory that can be used for keys, secrets, certificates, or user data.
The encryption (ECDSA, AES-256, SHA-256) and secure boot ROM features of the MAX32672 MCU also protect against intrusion and support the secure root of trust to ensure no malicious execution.
How does this secure the system?
The root of trust begins with safe key management. Sophisticated invasive attacks are frequently launched in an attempt to obtain cryptographic keys from secure ICs. If obtained, the security provided by the IC is thoroughly compromised. A key derived from a physically unclonable function (PUF) provides an unprecedented level of protection against invasive attacks, since the PUF-based key does not exist in memory or another static state.
Attackers can’t steal a key that isn’t there. ChipDNA provides symmetric key for encryption and decryption, as well as private keys for ECDSA and/or ECDHE. ChipDNA derives a cryptographic key from a precise analog characteristic of the IC. This key is based on a physically unclonable function and is not stored in memory or any other static state where it could be compromised. Each IC’s unique ChipDNA-generated key, since it is based on a physical unclonable function, is repeatable over temperature, voltage, and IC operating life conditions.
With legislative requirements such as the upcoming European Cyber Resilience Act (CRA), security will not only become more important, but mandated, for manufacturers of factory automation equipment/modules.
References