We shift focus from the importance of digital predistortion (DPD) to the heart of the AI-powered DPD engine: the neural network (NN) architectures that model power amplifier (PA) behavior, the training strategies that enable them to learn from data, and the optimization techniques that ensure real-time performance. These elements are crucial for transforming raw data into a dynamic, adaptive system that can keep pace with the fast-evolving wireless environment.
Tailoring AI to PA Nonlinearities and Memory Effects
The unique challenges posed by PAs (nonlinear distortion combined with memory effects) call for NNs specifically designed to capture both instantaneous and temporal dependencies in signals.
Table 1. NN Architectures
|
Architecture |
Structure |
Use in DPD |
Pros/Cons |
|
Feedforward Neural Networks (FNNs) |
Composed of multiple fully connected layers, FNNs map input vectors to output vectors without internal feedback loops. |
Can model the nonlinear static behavior of PAs effectively, especially when memory effects are negligible or can be approximated by including delayed input samples as features. |
Limitations: FNNs struggle with long memory effects and temporal dynamics because each output inference depends only on the current input vector.
|
|
Recurrent Neural Networks (RNNs) and Long Short-Term Memory (LSTM) Networks |
Have feedback loops allowing them to maintain an internal state that captures temporal context. LSTMs are a specialized RNN variant designed to capture long-term dependencies and avoid vanishing gradient problems during training. |
Ideal for modeling complex memory effects in PAs by considering sequences of input samples and their influence over time.
|
Advantages: Superior at learning temporal relationships and dynamic nonlinearities without requiring manual feature engineering. |
|
Convolutional Neural Networks (CNNs) |
Use convolutional layers to automatically extract local features from input sequences. |
CNNs can capture local time-correlated nonlinearities and memory effects by sliding filters over input data, enabling efficient parameter sharing and reduced model complexity. |
Advantages: Faster training and inference compared to RNNs, with good memory modeling capability.
|
As seen from the table, a single NN architecture cannot address both short- and long-term memory effects. As a result, ADI used a different approach: hybrid architectures. Combining CNNs and RNNs (or LSTMs) can leverage the strengths of both, extracting local features and modeling temporal dependencies, thus achieving enhanced accuracy and robustness.
Preparing Data for Neural Networks
The effectiveness of any NN depends heavily on the quality and format of its inputs. For DPD, input signals are fundamentally complex-valued, which shapes every decision we make in this stage.
We represent the PA input using the in-phase (I) and quadrature (Q) components of the baseband signal, feeding them either as separate real-valued features or combined as complex-valued inputs. To capture memory effects, multiple delayed versions of the input signal are stacked, creating a vector or tensor representing temporal context.
Beyond the raw IQ samples and their delayed copies, we can further enrich the input by engineering additional features such as instantaneous power, phase, or envelope metrics. These can be appended to enhance model awareness of PA-specific behaviors.
Training NNs for DPD: Learning to Linearize
Training the NN-based DPD models involves supervised learning using the PA characterization data collected in Part 1. We approach this in three structured stages: preparing the data, designing the loss function, and selecting the training algorithm.
- Data Preparation and Preprocessing
Input and output signals are normalized to zero mean and unit variance for stable training. The dataset is divided into training, validation, and test subsets to enable unbiased performance evaluation. Synthetic distortions or environmental variations can be introduced to improve model robustness.
- Loss Function Design
The mean squared error (MSE) is commonly used to minimize the difference between the PA output and the desired linear response. Where spectral performance is paramount, we incorporate custom loss functions that directly include domain-specific metrics such as adjacent channel power ratio (ACPR) or error vector magnitude (EVM). This allows the network to directly optimize signal quality measures.
- Training Algorithms
For the optimization algorithm, we rely on gradient descent variants. The adaptive moment estimation (ADAM) optimizer is popular for its adaptive learning rate and fast convergence. To prevent the model from memorizing training data at the expense of generalization, we apply regularization techniques like dropout, L2 weight decay, or early stopping based on validation loss. Batch size and the number of training epochs are carefully chosen to balance training speed and convergence.

Figure 1: Architecture of a Multiclass Prediction NN in Deep Learning
Model Validation and Performance Metrics
After training, the neural network DPD model undergoes rigorous validation to ensure it generalizes well to unseen data and operating conditions.
- Linearity Metrics: ACPR and EVM are measured on test signals to verify distortion reduction.
- Power Efficiency: Evaluating power-added efficiency (PAE) improvements with the model in the loop.
- Robustness Testing: Assessing model performance across temperature variations, hardware aging, and signal bandwidth changes.
- Computational Complexity: Measuring inference latency and resource utilization to ensure real-time deployability.
Bringing AI-Based DPD to Real-World Systems
Deploying NN-DPD models in commercial RF transceivers requires balancing complexity, latency, and power consumption.
Model compression techniques such as pruning, quantization, or knowledge distillation reduce model size without sacrificing accuracy. Hardware acceleration is addressed by leveraging specialized digital signal processors (DSPs), field-programmable gate arrays (FPGAs), or AI accelerators embedded in RF platforms like the ADRV9040.
We implement adaptive learning online or incremental learning to continuously update the model as PA characteristics drift over time. We pay close attention to integration with existing DSP chains, ensuring seamless coexistence with other baseband processing blocks.
The NN Engine Driving Intelligent DPD Forward
Neural networks unlock a new dimension of intelligence in DPD engines. By pairing architectures tailored to PA nonlinearity with hardware-aware deployment strategies, these AI-driven systems push amplifiers closer to their efficiency limits without sacrificing signal fidelity.
In Part 3, we'll explore adaptive learning, real-time optimization, and integration techniques that make intelligent DPD practical for next-generation wireless. Stay tuned.
Read the full technical article Toward Smarter Digital Predistortion Engines: A Neural Network-Based Approach.
Read all the blogs in the Smarter DPD Engines series.