by Unnikrishnan P.S
Developing safety-critical software in the automotive industry requires a strong commitment to both quality and safety. Adhering to the ISO 26262 standard, an international standard for functional safety of electrical and electronic (E/E) systems in road vehicles, is essential to ensure the software’s reliability and compliance with functional safety requirements. However, meeting the ISO26262 standard can be a complex and resource-heavy process due to extensive analysis, verification, and validation requirements.
Thankfully, by integrating ASPICE (Automotive SPICE) into the development process, automotive projects can streamline the entire workflow. ASPICE supports process improvement and maturity, making it easier to meet the requirements of ISO 26262, specifically Part 6/8, the sections that focus on software development and supporting processes.

Figure 1: Bridging ASPICE and ISO 26262: A Comparative Study 1, 2

Figure 2: Synergies Between ASPICE and ISO 26262 Parts 6,8
Cross-Compliance Between ASPICE and ISO 26262
In this blog, we’ll explore how ASPICE compliance can help reduce the effort in documentation and verification/Analysis activities when developing safety-critical software according to ISO 26262.
Streamlined Documentation Through Established Processes
ISO 26262 mandates thorough documentation across all development phases, including safety requirements, design, testing, and verification. ASPICE inherently supports this need by embedding structured documentation practices that align with ISO 26262 Part 6.
Improved Traceability
ISO 26262 places strong emphasis on the importance of traceability between safety requirements and their implementation, requiring continuous tracking from initial definition to final verification. With ASPICE’s robust framework in place, safety software development benefits from a well-structured methodology that ensures all requirements are systematically tracked and verified, aligning with ISO 26262 standards for functional safety.
Pre-defined Templates for Verification and Validation Activities
Verification and validation are key activities in ISO 26262, ensuring that safety requirements are thoroughly tested. ASPICE provides standardized templates for conducting these activities, including unit testing and integration testing, which directly align with ISO 26262’s verification requirements. This helps developers quickly implement software testing and validation strategies, ensuring that all testing activities meet ISO 26262's stringent requirements without the need for redundant work or manual test plan creation.
Clear Process Guidelines for Safety Lifecycle Management
ISO 26262 specifies a comprehensive safety lifecycle, including requirements analysis, design, implementation, verification, and validation. ASPICE provides clear, structured guidelines that fit well within this lifecycle. This ensures that every phase of the safety lifecycle is covered without duplicating efforts.
Efficient Management of Safety Requirements
ISO 26262 emphasizes the importance of managing safety requirements from start to finish. By following ASPICE, activities such as requirements elicitation and requirements tracking are streamlined and integrated into the development process.
Reduced Effort in Audit and Compliance Verification
One of the most challenging aspects of ISO 26262 is ensuring compliance throughout the software development process. ASPICE aids this by providing clear guidelines for audit preparation and compliance verification.
Since ASPICE already integrates structured processes for software development, compliance with ISO 26262 is inherently supported. This reduces the time and effort spent on preparing for audits and verifying compliance checks, making the process more efficient and ensuring that the development team is always aligned with safety standards.
Minimized Redundancy in Reviews and Documentation
In ISO 26262, frequent design reviews and safety assessments/audits are required to ensure that safety-critical software meets functional safety requirements at every stage of development. ASPICE ensures that these reviews are integrated into the process, reducing the risk of redundant or unnecessary reviews.
Faster Integration and Change Management
Managing changes to safety requirements and software design is crucial for ensuring that safety-critical systems remain compliant as they evolve. ISO 26262 requires structured change management and impact analysis to evaluate and document the effects of changes on safety. With ASPICE, change control procedures are already in place, allowing for more efficient management of changes.
Reduced Risk of Non-Compliance
By following ASPICE, the risk of non-compliance with ISO 26262 is significantly reduced. ASPICE’s structured processes inherently align with ISO 26262's requirements, ensuring safety standards are consistently met without the need for extensive rework or manual corrections.
ASPICE Increases Efficiency in Safety-Critical Software Development
Adhering to ISO 26262 is vital for ensuring the safety and reliability of automotive software. Nonetheless, the complex documentation and verification requirements can create a significant workload. By integrating ASPICE processes into the software development lifecycle, automotive companies can streamline many of these tasks, reducing effort and improving efficiency.

Figure 3: Comparative Overview of ISO 26262 Implementation Efforts
With ASPICE guiding the software development process, many of the critical activities required by ISO 26262 Part 6—including requirements analysis, design reviews, verification, validation, and safety assessments—are already organized in a structured way. This reduces the need for redundant tasks, minimizes manual effort, and ensures that safety requirements are consistently addressed.
For automotive developers working on safety-critical software, integrating ASPICE with ISO 26262-Part 6 is an established way to achieve higher quality, increased safety, and reduced effort in compliance. By using ASPICE to streamline these activities, organizations can focus on creating innovative and safe automotive systems with greater efficiency.
References
1 Road vehicles — Functional safety-Part 6: Product development at the software level. International Standard, Second edition ISO 26262: 2018, January 2019
2 Road vehicles — Functional safety-Part 8: Supporting processes. International Standard, Second edition ISO 26262:2018, December 2018
Read more from the Automotive FuSa blog series