Sensors are all around us. They help our gadgets, appliances, and electronic equipment "notice" what's happening in our environment. Essentially, they are tools that help detect changes around us, such as light, temperature, or movement. When something in the environment changes, sensors convert that change into an electrical signal.
Most sensors output a voltage signal, which is easy for electronic devices to read. But some sensors, like photodiodes (which detect light), generate a current signal instead. Since most electronic systems are designed to accept only voltage signals, the current signal from photodiodes often needs to be converted to a voltage signal before it can be used properly.
This three-part blog series will discuss the basic concepts of the stability analysis of an op amp configured as a Transimpedance Amplifier (TIA) and an op amp driving a capacitive load. For this first blog, the general current-to-voltage conversion process and challenges will be discussed. In addition, the EVAL-KW4503Z will be introduced, highlighting its capabilities and features useful in analyzing op amp stability.
Current to Voltage Conversion
A Transimpedance Amplifier (TIA) is a type of amplifier configuration that converts current into voltage. TIAs are used to transform the current output of sensors, like the photodiode, into a voltage signal that is compatible with most electronic circuits and instruments. They are commonly used in optical communication systems, imaging systems, medical devices, and many other applications.

Figure 1: Current to Voltage conversion using a Transimpedance Amplifier
The transformed voltage output from the TIA must be accurate, undistorted, and stable (does not oscillate) to preserve the integrity of the original signal and prevent potential damage to the instrument or system, particularly in the succeeding stages following the TIA. To do this, one must be knowledgeable about the factors that can cause the amplifier to become unstable, as well as the compensation techniques that can be used to reduce or eliminate these instabilities.

Figure 2: Unstable vs. Stable Output Voltage Signal coming from a Transimpedance Amplifier
Introducing the EVAL-KW4503Z
The EVAL-KW4503Z, or Stability + LED Carrier KWIK Demo Board, is a Know-how With Integrated Knowledge (KWIK) demonstration board used in conjunction with the ADALM2000. It is designed to educate its users about the stability analysis of an operational amplifier configured as a Transimpedance Amplifier or TIA.
Additionally, EVAL-KW4503Z also supports the stability analysis of a unity-gain follower operational amplifier driving a capacitive load. It is a complete demonstration board package that enables its users to predict, measure, and simulate the stability and phase margin of an operational amplifier. This is useful, especially in designing TIAs and driving capacitive loads to reduce errors, improve signal accuracy, and avoid damaging a component in the signal chain.

Figure 3: EVAL-KW4503Z (Stability + LED Carrier KWIK Demo Board)
The EVAL-KW4503Z uses the ADA4510-2, which is a dual-channel, 40 V, high-precision, low input bias current, low offset voltage, low offset voltage drift, low noise, rail-to-rail input, and output operational amplifier that can be used at any point of the signal chain, including sensing, conditioning, and output drive.
EVAL-KW4503Z uses one channel of the ADA4510-2 for the TIA stability KWIK demo, which provides a hands-on platform allowing users to select from three compensation options via a jumper-configurable feedback network: a marginally stable design, a design with 45° phase margin, and a design with >70° of phase margin.

Figure 4: Transimpedance Amplifier (TIA) Stability KWIK Demo
EVAL-KW4503Z uses the other channel of the ADA4510-2 for the capacitive load stability KWIK demo, which provides a hands-on platform showing how to stabilize a precision, 10 MHz op amp driving a 1nF capacitive load. This will enable users to learn how to eliminate unwanted oscillations in the output voltage signal while ensuring that the op amp and the subsequent stages in the signal chain remain protected from damage.
Figure 5: Capacitive Load Stability KWIK Demo
Both the TIA stability KWIK demo and Capacitive load stability KWIK demo are combined into a single, easy-to-use board that plugs directly into the ADALM2000. The ADALM2000 is an all-in-one package that combines several “bulky” laboratory equipment into a portable test and measurement instrument, just about the size of a calculator.
Figure 6: EVAL-KW4503Z’s Schematic

Figure 7: EVAL-KW4503Z with ADALM2000
Key Insights
Ensuring the stability of Transimpedance Amplifiers (TIAs) and operational amplifiers when driving capacitive loads is crucial in maintaining the integrity of the original input signal. Without compensating for these “instabilities”, unwanted oscillations will occur on the output signal of the op amp, which could potentially damage itself and other components after it.
Using the EVAL-KW4503Z, one can easily learn how to stabilize both an operational amplifier configured as a TIA and an operational amplifier driving a capacitive load. It will help users understand how to remove unwanted oscillations from the output signal, reduce errors, improve signal accuracy, and prevent damage to a component in the signal chain.
In the upcoming parts of this series, we’ll take a deeper dive into the Transimpedance Amplifier Stability KWIK Demo and the Capacitive Load Stability KWIK Demo.
Read all the blogs in the Amplifier Stability Essentials series.