The question isn’t whether space‑qualified RF transceivers demand careful power design; it’s how far you need to go once radiation, noise, and board area all start pushing back at the same time. That tension is exactly what the ADPS20174-RD was built to address: a high-reliability, radiation-hardened power architecture optimized for an agile RF transceiver, where noise performance, physical size, and qualification level are fixed constraints, not optimization knobs.
This design is not about assembling compliant parts. It is about making architectural decisions that survive real space‑system trade-offs.
When Flexibility is Critical, Powering Is Different
The AD9361S‑CSH is the commercial‑space, high‑reliability variant of ADI’s widely deployed agile RF transceiver, targeting satellite communications payloads where flexibility is critical. That flexibility, however, comes with a well‑understood sensitivity to supply noise.
Three rails dominate the power discussion:
- 3V analog core (VDDA_X) at approximately 1.1A
- 8V interface rail
- 3V GPO rail
The challenge is not regulation accuracy alone. The real risk is noise coupling between rails, particularly when digital activity contaminates analog domains. In space hardware, filtering is not a universal fallback. Added impedance in the supply path directly impacts transient response, limiting how quickly the rail can respond to load steps and increasing the risk of voltage droop under dynamic conditions. Board area, mass, and qualification constraints further restrict how far filtering can be pushed, making architectural partitioning, not post‑filtering, the primary tool for preserving supply integrity.
Architectural Principal
The question isn’t whether to collapse rails for simplicity; it’s how to preserve spectral integrity while managing power efficiently. In the ADPS20174‑RD architecture, noise‑sensitive rails are deliberately grouped and isolated from noisier domains, rather than forced into a common low‑voltage plane. This extends the proven partitioning strategy of the AD‑FMCOMMS5‑EBZ platform into a space-qualified implementation, reducing noise injection paths while avoiding the component overhead of fully discrete isolation. The alternative, tying all 1.3V rails together, saves area but couples analog, clock, and digital noise, a trade that inevitably surfaces as degraded RF margins. Instead, the design switches once using a radiation‑hardened RH1959 buck stage, then cleans up locally with RH3083MK and RH1086M low-dropout regulators (LDOs), all MIL‑PRF‑38535 Class V devices. The result is a controlled balance: high efficiency and manageable thermal dissipation at the front end, followed by low‑noise regulation where it matters, delivering approximately 45µVrms integrated noise on the 1.3V analog rail (VDDA), measured over the bandwidth relevant to RF performance.
Despite this deliberate partitioning and heritage‑driven architecture, the complete ADI solution remains remarkably compact, evidence that disciplined rail grouping and selective post‑regulation can preserve RF performance without sacrificing power density.

Figure 1: ADPS20174-RD Power Solution: Power Tree Block Diagram
Size vs. Noise: A Constraint That Never Disappears
Space power design always circles back to the same uncomfortable question:
Do you want the smallest solution, or the quietest one?
The practical answer is neither. You want the quietest solution that still fits.
The ADPS20174‑RD was designed around that boundary. Magnetic components and LDO count were minimized without collapsing noise domains. Output noise stays well below the 65µVrms requirements, while maintaining current margin on the 1.3V rail.
Cool Design Product Choice: Where the RH1959 Fits
In this architecture, the RH1959 is selected for its system-level efficiency rather than headline specifications. Its quiescent current of approximately 50µA reduces overhead power dissipation during light-load and standby conditions, which are common in duty-cycled or mode-switching payloads. When a single upstream converter feeds multiple low-noise rails, that reduction translates directly into thermal margin and longer-term reliability, not just improved efficiency on paper.
This Reference Design Is and Is Not
The ADPS20174‑RD is not a drop‑in power module. It is a validated architectural template for powering noise‑sensitive RF silicon in radiation‑constrained environments.
It answers the questions designers face:
- Which rails must remain isolated?
- Where does switching noise materially affect RF performance?
- How small can the solution be before margins erode?
Just as importantly, it shows where not to optimize.
Conclusion
Powering agile RF in space is never about finding one perfect answer. It's about navigating the tensions that define the design (noise against size, flexibility against isolation, efficiency against the margins) that keep your link alive when it matters most. The ADPS20174-RD reference design doesn't resolve those trade-offs for you; it gives you a proven architecture for making them with confidence. You know which rails to keep apart, where switching noise actually bites, and how far you can push toward compact before performance starts to slip. When your next mission asks the same uncomfortable question (smallest, or quietest?), you'll have a clear place to start, and a clearer sense of where not to compromise.
Click here to learn more about ADI System-Level Power Solutions
Read the SystemLevel Power Solutions series blogs.