Ambient temperature is critical to functional safety, and in this blog, I will explore several aspects of that assertion.
Semiconductors and all electronic products age faster and reach their end of life faster with increasing temperature, and if you have based your reliability predictions on an underestimated temperature, you might suffer premature failure. More importantly, if you buy a product rated from -40 °C to 105 °C and the temperature goes to 106 °C, you are using it outside its specification, which is not allowed. In fact, IEC 61508 requires derating and that you justify using any device at its limits. IEC 61800-5-2 requires specific testing to ensure all components are used within their specifications during normal operation.

Figure 1: An extract from IEC 61800-5-2:2016
But what if it’s not normal operating conditions? If the temperature is elevated because you:
- Underestimated how harsh the environment is
- A cooling system or fan has failed
- There is a failure of some component on your PCB heating all nearby components
In these cases, your safety function may no longer be operating as designed.
For redundant systems, exceeding the maximum operating temperature of your components is a good source of CCF (common cause failures), leading to both of your redundant channels failing in the same way at the same time.
Direct temperature measurement on your PCB is a very good solution for all the problems above.
Ideally, such a temperature sensor should be:
- Small - less PCB space and a lower thermal mass, so it responds quickly
- Require a minimum of external components - a small solution rather than just a small package
- Able to operate at much higher and lower temperatures than the circuits it protects, since if the temperature sensor can’t cope with unexpected temperatures, it won’t offer much protection.
- Able to work without a uC - otherwise a failure due to overtemperature in the uC can cause a failure in the temperature sensor or make it ineffective
- Be able to assert a safe state - typically stop communications, which is detectable at the system level, or somehow shut down the system
Some nice parts, such as the ADT7302 (specified from -40’C to 125’C) and ADT7301 (operates from -40’C to 150’C) come in an SOT-23 package and therefore meet most of the above requirements. However, they do require a uC to operate and shut down the system.

Figure 2: An extract from the ADT7301 datasheet
A temperature switch is better for functional safety. One such family of devices is the MAX31827/MAX31828/MAX31829 family. These parts are:
- Specified from -45’C to 145’C with +/-1.75’C accuracy and a tighter accuracy of +/-1’C from -40’C to 125’C
- Has an open-collector output that can be used directly without a uC to put other circuits or the uC into reset
- Built-in hysteresis so that if they trip, they won’t reset until the temperature changes by several degrees
- The standard part comes with a trip point set to 90’C and -40’C

Figure 3: Datasheet extract for the temperature switch
They can also be connected to a uC over an I2C bus, but for safety applications the open drain output is important to assert a safe state without requiring the uC.
There is also a series of 1-WIRE® devices with a similar temperature range and similar open-collector output, and they can be powered over the 1-WIRE® interface, but in this parasitically powered mode they lose the open-collector output functionality. An example part is the MAX31825.

Figure 4: 1-WIRE® temperature sensor
Multiple devices can exist on the same 1-WIRE® bus, and each has its own unique 64-bit chip ID, in case you implement multiple redundant sensors. This functionality can be important when you might need to monitor several points around your PCB.
For all previous blogs in this series, see here.
Related Blogs
- Derating in IEC 61508
- How to Quantify Common Cause Failures
- Reliability Predictions for Integrated Circuits
For the full suite of ADI blogs on the EngineerZone platform, see here.
For the full range of ADI products, see here.