ADRV9040
Recommended for New Designs
The ADRV9040 is a highly integrated, system on chip (SoC) radio
frequency (RF) agile transceiver with integrated digital front end
(DFE). The SoC contains...
Datasheet
ADRV9040 on Analog.com
LT8627SP
Recommended for New Designs
The LT8627SP synchronous step-down regulator features third-generation Silent Switcher technology which is uniquely designed to combine an ultralow noise...
Datasheet
LT8627SP on Analog.com
We will show you how Analog Devices, (ADI) ADRV9040 RF transceiver is transforming the way engineers design, implement, and evaluate modern 5G radio chains. We’re bringing it all together in this last part of the series: the 5G peaks challenge from Part 1, and how crest factor reduction (CFR) and digital predistortion (DPD) let us harness amplifier power from Part 2.
Every radio designer wants higher performance, a simpler bill of materials (BOM), and greener, more compact equipment. The ADRV9040 is manifest proof that, with the right technology, you really can have it all.
Legacy approaches to complex base station radios involved chains of separate FPGAs, digital signal processing (DSP) blocks, and countless custom interface headaches. The ADRV9040 changes the game.

Figure 1: An ADRV9040 High Level Functional Block Diagram
Eight transmitters, two observation receivers, eight receivers, an integrated local oscillator (LO), and clock synthesizers, plus a full digital front end with DPD, CFR, digital upconversion (DUC), and digital downconversion (DDC) on one silicon system-on-chip (SoC).
This RF system-on-chip does what used to take several discrete components, dramatically shrinking board space, reducing weight, and slashing power consumption. It’s not just for flagship macro radios, either. The ADRV9040’s agility brings massive MIMO, small cell, and multiband systems to life with minimal engineering friction.
Bandwidth matters, but so does form factor. Here’s where the zero-IF (ZIF) architecture shines. ZIF enables ultra-wide bandwidth, supports flexible, multicarrier radio units, and delivers size and power advantages over older architectures.
By cutting the number of external FPGAs and analog components needed, the ADRV9040 slashes RF BOM costs, enabling radios that are 40% lighter and ~10% more energy efficient.

Figure 2: 5G New Radio (NR) Signal Before and After Applying CFR
Even after peak reduction, the optimized complementary cumulative distribution function (CCDF) trace (right) closely resembles a Gaussian, indicating that designers can trust their signal integrity is preserved while keeping spectral regrowth in check.
Our implementation of CFR and DPD is truly set and forget. The three-stage CFR engine operates autonomously, detecting and correcting peaks using sophisticated pulse cancellation, and stays agile to system configuration needs (two correction pulses can be preloaded at once for seamless carrier switching).
On the DPD side, expect industry-leading results: the algorithm is grounded in a powerful blend of generalized memory polynomial and dynamic deviation reduction, computed right on the device’s dedicated Arm Cortex® A55 processor.

Figure 3: An Inverse PA Model Is Applied to the Interpolated Digital Baseband Samples
The DPD actuator recreates the anti-distortion profile by computing coefficients on-chip and supports both indirect (faster) and direct (finer-grained) adaptation.
No need for external DSPs; this is high science, natively integrated.

Figure 4: Power Spectral Density Showing Improvement in ACLR Post-DPD
Real-world proof: out-of-band mistakes on the left get cleaned up after the DPD is active (right), keeping your system compliant and your channel neighbors happy.
Our best-in-class Silent Switcher® regulators (such as the LT8627SP and ADM7172) power the ADRV9040 quietly, with lightning-fast transient response and ultra-low electromagnetic interference (EMI). First-symbol error vector magnitude (EVM) issues at time division duplex (TDD) transitions. Effectively banished.

Figure 5. System-level block diagram of a macro remote radio head (RRH) with the ADRV9040 power solutions.
Evaluation couldn’t be easier, either. With the ADS10-V1EBZ and ADRV904X-MB/PCBZ evaluation platform, just plug in your gear; these do the heavy lifting, and you can capture every performance metric and plot it fast.

Figure 6: The ADS10-V1EBZ (Motherboard) and ADRV904X-MB/PCBZ Evaluation Board
From taming 5G’s wildest peaks to integrating industry-leading linearization, the ADRV9040 transceiver isn’t just another chip; it’s a launchpad for the future of wireless. It enables sharper, smaller, greener radios, with all the intelligence for managing peak-to-average power ratio (PAPR), CFR, and DPD built in.
Read the full technical article Simplifying Your 5G Base Transceiver Station Transmitter Line-Up, Design, and Evaluation.
Read all the blogs in the 5G Transmitter Design series.