AD9956
Recommended for New Designs
The AD9956 is Analog Devices’s first AgileRF synthesizer.
The device is comprised of a DDS and PLL circuitry. The DDS
features a 14-bit DAC operating up...
Datasheet
AD9956 on Analog.com
AD9914
Recommended for New Designs
The AD9914 is a direct digital synthesizer (DDS) featuring a 12-bit DAC. The AD9914 uses advanced DDS technology, coupled with an internal high speed,...
Datasheet
AD9914 on Analog.com
AD9915
Recommended for New Designs
The AD9915 is a direct digital synthesizer (DDS) featuring a 12-bit DAC. The AD9915 uses advanced DDS technology, coupled with an internal high speed,...
Datasheet
AD9915 on Analog.com
AD9164
Recommended for New Designs
The AD91641 is a high performance, 16-bit digital-to-analog converter (DAC) and direct digital synthesizer (DDS) that supports update rates to 6 GSPS....
Datasheet
AD9164 on Analog.com
As promised in my last post, here is [PART 1 of] a review of some subtleties of the table contrasting DDS/PLL strengths. I know I didn’t [initially] say anything about breaking this up into 2 parts, but after I started writing, I realized it was getting too long for a single entry, so I went back, edited the last post and finished writing this!
I’ll start with the characteristics I identified as being better suited to a DDS.
Frequency Resolution – There are a few nuances here…
There exists a DDS which runs at 400 MSPS with a 48 bit tuning word (AD9956). This yields a tuning resolution of no worse than 1.42 µHz, yes that’s microHertz. The resolution of a standard PLL is limited by the depth of the dividers in the loop, and they are a few orders of magnitude worse than this. I would be remiss however if I didn’t point out that there are fractional-N PLLs (N being the division factor in the feedback divider in the PLL) which close the gap significantly. There is a downside to using a frac-N PLL: more spurs in the output. The signals are more jittery.
Another thing to note is that a standard DDS cannot hit many exact ratios. In the standard DDS frequency equation the denominator is a fixed power of 2. So, for example, if you have a 200 MHz sample clock, you can hit 50 MHZ exactly (/4), but you cannot hit 40 MHz exactly – you will be off by some tiny bit: if you used the AD9956, you could either be 0.142uHz less than 40 MHz, or 0.568uHz more than 40 MHz.
Standard PLLs hit these precise ratios quite easily. As such if you need exact ratios, avoid the standard DDS. BUT that doesn't mean you need to avoid DDS as a whole, if you like the other things about DDS, look to Programmable Modulus!
The Programmable Modulus DDS (which I, affectionately, refer to as p-mod) is a relatively recent innovation in DDS. A P-MOD DDS allows you to alter the DDS equation so that the denominator is no longer restricted to a power of 2. No PLL can compete with a P-MOD DDS (AD9913, AD9914, AD9915, AD9164 e.g.) for frequency resolution; I believe that is inherent. I suspect I will write more about P-MOD in a future entry; you can also read about it here.
Returning to the 40 MHz example above, the industrious engineer could design a system which used frequency hopping to spend 80% of the time just below 40 MHz and 20% just above 40 MHz, and you would not only end up with a signal that averaged 40 MHz, you would also mimicking the internal workings of a P-MOD.
I promise the rest of these will be shorter!
Frequency Agility
There are ways to introduce varying frequencies in PLLs, but they are not as well controlled, nor are they as repeatable as the digital approach available with DDS.
Frequency hops can be implemented with two parallel PLLs and a switch (They call ‘em ping-pong PLLs – no table, paddles or net required), but you either need one complete PLL for every frequency you might want to hop to, OR you need to allow some settling time if you change the frequency of the bypassed PLL.
You can also sweep frequency with a variable divider in the loop, but it is nowhere near as well-controlled or repeatable as a DDS based sweep
Phase Resolution & Agility
In an analog PLL, any adjustment to phase ends up cycling through the loop, so it’s not a precise, repeatable change like you get with a DDS. Digital PLLs enable some level of phase adjustment capability.
Amplitude Resolution & Agility
Amplitude is not a parameter that PLLs vary.
Look forward to part II in the not too distant future. Questions may be posed either in the comments, or in the DDS Product Section of ADI’s EngineerZone.