A humanoid index finger touching a human index finger.

Balancing Innovation and Safety in Humanoid Robotics

By Declan Staunton, Tracey Johnson & Margaret Naughton

Humanoid robots are no longer confined to research labs; they are beginning to appear in factories, warehouses, hospitals, and even public spaces. As we embrace this new generation of automation, one question becomes impossible to ignore: Are these robots safe enough to work alongside people?

Before answering the question of safety, let’s start by introducing a new acronym, DSIMR, which stands for Dynamically Stable Industrial Mobile Robot. Uniquely, this classification of robot actively balances itself and will fall over if they lose power. Humanoid robots fall into this category, with the potential for unpredictable recovery movements, so they require special safety rules.

In this blog, we will explore the emerging safety challenges of humanoid robots and examine the technologies, safety functions, and standards that will help ensure they can operate safely alongside people. To help address these emerging challenges, a panel of experts within ISO Technical Committee 299 (Robotics) has begun developing a series of standards focused on the safe deployment of humanoid and other dynamically stable mobile robots. One of the first standards under development is ISO/CD 25785-1, Robotics – Safety Requirements for Dynamically Stable Industrial Mobile Robots (Legged, Wheeled, or Other Forms of Locomotion) – Part 1: Robots. The standard is intended to provide requirements and guidance for risk reduction measures applicable to DSIMRs operating in industrial environments, helping manufacturers address the unique safety challenges posed by these highly mobile and adaptable machines. While not covered in any detail in this blog, part 2 of the standard shall address safety requirements for the integration and application of DSIMRs.

Building Upon Existing Standards

ISO 10218-1:2025 defines an industrial environment as a "workplace where the public is restricted from access or is not reasonably expected to be present for the intended tasks and robot application(s)." As a result, the scope of ISO 25785-1 is limited to industrial applications and does not cover humanoid robots operating in public spaces. As humanoids move outside the factory and into social spaces, the standards will evolve to incorporate these workplaces, but for now, humanoid standards focus on operating within industrial environments.

The Mechanics of Staying Upright

Most of us rarely think about what it takes to stay upright. Yet every step we take relies on a sophisticated balance system involving our brain, sensory organs, and musculoskeletal structure. Together, these systems continuously monitor and adjust our posture to keep our center of gravity above our base of support (the space between and including our feet). When the center of gravity moves outside this area, balance can no longer be maintained, and a fall becomes inevitable unless a rapid corrective action is taken. Understanding this principle is essential when considering how humanoid robots achieve and maintain stability while operating in the real world.

 Center of Gravity Basics

Figure 1: Center of Gravity Basics

The loss of stability in a humanoid robot can introduce significant hazards, particularly when the robot is operating in close proximity to people. Unlike traditional industrial robots that are typically fixed in place, humanoid robots rely on dynamic balancing to remain upright and perform their tasks. As a result, ensuring their safe operation requires the development of novel risk reduction measures, including controlled stability functions, separation monitoring to maintain safe distances from people, and continuous stability monitoring to detect and respond to conditions that could lead to a loss of balance or a fall.

 ISO 13855:2024 Subclause 4.8

Figure 2: ISO 13855:2024 Subclause 4.8

 

Speed and Separation Control (SSC)

Maintaining a safe distance between humanoid robots and the human body requires deploying the SSC safeguarding technique described in ISO 13855:2024. This approach reduces risk by maintaining a dynamic protective separation distance between the robot and a person, continuously adjusting the robot's speed, motion, or trajectory in response to human movement. If the separation distance falls below a predefined threshold, the robot can slow down, stop, or transition to a safe state before hazardous contact occurs.

 Speed and Separation Control Zones Overview

Figure 3: Speed and Separation Control Zones Overview

To ensure people can work safely alongside humanoid robots, the safety functions responsible for preventing hazardous situations must be highly dependable. Whether monitoring stability, stopping functions, or maintaining safe separation distances, these functions should be designed and validated to meet the performance requirements defined by internationally recognized functional safety standards, including ISO 13849-1, IEC 62061, and IEC 61508.

Key Takeaways

Unlike traditional industrial robots, humanoids must maintain dynamic balance while moving through shared human environments. As a result, future safety frameworks will increasingly focus on stability monitoring, speed and separation control, functional safety, and motion-control systems. Emerging standards such as ISO 25785 will be critical in ensuring that humanoid robots can safely coexist and collaborate with people in industrial settings.

At Analog Devices, our commitment to our customers includes a thorough product development process, an established zero-defect culture, and in-house industry-certified functional safety domain experts to help you build your products to meet third-party certification standards and accelerate your time to market. Read more on Tom Meany’s Safety Matters Blog Series.

Read all the blogs in the Humanoid Robotics series.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.