Phased-array radars, multi-channel spectrum analyzers, and massive MIMO front-ends require that all ADCs and DACs remain phase-coherent to operate as a single, synchronized system. JESD204B Subclass 1 achieves this using SYSREF and Multi-Chip Synchronization (MCS), providing deterministic latency across power cycles and resets. However, SYSREF requires careful implementation, as timing errors or distribution skew can cause phase slips and coherence loss.
Key Parameters

Figure 1. Key Timing Parameters and Concepts in JESD204 Subclass 1 Multi-Chip Synchronization (MCS).
Key timing parameters for JESD204 Subclass 1 synchronization, including SYSREF, LMFC/LEMC, and Multi-Chip Synchronization (MCS). The figure above also highlights SYSREF setup and hold requirements and the resulting phase ambiguity if timing constraints are violated.
Phase 1: SYSREF Signal Integrity
SYSREF must arrive at every device as a clean, low-jitter, correctly terminated differential signal. The four most common distribution failures are:
- Trace length mismatch. A 200-mil difference between the SYSREF+ and SYSREF rails introduces tens of picoseconds of skew. Match lengths to within 5 mils.
- Daisy chain topology. Each fanout stage accumulates delay. Use a star topology from a dedicated SYSREF fanout buffer instead.
- Missing termination. Place a 100 Ω differential termination resistor close to each receiver. Reflections without it will corrupt the capture edge.
- Supply noise. SYSREF is unusually jitter-sensitive. Dedicate a filtered LDO to the clock distribution network and never share a rail with high-current digital logic.
- Verify SYSREF integrity with a differential probe at each receiver before executing MCS. Any ringing or setup/hold violation observed here will become an intermittent MCS failure downstream.
Phase 2: The MCS Sequence
The MCS sequence forces every device to assert its LMFC rising edge at the same instant. For a multi-chip ADRV9009 system:
Step 1. Assert synchronous reset on all converters and the FPGA JESD204 IP simultaneously.
Step 2. Enable one-shot SYSREF capture on each device. Continuous mode risks relatching on a spurious edge during normal operation.
Step 3. Issue a single SYSREF pulse via the clock IC (HMC7044 or LMK04828), timed to land on a clean LMFC boundary. Confirm the pulse count in the clock IC status register.
Step 4. Release reset across all devices.
Step 5. Verify LMFC alignment by reading the phase status register in each device. ADI ACE exposes this under the JESD204 diagnostics panel.
The most common failure at this stage is that one device latches SYSREF exactly one LMFC cycle late, producing a fixed-looking phase offset that resembles a calibration error rather than a synchronization fault. The correct diagnostic is to repeat MCS ten times. A coherent system returns bit-exact offsets on every run. A device with a marginal SYSREF window does not.
Phase 3: Validation
Completing MCS is not proof of coherence. Three checks must always follow:
- Cross-device LMFC comparison. After every MCS run, the phase offset between any device and the reference must be zero or a known fixed value. Any variation across iterations points to a SYSREF timing margin problem.
- Power cycle repeatability. Power the system down and back up ten times, re-running MCS each time. The inter-device phase must be identical on every cycle. This is the test most lab bring-ups skip, and most production failures expose.
- Spectral coherence. Apply a common RF tone to all ADC inputs and compare FFT phase across channels. A phase offset that changes across resets confirms MCS is not achieving deterministic alignment.
Repeat the full validation sequence across the operating temperature range. Setup-and-hold margins shift with temperature, and a system that passes at room temperature can lose coherence at thermal extremes.
Phase 4: Real World Failure Modes

Figure 2. Common Real-World Failure Modes in JESD204 Multi-Chip Synchronization
The chart lists common synchronization failures encountered in practical JESD204 systems, their underlying causes, and recommended mitigation techniques to ensure reliable Multi-Chip Synchronization (MCS) and deterministic latency.

Figure 3: Coherence Failure Taxonomy: Signal Integrity Faults, MCS Sequence Errors, and Thermal Margin Loss
Key Takeaways
Multi-chip synchronization is a layered problem. Signal integrity must be solved before MCS can function reliably. The sequence must be executed in the correct order, with one-shot capture enabled, and then verified by reading LMFC phase offsets from each device. Validation must cover power cycle repeatability and temperature extremes, not just initial bring-up. The failure modes above, particularly silent phase ambiguity and chassis-induced jitter, are invisible to standard link health registers and only surface through deliberate coherence measurement.
Using ADI ACE SYSREF timing diagnostics alongside cross-device LMFC comparisons and spectral coherence checks turns MCS failures from mysterious to diagnosable. A few hours of careful measurement at bring-up is far less costly than discovering a coherence bug after full system integration.
Read all the blogs in the Transceiver to FPGA series.