A person at the peak of a snowy mountain overlooking other peaks watching the sunset.

SMPS Design Secrets: Master DCM and CCM Modes Today

Power supplies are the unsung heroes of electronic devices, ensuring precise, stable DC voltages reach your circuits. But the magic behind these workhorses lies in understanding how they operate, specifically, the critical distinction between Continuous Conduction Mode (CCM) and Discontinuous Conduction Mode (DCM). Whether you're designing cutting-edge power electronics or simply curious about what makes your devices tick, this comprehensive six-part blog series from the Engineering Mind will transform how you approach switching-mode power supply (SMPS) design.

Why These Modes Matter

At the heart of every buck, boost, and flyback converter lies an inductor whose current behavior determines efficiency, ripple, and overall performance. In CCM, the inductor current never drops to zero during a switching cycle, flowing continuously from input to output. This continuous flow creates predictable voltage relationships, lower output ripple, and higher efficiency at moderate to heavy loads. The current smoothly oscillates between minimum and maximum values, making it ideal for applications demanding stable power delivery.

In contrast, DCM occurs when the inductor fully discharges each cycle, with current dropping to zero for a portion of the switching period. This happens when loads are light, inductance is too small, or switching frequency is high. The cycle divides into three phases: T1 (coil charging), T2 (coil discharging to zero), and T3 (dead time with no current). While DCM introduces higher ripple and load-dependent voltage transfer functions, it offers advantages for low-power applications, including simpler magnetics and reduced component stress.

Between these extremes lies Boundary Conduction Mode (BCM), where the inductor current just touches zero at the end of each cycle. This sweet spot combines the benefits of both modes, making it attractive for wide-load-range operation.

Journey Through the Series

Part 1: Exploring DCM and CCM in SMPS sets the foundation by introducing the fundamental principles of inductor current operation. You'll discover how switching frequency, duty cycle, input/output voltages, and inductance values interact to determine which mode your converter inhabits. The post establishes that careful circuit design can influence whether your SMPS operates in CCM, DCM, or BCM, but warns that without proper attention, changing conditions can unexpectedly shift your design into another mode.

Part 2: Diving into Coil Events explores what actually happens inside the inductor during each conduction mode. The inductance principle ΔI = VL/L × t reveals that constant voltage across a coil creates linear current slopes. In SMPS designs, switching between Vin and ground creates characteristic sawtooth waveforms, one slope rising during the ON period, another falling during the OFF period. Understanding that VL and V'L depend on Vin, Vout, Ton, Toff, and L empowers you to size components correctly and predict circuit behavior.

Part 3: Mastering Efficient Voltage Regulation with a Buck Converter shifts focus to practical efficiency considerations. Buck converters excel at step-down voltage conversion, but choosing between CCM and DCM can significantly affect performance. The post explains how to calculate the boundary conduction current and select operating modes based on load range: maintain CCM above the boundary for optimal overall efficiency, allow DCM below to minimize quiescent losses, while considering control-loop compensation and component selection (low-RDS(on) MOSFETs, fast recovery diodes, appropriately sized inductors).

Part 4: Stepping into Transfer Functions of a Buck in DCM delivers the mathematical rigor engineers need. Using power balance methods (Pin = Pout at steady state), the series methodically derives that DCM's transfer function is more complex than CCM's simple Vout = d×Vin relationship. The output voltage becomes Vout = kVin/2 × [-1 + (1+2/k)^1/2], where k incorporates duty cycle, switching period, load resistance, and inductance. Despite this complexity, the mathematical proof confirms that buck converters in DCM still perform step-down conversion, validating their fundamental behavior while highlighting how the load current shapes the relationship between voltage and current.

Part 5: Jumping into Boost, Inverter, and Flyback Cases extends the principles of DCM and CCM beyond the basic buck topology. Each converter type boost (step-up), inverting (negative output), and flyback (isolated)exhibits unique behavior in different conduction modes, requiring tailored design approaches for optimal performance.

Part 6: Apples and Oranges: A Comparative Study brings the series full circle by directly comparing CCM and DCM across multiple dimensions. This comparative analysis helps you make informed decisions about which mode best suits your specific application requirements, load profiles, and efficiency targets.

Why You Should Read This Series

By mastering these conduction modes, you'll transform from simply following reference designs to truly understanding the "why" behind component selections and control strategies. You'll learn to:

  • Predict and control mode transitions as load conditions change
  • Optimize inductor sizing for your specific application
  • Design compensation networks appropriate for each mode
  • Maximize efficiency across wide load ranges
  • Troubleshoot unexpected behavior in existing designs
  • Make informed trade-offs between component cost, size, and performance

Whether you're fine-tuning an existing design or starting a fresh project, this knowledge proves invaluable for creating efficient, reliable power supplies that perform optimally under real-world conditions.

Start Your Journey Today

Don't let power supply design remain a mystery wrapped in datasheets and application notes. Head over to EngineerZone, The Engineering Mind Blog, and explore this six-part series on DCM and CCM in SMPS. Each installment builds on the previous, creating a comprehensive education in switching-mode power supply fundamentals that will elevate your engineering skills and empower you to design better power systems.

The engineering mind thrives on understanding, and there's no better way to understand your power supplies than mastering the modes that define their operation. Start reading today and unlock the full potential of your SMPS designs!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.