KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LM399
Production
The LM199/LM399 precision shunt reference features excellent temperature stability over a wide range of voltage, temperature and operating current conditions...
Datasheet
LM399 on Analog.com
AD5761
Production
The AD5761/AD5721 are single channel, 16-/12-bit serial input,
voltage output, digital-to-analog converters (DACs). They operate
from single supply voltages...
Datasheet
AD5761 on Analog.com
AD5781
Production
The AD5781 is a single 18-bit, unbuffered voltage-output DAC that operates from a bipolar supply of up to 33 V. The AD5781 accepts a positive reference...
Datasheet
AD5781 on Analog.com
AD5685R
Production
The AD5685R nanoDAC+â„¢ is a quad, 14-bit, rail-to-rail, voltage output DAC. The device includes a 2.5V, 2ppm/ËšC internal reference (enabled by default...
Datasheet
AD5685R on Analog.com
AD7982
Production
The AD7982 is an 18-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. The AD7982 contains...
Datasheet
AD7982 on Analog.com
AD4000
Production
The AD4000/AD4004/AD4008 are high accuracy, high speed, low power, 16-bit, precision successive approximation register (SAR) analog-to-digital converters...
Datasheet
AD4000 on Analog.com
ADHV4702-1
Recommended for New Designs
The ADHV4702-1 is a high voltage (220 V), unity-gain stable precision operational amplifier. The ADHV4702-1 offers high input impedance with low input...
Datasheet
ADHV4702-1 on Analog.com
ADA4700-1
Recommended for New Designs
The ADA4700-1 is a high voltage, precision, single-channel operational amplifier with a wide operating voltage range (±5 V to ±50 V) and relatively high...
Datasheet
ADA4700-1 on Analog.com
LT6375
Recommended for New Designs
The LT6375 is a unity-gain difference amplifier which combines excellent DC precision, a very high input common mode range and a wide supply voltage range...
Datasheet
LT6375 on Analog.com
LT1997-3
Recommended for New Designs
The LT1997-3 combines a precision operational amplifier with highly-matched resistors to form a one-chip solution for accurately amplifying voltages. Gains...
Datasheet
LT1997-3 on Analog.com
LT5400
Recommended for New Designs
The LT5400 is a quad resistor network with excellent matching specifications over the entire temperature range. Matching is also specified when the LT5400...
Datasheet
LT5400 on Analog.com
LT1997-2
Recommended for New Designs
The LT1997-2 is an attenuating (funnel) difference amplifier
that can be used to translate large differential signals to
the low voltage range compatible...
Datasheet
LT1997-2 on Analog.com
AD5522
Production
The AD5522 is a high performance, highly integrated parametric measurement unit consisting of four independent channels. Each per-pin parametric measurement...
Datasheet
AD5522 on Analog.com
Written by
hirobert and
mkaiserm
This blog post explains how to implement a leakage test using a common piece of equipment, a source measure unit (SMU) and introduces a simplified circuit based on high voltage amplifier components which forces voltage and measures current. In this blog, you will learn about how to apply these two methods to MOSFET leakage testing.
MOSFETs are a very common component found in switching and automotive applications, supporting low voltage or high voltage swings and with a wide range of current drive. The number of high power applications is increasing, generating additional demand for Power MOSFETs. To produce this growing number of Power MOSFETs, more manufacturing test capacity is required. Many companies are developing products to serve the Power MOSFET testing need in addition to established semiconductor ATE vendors.
On the Power MOSFET production line, each device is tested to ensure that it meets the datasheet specifications. Leakage is a key performance metric which can be challenging to test in high voltage devices.
Let’s take Infineon Power MOSFET IPA100N08N3 as an example. Figure 1 shows the electrical characteristics from IPA100N08N3 datasheet.

Figure 1
Gate leakage current is usually determined by forcing a voltage and measuring the resulting current. The leakage current can vary due to the quality of the oxide or the physical property of the materials.
For IPA100N08N3, when VGS, VDS=0V, the IGSS max value should be below 100nA. This IGSS leakage test determines what is a good part to be shipped to customers versus a bad one to be discarded.
Generally speaking, MOSFET gate driver voltage range is +-20V, and GaN may be even lower. Figure 2 shows basic topology to test gate leakage current value.

Figure 2
First the Source and Measure Unit (SMU) method is described and then a simplified force voltage, measure current circuit is introduced.
SMU
SMU is a four-quadrant source and sink operation equipment with measure functions, which adopts FVMI (force voltage, measure current) and FIMV (force current, measure voltage) modes. It can source a specified voltage and measure the current. It can also source a specified current and then measure the voltage through the DUT.
SMU’s can achieve a very low current range (nA, pA) with a resolution of fA, even aA. Therefore, there is no doubt that SMU’s can measure MOSFET leakage current accurately. Figure 3 gives the specification from Tektronix SMU2450 as an example.

Figure 3
Figure 4 shows the typical topology to test leakage current. Note that three SMU channels are required to implement the MOSFET leakage test.

Figure 4
FVMI mode: Set an output voltage typically from a DAC, amplify by power stage, measure current through selected sense resistor for the range, provide feedback on the voltage applied in DUT to the output voltage point, to make the DUT voltage is equal to the set voltage.
FIMV mode: Set an output current typically from a DAC, amplify by power stage, measure current through selected sense resistor for the range, provide feedback the voltage of sense resistor to output current setting point, to make sure the current flowing through DUT is equal to the set current.
Figure 5 shows a typical analog loop control SMU block diagram—for more information see Parametric Measurement | Analog Devices.

Figure 5
Some recommend parts are shown in Table 1:
|
Block Diagram Name |
Function |
Part Number |
Description |
|
VREF |
Voltage Reference |
LM399,ADR45xx D version |
0.5ppm/°C temperature drift |
|
SP DAC |
DAC |
AD5761, AD5781 |
precision output DAC, 16bit to 18bit, for setpoint |
|
CMP DAC |
DAC |
AD5685R |
14bit DAC, for setting compliance |
|
I ADC |
ADC |
AD717X series |
low speed, high precision sigma delta ADC |
|
V ADC |
AD7982,AD4000 series |
high speed, high precison SAR ADC |
|
|
Current sense
|
HV Buffer |
ADHV4702-1,ADA4700-1, LTC6090/1 |
Precision HV amp to buffer the input signal |
|
Difference Amp |
LT6375, LT1997-3, LT5400 + HV Buffer |
Difference amp to remove the common mode voltage |
|
|
Voltage sense |
HV Buffer |
ADHV4702-1,ADA4700-1, LTC6090/1 |
HV amp to buffer the input signal (Optional) |
|
Difference Amp |
LT1997-2, LT6375 |
Difference amp to remove the common mode voltage |
|
|
Driver Amp, AMP |
HV Amp |
ADHV4702-1, ADA4700-1, LTC6090/1 |
High voltage Amp(drive output stage) |
There is also digital loop control SMU which requires an ADC with higher precision and speed than the analog loop control SMU. A digital loop control SMU example is shown in Figure 6.

Figure 6
For SMU solutions based on AD5522 PMU (Parametric Measurement Unit) IC, see ADI Multichannel Source Measurement Unit (SMU) Solution Guide. A system block diagram from this guide is given below:

Simplified Force Voltage, Measure Current Circuit
Figure 7 is the basic block to test leakage current.

Figure 7
Voltage source V1 sets the voltage to the Amplifier (ADHV4702-1) non-inverting input node, and by simple Op-Amp theory, the inverting input will match it (V+=V-). The leakage current of the MOSFET gate will go through the resistance R1 if the Amplifier bias current is low enough compared with MOSFET leakage current and the common mode voltage of Amplifier is bigger than the voltage applied to MOSFET plus voltage of Sense resistance R.
IGSS =(Vout-V1)/R
Figure 8 and Figure 9 are the LTSpice simulation graphs with ADHV4702-1. A sense resistor of 10MOhm is recommended to measure a leakage current of 10nA. The voltage on the sense resistor varies from 100.00801mv to 99.981308mv, which shows that ADHV4702-1 can measure 10nA easily due to its low bias current (+-2pA level at 25°C) at DC voltage Sweep from -20V to 20V.

Figure 8

Figure 9
Figure 10 and Figure 11 show a recommended signal chain and board implementation for leakage current test based on high voltage amplifier components.

Figure 10

Figure 11
In summary, we have discussed two methods to test the leakage current, using a standard SMU and simplified force voltage, measure current circuit. The functionality of a SMU is very powerful and this equipment can be used in many kinds of tests, but the solution is very complex and the cost is high. The simplified circuit using high voltage amplifier components is an easy way to achieve the desired result but with limited function and low cost.
For additional precision signal chain recommendations, please refer to analog.com/precision. Precision High Voltage signal chain examples are coming soon.
REFERENCES
[1] Datasheet IPA100N08N3 G (infineon.com)
[2] Keithley Low level voltage measurements handbook
[3] Tektronix SMU 2450 datasheet
[4] LTspice XVII simulation software
[6] ADI Multichannel Source Measurement Unit (SMU) Solution Guide
[7] Parametric Measurement | Analog Devices
[8] Precision Technology Signal Chains | Analog Devices, Inc.