Child Looking at the First Step of Some Stairs

JESD204 Bring-Up: From Link-Up to Data Integrity

This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying the most common failure points at each stage. High-speed data converters like the ADRV9009 rely on the JESD204 serial interface to stream gigabit-rate samples between the converter and FPGA fabric. Compared to parallel LVDS, JESD204 significantly reduces pin count and improves signal integrity, but its multi-phase initialization sequence and strict latency requirements make bring-up challenging. A single misconfigured parameter, subclass setting, LMFC boundary, or lane mapping can either prevent the link from establishing entirely or, more critically, produce a link that appears healthy while silently carrying corrupted samples.


JESD204B Key Parameters

Before touching hardware, the following parameters must be agreed upon and programmed identically in both the FPGA IP core and the ADRV9009 register map. Any mismatch will prevent the link from advancing past the Initial Lane Alignment Sequence (ILAS).

Parameter

Description

L

Number of lanes per link

M

Number of converters per device

F

Octets per frame per lane

K

Frames per multiframe

N / N'

Converter resolution / total bits per sample

LMFC

Local multiframe clock — period = K × F × 10/8 sample clocks

 

Bring-Up Sequence

JESD204B initialization follows four sequential phases, each building on the last.

Phase 1: Code Group Synchronization (CGS)

CGS is the entry point of every JESD204B bring-up. The FPGA asserts SYNC~ low, which instructs the ADRV9009 to continuously transmit K28.5 comma characters across all lanes. The FPGA's GTH transceivers use these characters to lock their clock and data recovery circuits and achieve word alignment.

The most common failure here is that it displays no comma lock on one or more lanes. This almost always traces back to a lane rate mismatch which verifies that the ADRV9009 profile rate, interpolation or decimation settings, and the Xilinx JESD204 IP line rate are all consistent. Persistent disparity errors, or not-in-table errors, usually indicate a signal integrity problem such as trace length mismatch or insufficient GTH pre-emphasis. Once all lanes achieve comma lock, the FPGA drives SYNC~ high to signal readiness for ILAS.

Phase 2: Initial Lane Alignment Sequence (ILAS)

Following Code Group Synchronization, the ADRV9009 transmits four multiframes. Alignment characters bookend each multiframe, and the second multiframe carries the full link configuration: L, M, F, K, N, N', S, HD, and subclass. The FPGA IP captures these values and compares them against its own programmed settings.

A mismatch in F or K is the most frequent ILAS failure on the ADRV9009, particularly when switching between bandwidth profiles that alter the sample rate and framing structure. The Xilinx JESD204 IP exposes status registers showing received versus locally programmed fields side by side, making this comparison straightforward. Multiframe misalignment across lanes, where lanes arrive at different LMFC boundaries, usually points to excessive lane-to-lane PCB trace skew that the elastic buffer cannot absorb.

Phase 3: Deterministic Latency Alignment

Deterministic latency is the defining capability of JESD204B subclass 1, guaranteeing identical pipeline delay from ADC sample capture to FPGA data valid across every power cycle and reset, essential for phased-array beamforming, multi-channel synchronization, and any timing-critical DSP chain. Missing even one of the three conditions below breaks this guarantee entirely.

  • First, SYSREF must be captured on the same rising edge of the device clock at both the ADRV9009 and the FPGA, establishing a shared LMFC phase reference.
  • Second, the elastic buffer must release its held lane data at a fixed, predetermined LMFC boundary.
  • Third, the elastic buffer must be deep enough to absorb the worst-case lane-to-lane skew without overflow or underflow.

A latency that varies across resets almost always means SYSREF is arriving at a marginal timing window. Adjust the SYSREF phase until setup and hold margins are comfortably met at both devices. The ADI ACE software includes a dedicated SYSREF timing diagnostic for the ADRV9009 that simplifies this considerably.

Phase 4: Data Integrity Verification

A link that has completed initialization is transferring data, but transferring data correctly is a separate question entirely. Three checks should always follow before bring-up is declared complete.

A PRBS test comes first: configure the ADRV9009 to transmit a known pseudo-random binary sequence and enable the PRBS checker in the Xilinx GTH infrastructure. Zero errors over a sustained interval confirms physical layer integrity, making it the right first test before any attempt is made to interpret actual data.

Next, switch to the ADRV9009 ramp generator and verify that received samples increment by exactly one LSB per clock with no missing codes. This catches lane swap and bit-slip faults that PRBS passes through undetected, faults that would cause the FPGA to silently process samples from the wrong converter channel.

Finally, inject an internal tone at 10 MHz, capture samples via AXI-DMA to DDR, and compute an FFT. A clean single-tone spectrum confirms end-to-end signal chain integrity from converter to FPGA memory.

 Data Integrity Verification Flow — PRBS → Ramp Pattern → Spectral Confirmation

Figure 1: Data Integrity Verification Flow — PRBS → Ramp Pattern → Spectral Confirmation

 

Benefits of the Methodology

JESD204B bring-up on the ZCU102 + ADRV9009 platform is a methodical process that rewards working through each phase in order rather than jumping ahead. CGS establishes a physical lane lock, ILAS verifies that both ends of the link agree on framing parameters, deterministic latency alignment ensures repeatable timing across resets, and data integrity checks confirm that the full signal chain delivers correct samples. Combining the ADI ACE diagnostics with the Xilinx JESD204 IP status registers at each phase makes the process systematic, repeatable, and straightforward to debug, even when issues arise.

Read all the blogs in the Transceiver to FPGA series.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.