Electricity pylons in a field at Dusk.

How Galvanic Isolation Makes Your SMPS Safer and Smarter

Every time you plug in a device, you trust a thin barrier of isolation to keep you safe. Welcome to a summary of a four-part exploration into a critical challenge in power supply design: achieving galvanic isolation in switched-mode power supplies (SMPS) without sacrificing performance. In this series from The Engineering Mind on EngineerZone by Kuo-Chang, we cover everything from the "why" of isolation to the techniques that make it practical.

How Galvanic Isolation Ensures Safety in Your SMPS Design

This opening blog post explains what galvanic isolation is and why it matters.

  • Galvanic isolation separates input and output stages so no direct current path exists between them, which is critical for human safety and equipment protection.
  • In an isolated SMPS, disconnection must occur in four places: the power path, the feedback path, and both supply lines (including ground).
  • The core challenge is to split the low-voltage side while maintaining power transfer and feedback control, all without sharing a common ground.
  • Non-isolation risks range from shock hazards to equipment damage, making isolation essential in many designs.

How Energy Transfer Works Across Isolated SMPS Designs

Here we get into the "how." The blog post covers structures that ensure galvanic separation while moving energy from input to output, and previews five transfer methods from ADI.

  • The transformer is the best element for transferring energy without a galvanic connection, exchanging power between electric and magnetic fields.
  • Real transformers are not perfect: copper losses and core losses both affect efficiency.
  • The direct power path must address high voltage and current handling, efficiency, EMI, integration, and cost.
  • The feedback path must balance sensitivity, stability, speed, size, and cost while preserving isolation.
  • This post introduces five energy-transfer methods: Flyback (from buck-boost), Iso-Buck (from a classic buck), Forward, Forward with Active Clamp, and Resonant LLC.

How Power Transfer Techniques Transform Isolated SMPS

This third blog post zooms in on the five architectures that make isolated power transfer possible.

  • Flyback stores energy in the transformer during one switching phase and releases it to the output in the next. It is simple and low-cost, ideal for lower-power supplies.
  • Iso-Buck is essentially a synchronous buck driving a gapped transformer. Its feedback loop is intrinsic, dramatically reducing the bill of materials.
  • Forward converters offer a classic isolated approach with direct energy transfer during the on time. Forward with Active Clamp adds magnetic energy recovery, improving efficiency over the basic topology.
  • Resonant LLC behaves like a DC-to-AC-to-DC converter, using a resonant tank to achieve high efficiency and low EMI.
  • Each topology carries trade-offs in power range, complexity, robustness, and cost. The right choice depends on your application's priorities.

How Smart Feedback Techniques Regulate Isolated SMPS

The final blog post tackles the trickiest piece of the puzzle: how do we regulate output voltage when we can’t measure it directly? Isolation requires the feedback path to cross the barrier without a direct electrical connection. Traditionally, this meant adding bulky elements like an optocoupler or a third winding. There is a smarter way.

  • Primary-side sensing measures Vout without a third winding or an optocoupler. It repurposes the existing primary winding as the sensing element, yielding a simpler transformer, reduced board area, easier implementation, and lower cost.
  • The Iso-Buck topology takes this simplicity further. It is essentially a synchronous buck converter driving a gapped transformer rather than an inductor. When the switch is ON, the primary winding voltage is negative (equal to -VFB) while the secondary voltage is positive, transferring energy to the output. The roles reverse during the OFF time. The control loop closes on the primary side, eliminating the need for an optocoupler or third winding while remaining fully isolated.
  • Isolation techniques require additional bulky elements: a transformer, a third winding, an extra inductor, an optocoupler, diodes, and more. This is why many semiconductor companies, including Analog Devices, offer isolated DC-to-DC regulators in modules that integrate nearly all the necessary components, easing the design burden while preserving isolation and regulation performance.
  • The choice of feedback loop depends on the transfer scheme (flyback, iso-buck, forward) and on the desired performance in terms of regulation quality, speed, noise, size, and cost.
  • The series concludes with a powerful insight: isolation does not mean isolation from control. With clever engineering, we maintain precise regulation while keeping input and output safely separated.

Why You Should Read the Full Series

If you design power supplies, or simply want to understand how safe, efficient isolated conversion works, this series is worth your time. The full blog posts walk you through real topologies, real trade-offs, and real Analog Devices solutions with the depth you need. Explore the complete series on The Engineering  Mind on EngineerZone and discover what isolation can do for your next design.

 Enjoying this blog post? Check out all KCC blogs

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.