Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Energy
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Energy
Energy
Documents ADE1202
  • Q&A
  • File Uploads
  • Docs/ FAQs
  • Members
  • Tags
  • Cancel
  • +Product Documents
  • Hardware
  • Software
  • +Sensors Technology
  • -ADE1202: FAQ
    • ADE1202
  • +ADE77xx: FAQ
  • +ADE78xx: FAQ
  • +ADE7953: FAQ
  • +ADE79xx: FAQ
  • +ADE9xxx: FAQ

ADE1202

Table of Contents

  • Q1. Where I can download the GUI that accompanies the evaluation board?
  • Q2. I would like to write some embedded code for the ADE1202. Do you have any driver code available?
  • Q3. I would like to set the high current on time in the PL_HIGH_TIME register for 200ms to dissipate a large capacitive load. How can I do this?
  • Q4. What is the package creepage on the ADE1202?
  • Q5. On the ADE1202, can the you configure a different pulse current level for CH1 and CH2?
  • Q6. Can the SPI operate at 5V?
  • Q7. I have configured the part, but the binary input is not active. How can I fix it?
  • Q8. How long does it take for a register write to take effect?
  • Q9. I have modified some register configurations of the ADE1202 while in operation. I notice some unexpected pulse on Dout. What is wrong?
  • Q10. Does ADE1202 work with enhancement mode or depletion mode FETs?

Q1. Where I can download the GUI that accompanies the evaluation board?

A1. The GUI tool can be downloaded from this link

Q2. I would like to write some embedded code for the ADE1202. Do you have any driver code available?

A2. Yes, the ADE1202 driver code is written and compiled using the MBED online compiler. Follow this link to get the driver code. The code is written for the SDP-K1 evaluation board and can be connected to the ADE1202 evaluation board.

Q3. I would like to set the high current on time in the PL_HIGH_TIME register for 200ms to dissipate a large capacitive load. How can I do this?

A3. The maximum allowed high current time is 40.95 ms. The IC was designed with this limitation in mind to ensure the thermal limitations of the package are not breached. Another way to dissipate capacitive loads is to use a shorter pulse time and higher pulse current.

Q4. What is the package creepage on the ADE1202?

A4. The ADE1202 has an LGA package with 6.8mm creepage

Q5. On the ADE1202, can the you configure a different pulse current level for CH1 and CH2?

A5. No. There is no option to set different current levels. Both pulse current levels will be the same.

Q6. Can the SPI operate at 5V?

A6. No. The SPI must be within the absolute max limits which is VDD + 0.3V

Q7. I have configured the part, but the binary input is not active. How can I fix it?

A7. After configuring the registers on the ADE1202 write 0xADE1 to CONFIG_LOCK register for configuration setting to take effect.

Q8. How long does it take for a register write to take effect?

A8. It takes 100us for a register write to take effect when writing across the isolation barrier.

Q9. I have modified some register configurations of the ADE1202 while in operation. I notice some unexpected pulse on Dout. What is wrong?

A9. ADI recommends issuing a software reset of the part before modifying any configuration settings. This will flush out all internal filters and ensure correct operation of the part.

Q10. Does ADE1202 work with enhancement mode or depletion mode FETs?

A: ADE1202 works with enhancement mode FET’s which are more common than depletion mode FET’s.

Tags: ADE1202 Binary Input
  • Share
  • History
  • More