Post Go back to editing

Inquiry Regarding ADE9113 Isolation Ratings for 1000 VDC Measurement Applications

Category: Hardware
Product Number: ADE9113

We are considering the ADE9113 for use in a DC voltage measurement circuit and would appreciate clarification regarding the isolation ratings of the device.

Our intended application is as follows:

Maximum DC bus voltage: 1000 VDC
Voltage measurement via a resistive divider connected to the ADE9113 voltage input

Communication to a microcontroller located in a SELV domain through the ADE9113's integrated isolation barrier

Use of the integrated isolated power supply provided by the ADE9113

After reviewing the ADE9113 datasheet and certification documents, we found the following specifications:

Reinforced insulation: 415 Vrms
Basic insulation: 830 Vrms
VIOWM = 405 Vrms
VIORM = 573 Vpeak
VISO = 5000 Vrms (1 minute)

We would appreciate your guidance on the following questions:

Is the ADE9113 suitable for a 1000 VDC working voltage under standard industrial safety certifications (e.g., IEC 61010-1 or IEC 62368-1)?

If so, does it meet the requirements for Basic or Reinforced insulation at this voltage?

Can the ADE9113 isolation barrier be continuously subjected to an approximately 1000 VDC potential difference between the high-voltage side and the SELV side?

How should the following ratings be interpreted for a 1000 VDC application?

VIOWM = 405 Vrms
VIORM = 573 Vpeak
Reinforced insulation at 415 Vrms

Our primary concern is not the ADC input range, since the bus voltage will be scaled using a resistor divider.

Rather, we would like to confirm whether the isolation barrier inside the ADE9113 is certified and intended for continuous operation in a system where approximately 1000 VDC exists between the high-voltage measurement domain and the SELV control domain.

Parents
  • Thank you very much for the detailed explanation.

    Your explanation regarding the distinction between package limitations (creepage and clearance) and the internal signal isolation process was extremely helpful. I also appreciate your clarification regarding the use of IEC 60664-1 Table F.4 and the reasoning behind the estimated working voltages for the ADE9113 package.

    I have a few follow-up questions.

    The system I am developing is evaluated in accordance with IEC 60664-1.

    In addition, the PCB will be coated with a conformal coating that is intended to meet the requirements of Type 1 protection as defined in IEC 60664-3.

    Therefore, I believe the insulation coordination may be evaluated using Pollution Degree 1 rather than Pollution Degree 2.

    Under the following assumptions:

    - ADE9113
    - Material Group II
    - Creepage distance = 8.3 mm
    - Pollution Degree 1 (according to IEC 60664-3 Type 1 protection)
    - Altitude below 2000 m

    My interpretation of IEC 60664-1 Table F.4 is that the package creepage distance may support approximately:

    2160 V for basic insulation
    1080 V for reinforced insulation

    Could you please comment on whether this interpretation is correct?

    In other words, if the equipment is evaluated as Pollution Degree 1, would the package creepage limitation of the ADE9113 still be a concern for a working voltage around 1000 VDC,

    or would the package-related limitations be considered acceptable in this case?

    Regarding the internal signal isolation process, you mentioned that:

    "The characterized DC working voltages are much higher than those reported in the datasheet for AC."

    This is very interesting.

    Would it be possible to share any characterized DC working-voltage data, lifetime data, application note, or engineering guidance related to the ADE9113 isolation barrier under DC stress?

    If the detailed data cannot be shared, could you at least indicate the maximum continuous DC working voltage that Analog Devices has characterized internally for the ADE9113 isolation barrier?

    I am trying to understand whether the remaining limitation is primarily the package insulation coordination requirements or the long-term reliability of the internal isolation barrier itself.

    Thank you again for your support and detailed explanations.

Reply
  • Thank you very much for the detailed explanation.

    Your explanation regarding the distinction between package limitations (creepage and clearance) and the internal signal isolation process was extremely helpful. I also appreciate your clarification regarding the use of IEC 60664-1 Table F.4 and the reasoning behind the estimated working voltages for the ADE9113 package.

    I have a few follow-up questions.

    The system I am developing is evaluated in accordance with IEC 60664-1.

    In addition, the PCB will be coated with a conformal coating that is intended to meet the requirements of Type 1 protection as defined in IEC 60664-3.

    Therefore, I believe the insulation coordination may be evaluated using Pollution Degree 1 rather than Pollution Degree 2.

    Under the following assumptions:

    - ADE9113
    - Material Group II
    - Creepage distance = 8.3 mm
    - Pollution Degree 1 (according to IEC 60664-3 Type 1 protection)
    - Altitude below 2000 m

    My interpretation of IEC 60664-1 Table F.4 is that the package creepage distance may support approximately:

    2160 V for basic insulation
    1080 V for reinforced insulation

    Could you please comment on whether this interpretation is correct?

    In other words, if the equipment is evaluated as Pollution Degree 1, would the package creepage limitation of the ADE9113 still be a concern for a working voltage around 1000 VDC,

    or would the package-related limitations be considered acceptable in this case?

    Regarding the internal signal isolation process, you mentioned that:

    "The characterized DC working voltages are much higher than those reported in the datasheet for AC."

    This is very interesting.

    Would it be possible to share any characterized DC working-voltage data, lifetime data, application note, or engineering guidance related to the ADE9113 isolation barrier under DC stress?

    If the detailed data cannot be shared, could you at least indicate the maximum continuous DC working voltage that Analog Devices has characterized internally for the ADE9113 isolation barrier?

    I am trying to understand whether the remaining limitation is primarily the package insulation coordination requirements or the long-term reliability of the internal isolation barrier itself.

    Thank you again for your support and detailed explanations.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.