Post Go back to editing

Intermittent CRC Errors

Category: Software
Product Number: ADE9430

We are operating in Burst mode using BURST_EN: set in CONFIG1 Register Bit[11], which enables fast burst-read functionality for registers 0x500 to 0x6FF (such as the waveform buffer). 

While BURST_EN is active we are also verifying CRC for registers outside of the burst read section of the registers. (0x500 to 0x6FF).. When we do this we are seeing intermittent CRC errors when we read these registers. 

The strange thing we are seeing when a CRC error is detected is the CRC returned from the ADE9430 is is either one of two values  3374 decimal or 21171 decimal .  See below:

  1. Can BURST_EN be active while we are checking the CRC on registers outside the burst register range 0x500 to 0x6FF?
  2. Are there any known issues with CRC when  BURST_EN is enabled? i did an internet search for known CRC/Burst issues and they mentioned there were issues.    link: https://www.google.com/search?q=ade9430+BURST_EN+is+set+in+Config+Register+1+Bit%5B11%5D+AND+crc&sa…
  3. Lastly I tried to test CRC using the  Power Quality library running on the EVAL-ADE9430 board and CRC checking s defaulted to disabled. When I tried to enable it, it did not work. could this be related to 

Best regards, 

- mike

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.