Post Go back to editing

Investigating Accuracy Drift at Negative Temperatures with ADE9000

Category: Hardware
Product Number: ADE9000

Hello,

We are currently working on an energy monitoring device which is implemented with an ADE9000.

During the qualification of the product under different temperature conditions, we experienced precision drifts at negative temperatures for V, I, and consequently P, as shown below:

injected -5°C Errors
V1 (V) I1 (A) PF P1 th (W) measured V1  (V) Measured Current I1 (A) measured Power P1 (W) absolute drift V1 (V) Relative Err V1   absolute drift I1 (mA) Relative Error I1  Absolute error P1 (W) Relative Power Error
230 10,00 1 2300,000 229,62 9,9907 2293,01 -0,38 -0,17% -9,3000 -0,09% -6,99 -0,30%
230 5,00 1 1150,000 229,62 4,9957 1146,59 -0,38 -0,17% -4,3000 -0,09% -3,41 -0,30%
230 2,50 1 575,000 229,63 2,4981 573,36 -0,37 -0,16% -1,9000 -0,08% -1,64 -0,29%
230 1,00 1 230,000 229,63 0,9992 229,34 -0,37 -0,16% -0,8000 -0,08% -0,66 -0,29%
230 0,50 1 115,000 229,63 0,4996 114,66 -0,37 -0,16% -0,4000 -0,08% -0,34 -0,30%
230 0,25 1 57,500 229,63 0,2499 57,34 -0,37 -0,16% -0,1000 -0,04% -0,16 -0,28%

-> we can see what looks like an offset in the voltage measurement, do you have any explanation for this? 

1- As a first step, we mounted 25 ppm resistors and then 10 ppm resistors for voltage channels, without improvement.

2- After that, we monitored the input voltage at the entry of the ADE9000 on channel V2, and we didn't get a real difference or drift after the resistor divider stage.

3- Also, we measured the internal 1.2V Vref, and we didn't see a large drift: Vref = 1.2556V @ 23°C and Vref = 1.2561V @ -5°C -> 11 ppm/°C.

Now we aim to integrate drift and gain compensation over temperature, as mentioned in the datasheet.

Is it possible to determine the drift profile of the ADE9000 in our hardware implementation?

Can we determine a general compensation factor based on experimental tests, rather than requiring calibration for each product?

Thanks,

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.